<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックSame FTM module used for Input capture and PWM output</title>
    <link>https://community.nxp.com/t5/S32K/Same-FTM-module-used-for-Input-capture-and-PWM-output/m-p/657370#M565</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear support Team,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using freescale S32K144 Evaluation board.I am trying to use PWMO and input capture on the same FTM(Channel 6 for Input capture and Channel 5 for PWM out put).I configured it successfully for the given frequency and duty cycle.When i am connecting input to the input capture channel output PWM goes off and remain off till i connected input.Please let me know if it is the limitation of SOC or there is some other way to use both&amp;nbsp;PWMO and input capture simultaneously.&lt;/P&gt;&lt;P&gt;As far as my knowledge is concern about FTM there is single MOD register for all channels and this is the limitation to achieve simultaneous operations.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Nitin verma&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Nov 2016 09:35:38 GMT</pubDate>
    <dc:creator>nitinverma</dc:creator>
    <dc:date>2016-11-14T09:35:38Z</dc:date>
    <item>
      <title>Same FTM module used for Input capture and PWM output</title>
      <link>https://community.nxp.com/t5/S32K/Same-FTM-module-used-for-Input-capture-and-PWM-output/m-p/657370#M565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear support Team,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using freescale S32K144 Evaluation board.I am trying to use PWMO and input capture on the same FTM(Channel 6 for Input capture and Channel 5 for PWM out put).I configured it successfully for the given frequency and duty cycle.When i am connecting input to the input capture channel output PWM goes off and remain off till i connected input.Please let me know if it is the limitation of SOC or there is some other way to use both&amp;nbsp;PWMO and input capture simultaneously.&lt;/P&gt;&lt;P&gt;As far as my knowledge is concern about FTM there is single MOD register for all channels and this is the limitation to achieve simultaneous operations.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Nitin verma&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Nov 2016 09:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Same-FTM-module-used-for-Input-capture-and-PWM-output/m-p/657370#M565</guid>
      <dc:creator>nitinverma</dc:creator>
      <dc:date>2016-11-14T09:35:38Z</dc:date>
    </item>
    <item>
      <title>Re: Same FTM module used for Input capture and PWM output</title>
      <link>https://community.nxp.com/t5/S32K/Same-FTM-module-used-for-Input-capture-and-PWM-output/m-p/657371#M566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This should work normally, it is different channels that have own control register.&lt;/P&gt;&lt;P&gt;Be sure you do not set the CnSC[ICRST] bit on channel configured for capture mode, otherwise a counter will be reseted on capture event.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Nov 2016 15:51:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Same-FTM-module-used-for-Input-capture-and-PWM-output/m-p/657371#M566</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2016-11-15T15:51:52Z</dc:date>
    </item>
  </channel>
</rss>