<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Need help with flashing S32K344 with PyOCD</title>
    <link>https://community.nxp.com/t5/S32K/Need-help-with-flashing-S32K344-with-PyOCD/m-p/2303261#M56471</link>
    <description>&lt;P&gt;For anyone running into the same issue, downgrading pyocd to v0.36.0 fixes it. v0.37.0 and later do not work&lt;/P&gt;</description>
    <pubDate>Thu, 29 Jan 2026 21:59:38 GMT</pubDate>
    <dc:creator>danielfu11</dc:creator>
    <dc:date>2026-01-29T21:59:38Z</dc:date>
    <item>
      <title>Need help with flashing S32K344 with PyOCD</title>
      <link>https://community.nxp.com/t5/S32K/Need-help-with-flashing-S32K344-with-PyOCD/m-p/2290496#M56001</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to flash a S32K344 MCU (specifically, on the MR-CANHUBK344 board) with PyOCD. Mostly, I am trying to get it to work with MCU-Link. However, flashing does not work with MCU-Link or J-Link.&lt;/P&gt;&lt;P&gt;I've confirmed that flashing works with J-Link when I use Segger's software, so my hardware setup is good.&lt;/P&gt;&lt;P&gt;I pasted the error that I get after running `pyocd load -t s32k344 -O connect_mode=reset-and-halt &amp;lt;path_to_my_hex&amp;gt; -vv` at the bottom of this post. I get this same error with MCU-Link or J-Link. Resetting the core seems to work, FWIW.&lt;/P&gt;&lt;P&gt;Can someone tell me what I am doing wrong, or can suggest how I can continue debugging this? I am using pyocd 0.42.0&lt;BR /&gt;&lt;BR /&gt;Any helps, tips, or points in the right direction is very appreciated. Thanks in advance!&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;```&lt;BR /&gt;0000246 I Target type is s32k344 [board]&lt;BR /&gt;0000258 D Running task load_svd [sequencer]&lt;BR /&gt;0000258 D Running task pre_connect [sequencer]&lt;BR /&gt;0000258 D Running task dp_init [sequencer]&lt;BR /&gt;0000258 D Running task lock_probe [sequencer]&lt;BR /&gt;0000258 D Running task get_probe_capabilities [sequencer]&lt;BR /&gt;0000258 D Running task connect [sequencer]&lt;BR /&gt;0000260 D Default wire protocol selected; using SWD [dap]&lt;BR /&gt;0000261 I DP IDR = 0x6ba02477 (v2 rev6) [dap]&lt;BR /&gt;0000261 D Running task clear_sticky_err [sequencer]&lt;BR /&gt;0000261 D Running task power_up_debug [sequencer]&lt;BR /&gt;0000261 D Running task check_version [sequencer]&lt;BR /&gt;0000261 D Running task unlock_probe [sequencer]&lt;BR /&gt;0000261 D Running task unlock_device [sequencer]&lt;BR /&gt;0000261 D Running task create_discoverer [sequencer]&lt;BR /&gt;0000261 D Running task discovery [sequencer]&lt;BR /&gt;0000261 D Running task find_aps [sequencer]&lt;BR /&gt;0000262 D Running task create_aps [sequencer]&lt;BR /&gt;0000262 D Running task create_ap.1 [sequencer]&lt;BR /&gt;0000264 D APB-AP#1 default HPROT=0 HNONSEC=0 [ap]&lt;BR /&gt;0000264 D APB-AP#1 implemented HPROT=0 HNONSEC=0 [ap]&lt;BR /&gt;0000265 I APB-AP#1 IDR = 0x54770002 (APB-AP var0 rev5) [discovery]&lt;BR /&gt;0000265 D Running task create_ap.4 [sequencer]&lt;BR /&gt;0000266 D AHB-AP#4 default HPROT=b HNONSEC=0 [ap]&lt;BR /&gt;0000267 D AHB-AP#4 implemented HPROT=f HNONSEC=1 [ap]&lt;BR /&gt;0000267 I AHB-AP#4 IDR = 0x84770001 (AHB-AP var0 rev8) [discovery]&lt;BR /&gt;0000267 D Running task create_ap.6 [sequencer]&lt;BR /&gt;0000268 I AP#6 IDR = 0x001c0030 (AP var3 rev0) [discovery]&lt;BR /&gt;0000268 D Running task create_ap.7 [sequencer]&lt;BR /&gt;0000268 I AP#7 IDR = 0x001c0040 (AP var4 rev0) [discovery]&lt;BR /&gt;0000268 D Running task enable_debug [sequencer]&lt;BR /&gt;0000268 D Running task find_components [sequencer]&lt;BR /&gt;0000268 D Running task init_ap.1 [sequencer]&lt;BR /&gt;0000271 I APB-AP#1 Class 0x1 ROM table #0 @ 0x80000000 (designer=00e:NXP part=995) [rom_table]&lt;BR /&gt;0000277 I [0]&amp;lt;80001000:Trace Funnel CS-400 class=9 designer=43b:Arm part=908 devtype=12 archid=0000 devid=38:0:0&amp;gt; [rom_table]&lt;BR /&gt;0000281 I [1]&amp;lt;80002000:Trace Funnel CS-400 class=9 designer=43b:Arm part=908 devtype=12 archid=0000 devid=38:0:0&amp;gt; [rom_table]&lt;BR /&gt;0000284 I [2]&amp;lt;80003000:Trace Funnel CS-400 class=9 designer=43b:Arm part=908 devtype=12 archid=0000 devid=38:0:0&amp;gt; [rom_table]&lt;BR /&gt;0000288 I [3]&amp;lt;80004000:ETF class=9 designer=43b:Arm part=961 devtype=32 archid=0000 devid=380:0:0&amp;gt; [rom_table]&lt;BR /&gt;0000292 I [4]&amp;lt;80005000:ETF class=9 designer=43b:Arm part=961 devtype=32 archid=0000 devid=480:0:0&amp;gt; [rom_table]&lt;BR /&gt;0000295 I [5]&amp;lt;80006000:ETF class=9 designer=43b:Arm part=961 devtype=32 archid=0000 devid=380:0:0&amp;gt; [rom_table]&lt;BR /&gt;0000299 I [6]&amp;lt;80007000:ETF class=9 designer=43b:Arm part=961 devtype=32 archid=0000 devid=380:0:0&amp;gt; [rom_table]&lt;BR /&gt;0000303 I [7]&amp;lt;80008000:HTM CS-400 class=9 designer=43b:Arm part=917 devtype=43 archid=0000 devid=0:0:0&amp;gt; [rom_table]&lt;BR /&gt;0000306 I [8]&amp;lt;80009000:CTI CS-400 class=9 designer=43b:Arm part=906 devtype=14 archid=0000 devid=40800:0:0&amp;gt; [rom_table]&lt;BR /&gt;0000312 I [9]&amp;lt;8000a000:TPIU CS-400 class=9 designer=43b:Arm part=912 devtype=11 archid=0000 devid=a0:0:0&amp;gt; [rom_table]&lt;BR /&gt;0000315 I [10]&amp;lt;8000b000:SWO CS-400 class=9 designer=43b:Arm part=914 devtype=11 archid=0000 devid=ea0:0:0&amp;gt; [rom_table]&lt;BR /&gt;0000318 I [11]&amp;lt;8000c000:TSGEN class=15 designer=43b:Arm part=101&amp;gt; [rom_table]&lt;BR /&gt;0000318 D [12]&amp;lt;0000d002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000318 D [13]&amp;lt;0000e002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000318 D [14]&amp;lt;0000f002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000318 D [15]&amp;lt;00010002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000318 D [16]&amp;lt;00011002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000318 D [17]&amp;lt;00012002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000320 D [18]&amp;lt;00013002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000320 D [19]&amp;lt;00014002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000320 D [20]&amp;lt;00015002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000320 D [21]&amp;lt;00016002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000320 D [22]&amp;lt;00017002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000320 D [23]&amp;lt;00018002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000320 D [24]&amp;lt;00019002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000320 D [25]&amp;lt;0001a002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000320 D [26]&amp;lt;0001b002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000322 D [27]&amp;lt;0001c002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000322 D [28]&amp;lt;0001d002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000322 D [29]&amp;lt;0001e002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000322 D [30]&amp;lt;0001f002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000322 D [31]&amp;lt;00020002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000322 D Running task init_ap.4 [sequencer]&lt;BR /&gt;0000326 I AHB-AP#4 Class 0x1 ROM table #0 @ 0xe00fe000 (designer=43b:Arm part=4c8) [rom_table]&lt;BR /&gt;0000330 I [0]&amp;lt;e00ff000:ROM class=1 designer=43b:Arm part=4c7&amp;gt; [rom_table]&lt;BR /&gt;0000330 I AHB-AP#4 Class 0x1 ROM table #1 @ 0xe00ff000 (designer=43b:Arm part=4c7) [rom_table]&lt;BR /&gt;0000335 I [0]&amp;lt;e000e000:SCS v7-M class=14 designer=43b:Arm part=00c&amp;gt; [rom_table]&lt;BR /&gt;0000337 I [1]&amp;lt;e0001000:DWT v7-M class=14 designer=43b:Arm part=002&amp;gt; [rom_table]&lt;BR /&gt;0000340 I [2]&amp;lt;e0002000:FPB v7-M class=14 designer=43b:Arm part=00e&amp;gt; [rom_table]&lt;BR /&gt;0000342 I [3]&amp;lt;e0000000:ITM v7-M class=14 designer=43b:Arm part=001&amp;gt; [rom_table]&lt;BR /&gt;0000342 D [4]&amp;lt;fff41002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000342 D [5]&amp;lt;fff42002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000346 I [1]&amp;lt;e0041000:ETM M7 class=9 designer=43b:Arm part=975 devtype=13 archid=4a13 devid=0:0:0&amp;gt; [rom_table]&lt;BR /&gt;0000349 I [2]&amp;lt;e0042000:CTI CS-400 class=9 designer=43b:Arm part=906 devtype=14 archid=0000 devid=40800:0:0&amp;gt; [rom_table]&lt;BR /&gt;0000349 D [3]&amp;lt;1ff02002 not present&amp;gt; [rom_table]&lt;BR /&gt;0000349 D Running task create_cores [sequencer]&lt;BR /&gt;0000349 D Creating SCS component [discovery]&lt;BR /&gt;0000349 D selected core #0 [soc_target]&lt;BR /&gt;0000353 I CPU core #0: Cortex-M7 r1p2, v7.0-M architecture [cortex_m]&lt;BR /&gt;0000353 I Extensions: [DSP, FPU, FPU_V5, MPU] [cortex_m]&lt;BR /&gt;0000353 I FPU present: FPv5-SP-D16-M [cortex_m]&lt;BR /&gt;0000353 D Running task create_components [sequencer]&lt;BR /&gt;0000353 D Creating Trace Funnel component [discovery]&lt;BR /&gt;0000354 D Creating Trace Funnel component [discovery]&lt;BR /&gt;0000355 D Creating Trace Funnel component [discovery]&lt;BR /&gt;0000356 D Creating TPIU component [discovery]&lt;BR /&gt;0000357 D Creating SWO component [discovery]&lt;BR /&gt;0000357 D Creating DWT component [discovery]&lt;BR /&gt;0000358 I 4 hardware watchpoints [dwt]&lt;BR /&gt;0000360 D Creating FPB component [discovery]&lt;BR /&gt;0000360 I 8 hardware breakpoints, 1 literal comparators [fpb]&lt;BR /&gt;0000360 D fpb has been disabled [fpb]&lt;BR /&gt;0000363 D Creating ITM component [discovery]&lt;BR /&gt;0000364 D Running task check_for_cores [sequencer]&lt;BR /&gt;0000364 D Running task halt_on_connect [sequencer]&lt;BR /&gt;0000364 D halting core 0 [cortex_m]&lt;BR /&gt;0000364 D Running task post_connect [sequencer]&lt;BR /&gt;0000364 D Running task post_connect_hook [sequencer]&lt;BR /&gt;0000364 D Running task create_flash [sequencer]&lt;BR /&gt;0000365 D Running task notify [sequencer]&lt;BR /&gt;0000365 D set reset catch, core 0 [cortex_m]&lt;BR /&gt;0000365 D removing all breakpoints before reset [manager]&lt;BR /&gt;0000365 D halting core 0 [cortex_m]&lt;BR /&gt;0000366 D reset, core 0, type=VECTRESET [cortex_m]&lt;BR /&gt;0000366 D no delegate or debug sequence handled reset; performing VECTRESET reset, core 0 [cortex_m]&lt;BR /&gt;0000469 D clear reset catch, core 0 [cortex_m]&lt;BR /&gt;0000470 D disabling hardware breakpoints after reset [manager]&lt;BR /&gt;0000472 I Loading &amp;lt;path_to_my_hex&amp;gt; [load_cmd]&lt;BR /&gt;0000520 D halting core 0 [cortex_m]&lt;BR /&gt;0000782 D resuming core 0 [cortex_m]&lt;BR /&gt;0000782 D added=[] removed=[] [manager]&lt;BR /&gt;0000782 D bps after flush={} [manager]&lt;BR /&gt;0000811 D Analyze time: 0.291050 [builder]&lt;BR /&gt;0000811 D halting core 0 [cortex_m]&lt;BR /&gt;0000815 D resuming core 0 [cortex_m]&lt;BR /&gt;0000815 D added=[] removed=[] [manager]&lt;BR /&gt;0000815 D bps after flush={} [manager]&lt;BR /&gt;0000827 D resuming core 0 [cortex_m]&lt;BR /&gt;0000827 D added=[] removed=[] [manager]&lt;BR /&gt;0000827 D bps after flush={} [manager]&lt;BR /&gt;0000834 D resuming core 0 [cortex_m]&lt;BR /&gt;0000835 D added=[] removed=[] [manager]&lt;BR /&gt;0000835 D bps after flush={} [manager]&lt;BR /&gt;0000842 D resuming core 0 [cortex_m]&lt;BR /&gt;0000842 D added=[] removed=[] [manager]&lt;BR /&gt;0000842 D bps after flush={} [manager]&lt;BR /&gt;0000845 D halting core 0 [cortex_m]&lt;BR /&gt;0000854 D resuming core 0 [cortex_m]&lt;BR /&gt;0000854 D added=[] removed=[] [manager]&lt;BR /&gt;0000854 D bps after flush={} [manager]&lt;BR /&gt;0001178 D resuming core 0 [cortex_m]&lt;BR /&gt;0001178 D added=[] removed=[] [manager]&lt;BR /&gt;0001178 D bps after flush={} [manager]&lt;BR /&gt;0001182 D uninit session &amp;lt;pyocd.core.session.Session object at 0x7fb9f7f447d0&amp;gt; [session]&lt;BR /&gt;0001182 D uninit board &amp;lt;pyocd.board.board.Board object at 0x7fb9fa9f2660&amp;gt; [board]&lt;BR /&gt;0001183 D resuming core 0 [cortex_m]&lt;BR /&gt;0001183 D added=[] removed=[] [manager]&lt;BR /&gt;0001183 D bps after flush={} [manager]&lt;BR /&gt;0001196 C flash program page failure (address 0x00400000; result code 0x1) [__main__]&lt;BR /&gt;```&lt;/P&gt;&lt;P&gt;If it is helpful, pyocd can detect both debug probes. here is the output of `pyocd list -v`&lt;BR /&gt;```&lt;BR /&gt;# Probe/Board Unique ID Target&lt;BR /&gt;------------------------------------------------------------------------------------&lt;BR /&gt;0 NXP Semiconductors MCU-LINK (r0FB) CMSIS-DAP V3.167 YVIKSUH0XBMF0 n/a&lt;/P&gt;&lt;P&gt;1 Segger J-Link Compact Base 823001019 n/a&lt;BR /&gt;```&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jan 2026 23:32:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-help-with-flashing-S32K344-with-PyOCD/m-p/2290496#M56001</guid>
      <dc:creator>danielfu11</dc:creator>
      <dc:date>2026-01-08T23:32:44Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with flashing S32K344 with PyOCD</title>
      <link>https://community.nxp.com/t5/S32K/Need-help-with-flashing-S32K344-with-PyOCD/m-p/2291016#M56024</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;DIV&gt;
&lt;P&gt;It looks like you’re asking about pyOCD usage for flashing the S32K344. The best place for detailed support on pyOCD is its official GitHub repository, as recommended in the board’s GitBook. Please refer to the documentation for this open-source project here:&amp;nbsp;&lt;A href="https://github.com/pyocd/pyOCD/tree/v0.36.0" target="_blank"&gt;https://github.com/pyocd/pyOCD/tree/v0.36.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I noticed you’ve already opened a discussion there, which is great—maintainers and contributors on GitHub can provide the most accurate guidance for pyOCD-specific issues.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Fri, 09 Jan 2026 12:37:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-help-with-flashing-S32K344-with-PyOCD/m-p/2291016#M56024</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2026-01-09T12:37:25Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with flashing S32K344 with PyOCD</title>
      <link>https://community.nxp.com/t5/S32K/Need-help-with-flashing-S32K344-with-PyOCD/m-p/2303261#M56471</link>
      <description>&lt;P&gt;For anyone running into the same issue, downgrading pyocd to v0.36.0 fixes it. v0.37.0 and later do not work&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jan 2026 21:59:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-help-with-flashing-S32K344-with-PyOCD/m-p/2303261#M56471</guid>
      <dc:creator>danielfu11</dc:creator>
      <dc:date>2026-01-29T21:59:38Z</dc:date>
    </item>
  </channel>
</rss>