<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K312 UART in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-UART/m-p/2302953#M56448</link>
    <description />
    <pubDate>Thu, 29 Jan 2026 10:37:43 GMT</pubDate>
    <dc:creator>chris_010</dc:creator>
    <dc:date>2026-01-29T10:37:43Z</dc:date>
    <item>
      <title>S32K312 UART</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-UART/m-p/2130453#M50693</link>
      <description>&lt;P&gt;Hello, I have a problem when using S32K312.&lt;BR /&gt;The CAN CLOCK I used originally was 60M, but I want to change it to 40M.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;But after I changed it to 40M, the LPUART1 I used could send messages but could not receive messages (LPUART1 is normal at 60M).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The problem is that I see that the CLOCK of LPUART1 is AIPS_SLOW_CLK. Even if I change the CAN CLOCK from 60M to 40M, the value of AIPS_SLOW_CLK is not changed.&lt;BR /&gt;How can I solve this problem?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The following is the CLOCK setting of CAN CLOCK60M&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="60M.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/346634iAD00F06EE7E0CA02/image-size/large?v=v2&amp;amp;px=999" role="button" title="60M.png" alt="60M.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;60M.png&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;The following is the CLOCK setting of CAN CLOCK40M&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="40M.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/346635i7F66019386F80C4E/image-size/large?v=v2&amp;amp;px=999" role="button" title="40M.png" alt="40M.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;40M.png&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;The following is the setting of LPUART1&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="UART.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/346636i21FC12B10F0FE832/image-size/large?v=v2&amp;amp;px=999" role="button" title="UART.png" alt="UART.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;UART.png&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;The following is the UART send/receive function I use&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="FUNCTION.png" style="width: 675px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/346637i373A79AC399A691C/image-size/large?v=v2&amp;amp;px=999" role="button" title="FUNCTION.png" alt="FUNCTION.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;FUNCTION.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 01:11:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-UART/m-p/2130453#M50693</guid>
      <dc:creator>lua40927</dc:creator>
      <dc:date>2025-07-09T01:11:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 UART</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-UART/m-p/2130637#M50705</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;keep the CORE/PLAT/SLOW clk ratios as stated in the chapter&amp;nbsp;24.7.2 System clocking configurations of the device RM. So for Option B config it is 1/2/4. If you need 40MHz on AIPS_PLAT_CLK, you should lower other clks as well to keep ratios as stated for this config.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 06:23:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-UART/m-p/2130637#M50705</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-07-09T06:23:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 UART</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-UART/m-p/2130693#M50713</link>
      <description>&lt;P&gt;Thank you very much for your reply&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 07:19:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-UART/m-p/2130693#M50713</guid>
      <dc:creator>lua40927</dc:creator>
      <dc:date>2025-07-09T07:19:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 UART</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-UART/m-p/2302953#M56448</link>
      <description />
      <pubDate>Thu, 29 Jan 2026 10:37:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-UART/m-p/2302953#M56448</guid>
      <dc:creator>chris_010</dc:creator>
      <dc:date>2026-01-29T10:37:43Z</dc:date>
    </item>
  </channel>
</rss>