<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Need working RTD version for S32 DS 3.6.4 with sample CAN application for S32K344 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Need-working-RTD-version-for-S32-DS-3-6-4-with-sample-CAN/m-p/2292359#M56083</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;We just received multiple EVBs:&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/MR-CANHUBK344" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/MR-CANHUBK344&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;We want to test out each board for working CAN interfaces. For this purpose please point to working CAN example projects and RTD version which have been tested. I am not interested in loopback examples, but full CAN example which demonstrate RX and TX on the given board.&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Tue, 13 Jan 2026 08:57:47 GMT</pubDate>
    <dc:creator>rizwan_at_disruptdotcom</dc:creator>
    <dc:date>2026-01-13T08:57:47Z</dc:date>
    <item>
      <title>Need working RTD version for S32 DS 3.6.4 with sample CAN application for S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Need-working-RTD-version-for-S32-DS-3-6-4-with-sample-CAN/m-p/2292359#M56083</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;We just received multiple EVBs:&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/MR-CANHUBK344" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/MR-CANHUBK344&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;We want to test out each board for working CAN interfaces. For this purpose please point to working CAN example projects and RTD version which have been tested. I am not interested in loopback examples, but full CAN example which demonstrate RX and TX on the given board.&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jan 2026 08:57:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-working-RTD-version-for-S32-DS-3-6-4-with-sample-CAN/m-p/2292359#M56083</guid>
      <dc:creator>rizwan_at_disruptdotcom</dc:creator>
      <dc:date>2026-01-13T08:57:47Z</dc:date>
    </item>
    <item>
      <title>Re: Need working RTD version for S32 DS 3.6.4 with sample CAN application for S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Need-working-RTD-version-for-S32-DS-3-6-4-with-sample-CAN/m-p/2292527#M56087</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;there is direct "&lt;SPAN&gt;IEEE1722 demo app&lt;/SPAN&gt;" demo example for this board available from its web page. But it was designed in S32DS3.4 and RTD2.0.0. You can simple refer to it. Most probably this will need to be ported, if you want to use latest S32DS, not sure of the RTD version you have. There was some successful port to S32DS3.5 and RTD300;&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/Porting-MR-CANHUBK344-IEEE1722-to-work-with-newer-S32DS-3-5-and/td-p/1775199" target="_blank"&gt;https://community.nxp.com/t5/S32K/Porting-MR-CANHUBK344-IEEE1722-to-work-with-newer-S32DS-3-5-and/td-p/1775199&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Simple CAN demo for FlexCAN0 is posted on&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/RTD600-MCAL-amp-IP-S32K3X4EVB-T172-FlexCAN-Example-Interrupt/ta-p/2142069" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/RTD600-MCAL-amp-IP-S32K3X4EVB-T172-FlexCAN-Example-Interrupt/ta-p/2142069&lt;/A&gt;&lt;BR /&gt;This should work on MR-CANHUBK344 as well, only check/modify the pin used for CAN0 EN/STB_N pins.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jan 2026 11:24:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-working-RTD-version-for-S32-DS-3-6-4-with-sample-CAN/m-p/2292527#M56087</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2026-01-13T11:24:46Z</dc:date>
    </item>
  </channel>
</rss>