<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: SENT Driver integration</title>
    <link>https://community.nxp.com/t5/S32K/SENT-Driver-integration/m-p/2290417#M55999</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256605"&gt;@annappa&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Example codes using low-level drivers (IP) and high-level drivers (MCAL) are provided with the RTDs. These examples are named Flexio_Sent_Ip_Receiver_S32K3xx and Sent_Receiver_S32K3xx (where xx refers to the specific derivative). They are available for the following devices: S32K396, S32K344, S32K358, S32K388, and S32K389.&lt;/P&gt;
&lt;P&gt;If you are using S32 Design Studio (S32DS), you can create a project directly from an example (&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-S32-Design-Studio-Create-a-New-S32DS-Project-from-Example/ta-p/1098969" target="_blank" rel="noopener"&gt;HOWTO: S32 Design Studio - Create a New S32DS Project from Example&lt;/A&gt;). For EB Tresos, you can find the examples in a path similar to the following:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Sent_TS_T40D34M60I0R0\examples\EBT&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
    <pubDate>Thu, 08 Jan 2026 18:49:04 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2026-01-08T18:49:04Z</dc:date>
    <item>
      <title>SENT Driver integration</title>
      <link>https://community.nxp.com/t5/S32K/SENT-Driver-integration/m-p/2290336#M55993</link>
      <description>&lt;P&gt;We have integrated the new NXP SENT driver&amp;nbsp;S32K3_RTD_6_0_0_D2506_ASR_REL_4_7_REV_0000_20250610&lt;/P&gt;&lt;P&gt;but when we call the Sent_Init() function we are getting some reset, so can you pls share the example/Demo project that uses the SENT driver .&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jan 2026 15:24:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SENT-Driver-integration/m-p/2290336#M55993</guid>
      <dc:creator>annappa</dc:creator>
      <dc:date>2026-01-08T15:24:14Z</dc:date>
    </item>
    <item>
      <title>Re: SENT Driver integration</title>
      <link>https://community.nxp.com/t5/S32K/SENT-Driver-integration/m-p/2290417#M55999</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256605"&gt;@annappa&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Example codes using low-level drivers (IP) and high-level drivers (MCAL) are provided with the RTDs. These examples are named Flexio_Sent_Ip_Receiver_S32K3xx and Sent_Receiver_S32K3xx (where xx refers to the specific derivative). They are available for the following devices: S32K396, S32K344, S32K358, S32K388, and S32K389.&lt;/P&gt;
&lt;P&gt;If you are using S32 Design Studio (S32DS), you can create a project directly from an example (&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-S32-Design-Studio-Create-a-New-S32DS-Project-from-Example/ta-p/1098969" target="_blank" rel="noopener"&gt;HOWTO: S32 Design Studio - Create a New S32DS Project from Example&lt;/A&gt;). For EB Tresos, you can find the examples in a path similar to the following:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Sent_TS_T40D34M60I0R0\examples\EBT&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jan 2026 18:49:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SENT-Driver-integration/m-p/2290417#M55999</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2026-01-08T18:49:04Z</dc:date>
    </item>
  </channel>
</rss>