<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K3xx question</title>
    <link>https://community.nxp.com/t5/S32K/S32K3xx-question/m-p/2289029#M55911</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;I have downloaded the file package "unified_bootloader_demo_V2.1", which includes three file packages: See the attachment. The first one is clearly a BOOTLOADER, but what are the purposes of the latter two files?And I compiled the first one. What should I do with the other two？&lt;BR /&gt;Thank you for your assistance.&lt;/P&gt;</description>
    <pubDate>Wed, 07 Jan 2026 02:23:06 GMT</pubDate>
    <dc:creator>ruixi</dc:creator>
    <dc:date>2026-01-07T02:23:06Z</dc:date>
    <item>
      <title>S32K3xx question</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-question/m-p/2289029#M55911</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I have downloaded the file package "unified_bootloader_demo_V2.1", which includes three file packages: See the attachment. The first one is clearly a BOOTLOADER, but what are the purposes of the latter two files?And I compiled the first one. What should I do with the other two？&lt;BR /&gt;Thank you for your assistance.&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jan 2026 02:23:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-question/m-p/2289029#M55911</guid>
      <dc:creator>ruixi</dc:creator>
      <dc:date>2026-01-07T02:23:06Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3xx question</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-question/m-p/2289474#M55951</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258525"&gt;@ruixi&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;App Demo is an application which will&amp;nbsp; be loaded to flash by the bootloader. User config folder then contains json configuration file for UI and binary form of the application.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please notice that Unified Bootloader is only unofficial demo provided AS IS with no guarantees and no support. It's not production code.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jan 2026 13:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-question/m-p/2289474#M55951</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2026-01-07T13:00:45Z</dc:date>
    </item>
  </channel>
</rss>