<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Inquiry about multicore example projects for S32K344MINI-EVB</title>
    <link>https://community.nxp.com/t5/S32K/Inquiry-about-multicore-example-projects-for-S32K344MINI-EVB/m-p/2288975#M55904</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258502"&gt;@asdfghj&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Currently, there are no examples available for multicore implementation using the S32K344MINI-EVB. However, I have listed several links to example codes for S32K3 devices that may be useful. While not all examples are specifically intended for the S32K344 device, the functionality is generally consistent across all S32K3 devices unless otherwise noted in the Reference Manual.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K324-Multi-Core-Example-Project-based-on-Whiteboard/m-p/1547771" target="_blank" rel="noopener"&gt;S32K324 Multi-Core Example Project based on Whiteboard&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-decouple-RTD400-Ip-C40-DS35/ta-p/1866329" target="_blank" rel="noopener"&gt;Example_S32K344_decouple_RTD400_Ip_C40_DS35&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K358-Multicore-Start-CM7-2-from-CM7-0/ta-p/1923889" target="_blank" rel="noopener"&gt;S32K358 Multicore Start CM7_2 from CM7_0&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Additionally, we provide examples of the Inter-Platform Communication Framework (IPCF), a subsystem that enables applications running on multiple homogeneous or heterogeneous processing cores to communicate over various transport interfaces.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
    <pubDate>Tue, 06 Jan 2026 21:07:38 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2026-01-06T21:07:38Z</dc:date>
    <item>
      <title>Inquiry about multicore example projects for S32K344MINI-EVB</title>
      <link>https://community.nxp.com/t5/S32K/Inquiry-about-multicore-example-projects-for-S32K344MINI-EVB/m-p/2288736#M55890</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I am currently working with the S32K344MINI-EVB&amp;nbsp; and would like to learn multicore startup and basic multicore operation on this platform.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Are there any official multicore example projects available for the S32K344MINI-EVB?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If not, are there any generic S32K344 multicore examples that can be used as a reference?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;If such examples are available, I would appreciate it if you could advise what configurations need to be modified to run them on the S32K344MINI-EVB.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jan 2026 10:09:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Inquiry-about-multicore-example-projects-for-S32K344MINI-EVB/m-p/2288736#M55890</guid>
      <dc:creator>asdfghj</dc:creator>
      <dc:date>2026-01-06T10:09:12Z</dc:date>
    </item>
    <item>
      <title>Re: Inquiry about multicore example projects for S32K344MINI-EVB</title>
      <link>https://community.nxp.com/t5/S32K/Inquiry-about-multicore-example-projects-for-S32K344MINI-EVB/m-p/2288975#M55904</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258502"&gt;@asdfghj&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Currently, there are no examples available for multicore implementation using the S32K344MINI-EVB. However, I have listed several links to example codes for S32K3 devices that may be useful. While not all examples are specifically intended for the S32K344 device, the functionality is generally consistent across all S32K3 devices unless otherwise noted in the Reference Manual.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K324-Multi-Core-Example-Project-based-on-Whiteboard/m-p/1547771" target="_blank" rel="noopener"&gt;S32K324 Multi-Core Example Project based on Whiteboard&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-decouple-RTD400-Ip-C40-DS35/ta-p/1866329" target="_blank" rel="noopener"&gt;Example_S32K344_decouple_RTD400_Ip_C40_DS35&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K358-Multicore-Start-CM7-2-from-CM7-0/ta-p/1923889" target="_blank" rel="noopener"&gt;S32K358 Multicore Start CM7_2 from CM7_0&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Additionally, we provide examples of the Inter-Platform Communication Framework (IPCF), a subsystem that enables applications running on multiple homogeneous or heterogeneous processing cores to communicate over various transport interfaces.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jan 2026 21:07:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Inquiry-about-multicore-example-projects-for-S32K344MINI-EVB/m-p/2288975#M55904</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2026-01-06T21:07:38Z</dc:date>
    </item>
  </channel>
</rss>