<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックADKP Password Change</title>
    <link>https://community.nxp.com/t5/S32K/ADKP-Password-Change/m-p/2281589#M55875</link>
    <description>&lt;P&gt;Hello NXP,&lt;BR /&gt;We are using the S32K312 board.&lt;BR /&gt;We would like to know whether it is possible to change (or reset) the previously configured ADKP after Configuration Lock when the Life-Cycle is in the In-Field state.&lt;/P&gt;&lt;P&gt;Additionally, we would like to know whether it is possible to change the Life-Cycle from IN_FIELD to CUST_DEL.&lt;/P&gt;</description>
    <pubDate>Tue, 06 Jan 2026 02:39:59 GMT</pubDate>
    <dc:creator>jeongwoo</dc:creator>
    <dc:date>2026-01-06T02:39:59Z</dc:date>
    <item>
      <title>ADKP Password Change</title>
      <link>https://community.nxp.com/t5/S32K/ADKP-Password-Change/m-p/2281589#M55875</link>
      <description>&lt;P&gt;Hello NXP,&lt;BR /&gt;We are using the S32K312 board.&lt;BR /&gt;We would like to know whether it is possible to change (or reset) the previously configured ADKP after Configuration Lock when the Life-Cycle is in the In-Field state.&lt;/P&gt;&lt;P&gt;Additionally, we would like to know whether it is possible to change the Life-Cycle from IN_FIELD to CUST_DEL.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jan 2026 02:39:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADKP-Password-Change/m-p/2281589#M55875</guid>
      <dc:creator>jeongwoo</dc:creator>
      <dc:date>2026-01-06T02:39:59Z</dc:date>
    </item>
    <item>
      <title>Re: ADKP Password Change</title>
      <link>https://community.nxp.com/t5/S32K/ADKP-Password-Change/m-p/2281658#M55877</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;DIV&gt;Section&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;4.2.1 Configurable HSE system attributes&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/STRONG&gt;of&amp;nbsp;&lt;STRONG&gt;&lt;EM&gt;RM758227-RM00286 HSE-B Firmware Reference Manual - V2.7(2.7).pdf&lt;/EM&gt;&lt;/STRONG&gt;&lt;EM&gt;:&lt;/EM&gt;&lt;BR clear="none" /&gt;&lt;FONT color="#808080"&gt;A set of programmable HSE system attributes within the secure NVM can be provisioned by the host via HSE administration services. Some of these attributes, once set, cannot be updated.&lt;/FONT&gt;&lt;/DIV&gt;
&lt;DIV&gt;&lt;STRONG&gt;ADKP&lt;/STRONG&gt; is listed in&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;Table 16. One-time configurable HSE system attributes&lt;/STRONG&gt;&lt;/DIV&gt;
&lt;DIV&gt;Therefore, it is impossible to update ADKP anymore.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;Page 17/299 states:&lt;/DIV&gt;
&lt;DIV&gt;&lt;FONT color="#808080"&gt;An LC transition is always one way. Reverting to a previous LC state is never possible.&lt;/FONT&gt;&lt;/DIV&gt;
&lt;DIV&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;</description>
      <pubDate>Tue, 06 Jan 2026 04:30:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADKP-Password-Change/m-p/2281658#M55877</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2026-01-06T04:30:39Z</dc:date>
    </item>
  </channel>
</rss>