<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K344 - Using built-in CRC engine to compute FS26 CRC-8 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-Using-built-in-CRC-engine-to-compute-FS26-CRC-8/m-p/2266974#M55621</link>
    <description>&lt;P&gt;As the title implies, I'm wondering if it's possible to use the built-in CRC enginer on my S32K344 to generate CRC-8 checksums required for SPI communication with the FS26.&lt;/P&gt;&lt;P&gt;The Seed and Polynomial is defined here, as per NXP's public AN14492:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="fede_ls_0-1766151122188.png" style="width: 615px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/370791i24265F817A448FA9/image-dimensions/615x249?v=v2" width="615" height="249" role="button" title="fede_ls_0-1766151122188.png" alt="fede_ls_0-1766151122188.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I already wrote my own CRC driver but I noticed that &lt;U&gt;the Reference Manual S32K3XXRM "58.3.2&lt;/U&gt;&lt;BR /&gt;&lt;U&gt;CRC calculations" does not define a method for calculating 8-bit CRC.&lt;/U&gt;&lt;/P&gt;&lt;P&gt;Is it possible to use the CRC engine to generate 8-bit checksums?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 19 Dec 2025 13:36:52 GMT</pubDate>
    <dc:creator>fede_ls</dc:creator>
    <dc:date>2025-12-19T13:36:52Z</dc:date>
    <item>
      <title>S32K344 - Using built-in CRC engine to compute FS26 CRC-8</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Using-built-in-CRC-engine-to-compute-FS26-CRC-8/m-p/2266974#M55621</link>
      <description>&lt;P&gt;As the title implies, I'm wondering if it's possible to use the built-in CRC enginer on my S32K344 to generate CRC-8 checksums required for SPI communication with the FS26.&lt;/P&gt;&lt;P&gt;The Seed and Polynomial is defined here, as per NXP's public AN14492:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="fede_ls_0-1766151122188.png" style="width: 615px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/370791i24265F817A448FA9/image-dimensions/615x249?v=v2" width="615" height="249" role="button" title="fede_ls_0-1766151122188.png" alt="fede_ls_0-1766151122188.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I already wrote my own CRC driver but I noticed that &lt;U&gt;the Reference Manual S32K3XXRM "58.3.2&lt;/U&gt;&lt;BR /&gt;&lt;U&gt;CRC calculations" does not define a method for calculating 8-bit CRC.&lt;/U&gt;&lt;/P&gt;&lt;P&gt;Is it possible to use the CRC engine to generate 8-bit checksums?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Dec 2025 13:36:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Using-built-in-CRC-engine-to-compute-FS26-CRC-8/m-p/2266974#M55621</guid>
      <dc:creator>fede_ls</dc:creator>
      <dc:date>2025-12-19T13:36:52Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 - Using built-in CRC engine to compute FS26 CRC-8</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Using-built-in-CRC-engine-to-compute-FS26-CRC-8/m-p/2268439#M55676</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Thank you for your patience.&lt;/P&gt;
&lt;P&gt;CRC in S32K3 supports 16-bit or 32-bit mode. This means CRC-8 could not be implemented by HW.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I recommend that you download FS26's RTD, as its API already includes a CRC-8 software implementation. Click&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D" target="_self"&gt;S32K3 Standard Software&lt;/A&gt; -&amp;gt; Automotive SW - SBC/PMIC - Real Time Drivers&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#808080"&gt;Please note that during the Christmas holiday period, our support response times may be longer than usual. In some cases, your request might be addressed after the New Year. Thank you for your understanding.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 24 Dec 2025 03:16:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Using-built-in-CRC-engine-to-compute-FS26-CRC-8/m-p/2268439#M55676</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-12-24T03:16:27Z</dc:date>
    </item>
  </channel>
</rss>