<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic lpuart overrun  interrupt in S32K</title>
    <link>https://community.nxp.com/t5/S32K/lpuart-overrun-interrupt/m-p/974865#M5555</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When the lpuart is at the 1 m baud rate, the overrun interrupt will always occur。How to solve it&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Jan 2020 09:27:33 GMT</pubDate>
    <dc:creator>ninghongxie</dc:creator>
    <dc:date>2020-01-06T09:27:33Z</dc:date>
    <item>
      <title>lpuart overrun  interrupt</title>
      <link>https://community.nxp.com/t5/S32K/lpuart-overrun-interrupt/m-p/974865#M5555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When the lpuart is at the 1 m baud rate, the overrun interrupt will always occur。How to solve it&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jan 2020 09:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/lpuart-overrun-interrupt/m-p/974865#M5555</guid>
      <dc:creator>ninghongxie</dc:creator>
      <dc:date>2020-01-06T09:27:33Z</dc:date>
    </item>
    <item>
      <title>Re: lpuart overrun  interrupt</title>
      <link>https://community.nxp.com/t5/S32K/lpuart-overrun-interrupt/m-p/974866#M5556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can advise some points on how to prevent overrun error:&lt;/P&gt;&lt;P&gt;- Decrease the BaudRate value&lt;/P&gt;&lt;P&gt;- Set the higher priority of LPUART interrupt&lt;/P&gt;&lt;P&gt;- Choose the fastest clock source for the LPUART&lt;/P&gt;&lt;P&gt;- You can consider using&amp;nbsp;the FIFO register, see 51.3.1.12 LPUART FIFO Register (FIFO) in the RM rev. 11.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jan 2020 11:45:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/lpuart-overrun-interrupt/m-p/974866#M5556</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2020-01-08T11:45:32Z</dc:date>
    </item>
  </channel>
</rss>