<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K396 ADC</title>
    <link>https://community.nxp.com/t5/S32K/S32K396-ADC/m-p/2264557#M55522</link>
    <description>&lt;P&gt;Our processor is S32K396. When using ADC, the following error occurred:&lt;BR /&gt;I have a total of 5 ADCs. Two of them use the channels 1 and 3 of the AD5 controller respectively. Occasionally, there will be abnormal data collection from channel 1. At this time, by measuring with a multimeter, there is voltage on the pins, but no values can be obtained. When channel 3 is shielded, channel 1 works normally.&lt;BR /&gt;The remaining 3 channels of ADC are each using a separate AD controller, and all are functioning properly.&lt;BR /&gt;The attachment contains the configuration of my AD5 components and the ADC acquisition code. Please take a look and let me know if there are any issues.&lt;BR /&gt;Thank you!&lt;/P&gt;&lt;P&gt;我们处理器为S32K396，使用ADC时出现如下错误：&lt;/P&gt;&lt;P&gt;我共有5路ADC，其中有两路分别用了AD5控制器的通道1和通道3；此时会偶发性出现通道1采集异常，此时通过万用表测量管脚上存在电压，但是采集不到值。当把通道3屏蔽掉之后，通道1工作正常。&lt;/P&gt;&lt;P&gt;剩余3路ADC分别单独使用一个AD控制器，均工作正常。&lt;/P&gt;&lt;P&gt;附件是我的AD5组件配置及ADC采集代码，麻烦看下什么问题。&lt;/P&gt;&lt;P&gt;谢谢!&lt;/P&gt;</description>
    <pubDate>Wed, 17 Dec 2025 08:24:07 GMT</pubDate>
    <dc:creator>YY2410</dc:creator>
    <dc:date>2025-12-17T08:24:07Z</dc:date>
    <item>
      <title>S32K396 ADC</title>
      <link>https://community.nxp.com/t5/S32K/S32K396-ADC/m-p/2264557#M55522</link>
      <description>&lt;P&gt;Our processor is S32K396. When using ADC, the following error occurred:&lt;BR /&gt;I have a total of 5 ADCs. Two of them use the channels 1 and 3 of the AD5 controller respectively. Occasionally, there will be abnormal data collection from channel 1. At this time, by measuring with a multimeter, there is voltage on the pins, but no values can be obtained. When channel 3 is shielded, channel 1 works normally.&lt;BR /&gt;The remaining 3 channels of ADC are each using a separate AD controller, and all are functioning properly.&lt;BR /&gt;The attachment contains the configuration of my AD5 components and the ADC acquisition code. Please take a look and let me know if there are any issues.&lt;BR /&gt;Thank you!&lt;/P&gt;&lt;P&gt;我们处理器为S32K396，使用ADC时出现如下错误：&lt;/P&gt;&lt;P&gt;我共有5路ADC，其中有两路分别用了AD5控制器的通道1和通道3；此时会偶发性出现通道1采集异常，此时通过万用表测量管脚上存在电压，但是采集不到值。当把通道3屏蔽掉之后，通道1工作正常。&lt;/P&gt;&lt;P&gt;剩余3路ADC分别单独使用一个AD控制器，均工作正常。&lt;/P&gt;&lt;P&gt;附件是我的AD5组件配置及ADC采集代码，麻烦看下什么问题。&lt;/P&gt;&lt;P&gt;谢谢!&lt;/P&gt;</description>
      <pubDate>Wed, 17 Dec 2025 08:24:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K396-ADC/m-p/2264557#M55522</guid>
      <dc:creator>YY2410</dc:creator>
      <dc:date>2025-12-17T08:24:07Z</dc:date>
    </item>
  </channel>
</rss>