<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Which SDK should be used to meet ASIL B standards for the FS32K144HAT0MMHT, and how can the firmware in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2264039#M55487</link>
    <description>&lt;P&gt;Which software development kit (SDK) is recommended for developing firmware that meets ASIL-B standards on the FS32K144HAT0MMHT microcontroller? Additionally, what specific firmware design practices, safety mechanisms, and implementation guidelines should be followed to ensure full ASIL-B compliance?&lt;/P&gt;</description>
    <pubDate>Tue, 16 Dec 2025 14:24:16 GMT</pubDate>
    <dc:creator>ARIVALAGAN</dc:creator>
    <dc:date>2025-12-16T14:24:16Z</dc:date>
    <item>
      <title>Which SDK should be used to meet ASIL B standards for the FS32K144HAT0MMHT, and how can the firmware</title>
      <link>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2264039#M55487</link>
      <description>&lt;P&gt;Which software development kit (SDK) is recommended for developing firmware that meets ASIL-B standards on the FS32K144HAT0MMHT microcontroller? Additionally, what specific firmware design practices, safety mechanisms, and implementation guidelines should be followed to ensure full ASIL-B compliance?&lt;/P&gt;</description>
      <pubDate>Tue, 16 Dec 2025 14:24:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2264039#M55487</guid>
      <dc:creator>ARIVALAGAN</dc:creator>
      <dc:date>2025-12-16T14:24:16Z</dc:date>
    </item>
    <item>
      <title>Re: Which SDK should be used to meet ASIL B standards for the FS32K144HAT0MMHT, and how can the firm</title>
      <link>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2264231#M55497</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258058"&gt;@ARIVALAGAN&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The SDK has not been developed in compliance to ISO26262, but with a Quality Managed Process instead.&lt;/P&gt;
&lt;P&gt;You can refer to the &lt;A href="https://www.nxp.com/design/design-center/software/automotive-software-and-tools/real-time-drivers-rtd:AUTOMOTIVE-RTD" target="_self"&gt;Real-Time Drivers (RTD)&lt;/A&gt;. They target&amp;nbsp;&lt;SPAN&gt;AUTOSAR applications and have full ISO 26262 compliance.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regarding the design practices, mechanisms, implementations, etc. please keep in mind that these considerations are fully up to the customer, and the safety standards which needs to be met by the project, since the ASIL grade is for the whole ECU system. My colleague explains it in this other community thread in more detail:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/What-makes-the-MCU-ASIL-compliant/td-p/960208" target="_blank"&gt;Solved: What makes the MCU ASIL compliant? - NXP Community&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;RTD and S32K1 both are designed as Safety Element out of Context (SEooC) integrated to ASIL applications up to level B (S32K3 + RTD up to ASIL D). So, RTDs being a software meant to be integrated to the application, the ASIL level depends on the integration environment and assumptions of use are part of the safety manual available in safety package.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There are some documents, guides and SW to follow for safety implementation, for example:&lt;/SPAN&gt;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN14068.pdf" target="_blank"&gt;AN14068 - S32K3/S32K1 + FS23 hardware and safety application - application note&lt;/A&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/design/design-center/software/functional-safety-software/s32-safety-software-framework-saf-and-safety-peripheral-drivers-spd:SAF" target="_blank"&gt;S32 Framework Boosts Vehicle Safety | NXP Semiconductors&lt;/A&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;SPAN&gt;Most of the remaining documentation is under "Secure Files". Please follow this guide:&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=SAFETY-DOC-PROCESS" target="_self"&gt;How to Request Access to NXP's Safety Documentation for NXP MCUs and MPUs&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Dec 2025 22:06:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2264231#M55497</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-12-16T22:06:43Z</dc:date>
    </item>
    <item>
      <title>Re: Which SDK should be used to meet ASIL B standards for the FS32K144HAT0MMHT, and how can the firm</title>
      <link>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2264388#M55506</link>
      <description>&lt;P&gt;Thanks for the reply. The NXP website mentions that the S32K144 supports some SCST libraries. What is the purpose of these libraries, and how can we test them?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Lib link :&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/software/functional-safety-software/structural-core-self-test-scst-library:SCST" target="_blank"&gt;Structural Core Self-Test (SCST) Library | NXP Semiconductors&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SCST_Image.JPG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/370342i0ECBEC8C65AB7FDB/image-size/large?v=v2&amp;amp;px=999" role="button" title="SCST_Image.JPG" alt="SCST_Image.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Dec 2025 04:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2264388#M55506</guid>
      <dc:creator>ARIVALAGAN</dc:creator>
      <dc:date>2025-12-17T04:49:35Z</dc:date>
    </item>
    <item>
      <title>Re: Which SDK should be used to meet ASIL B standards for the FS32K144HAT0MMHT, and how can the firm</title>
      <link>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2265243#M55551</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258058"&gt;@ARIVALAGAN&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The SCST is ISO 26262 Functional Safety compliant up to ASIL B and targets 90% diagnostic coverage (DC).&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The included tests cover most of the core instructions, as well as the tests targeting specific IP blocks of the core. Mainly:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Core control logic (branch control, exception control)&lt;/LI&gt;
&lt;LI&gt;Core data path including:&lt;BR /&gt;
&lt;UL&gt;
&lt;LI&gt;Register file and register multiplexing.&lt;/LI&gt;
&lt;LI&gt;ALU, Multiplier, Load/Store, and other execution units.&lt;/LI&gt;
&lt;LI&gt;Instruction decoder, 16-Bit, 32-Bit.&lt;/LI&gt;
&lt;LI&gt;SIMD logic&lt;/LI&gt;
&lt;/UL&gt;
&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;SPAN&gt;Keep in mind that this is a licensed premium software. Please contact your local NXP sales office for details about the pricing and ordering. The package includes the user manual documentation.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Dec 2025 17:50:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2265243#M55551</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-12-17T17:50:31Z</dc:date>
    </item>
    <item>
      <title>Re: Which SDK should be used to meet ASIL B standards for the FS32K144HAT0MMHT, and how can the firm</title>
      <link>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2265679#M55571</link>
      <description>&lt;P&gt;Can I get the Tech Support team’s email ID for India (Chennai and Bangalore)?&lt;/P&gt;</description>
      <pubDate>Thu, 18 Dec 2025 05:03:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2265679#M55571</guid>
      <dc:creator>ARIVALAGAN</dc:creator>
      <dc:date>2025-12-18T05:03:50Z</dc:date>
    </item>
    <item>
      <title>Re: Which SDK should be used to meet ASIL B standards for the FS32K144HAT0MMHT, and how can the firm</title>
      <link>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2265682#M55572</link>
      <description>&lt;P&gt;I've one more query ...&amp;nbsp;&lt;/P&gt;&lt;P&gt;Safety-peripheral-drivers&amp;nbsp; &amp;nbsp; - is It free for FS32K144HAT0MMHT&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/functional-safety-software/s32-safety-software-framework-saf-and-safety-peripheral-drivers-spd:SAF" target="_self"&gt;https://www.nxp.com/design/design-center/software/functional-safety-software/s32-safety-software-framework-saf-and-safety-peripheral-drivers-spd:SAF&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Dec 2025 05:07:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2265682#M55572</guid>
      <dc:creator>ARIVALAGAN</dc:creator>
      <dc:date>2025-12-18T05:07:43Z</dc:date>
    </item>
    <item>
      <title>Re: Which SDK should be used to meet ASIL B standards for the FS32K144HAT0MMHT, and how can the firm</title>
      <link>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2266252#M55592</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258058"&gt;@ARIVALAGAN&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;1. I cannot share the contact for direct support in the public community. This space is strictly for technical support. Please contact your distributor instead.&lt;/P&gt;
&lt;P&gt;2. Yes. SPD is standard software free of charge, included in the silicon price:&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K1-SPD-D&amp;amp;_gl=1*nhab2i*_ga*MTExODE0MzQ3My4xNzY1MjA3NjEw*_ga_WM5LE0KMSH*czE3NjYwNjgxOTQkbzEwJGcxJHQxNzY2MDcxOTg3JGozMiRsMCRoNzcwODk4NjM1" target="_blank" rel="nofollow noopener noreferrer"&gt;SW32K1-SPD-D&lt;/A&gt;&lt;SPAN&gt;. Please notice that SPD requires specific RTD package. It’s mentioned in the release notes file.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Dec 2025 15:40:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2266252#M55592</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-12-18T15:40:43Z</dc:date>
    </item>
    <item>
      <title>Re: Which SDK should be used to meet ASIL B standards for the FS32K144HAT0MMHT, and how can the firm</title>
      <link>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2266498#M55609</link>
      <description>&lt;P&gt;How do we use SPD in S32K1 RTD drivers using Design Studio software?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any proper document is there?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you suggest any RTD Version which support SPD ?&lt;/P&gt;</description>
      <pubDate>Fri, 19 Dec 2025 05:15:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2266498#M55609</guid>
      <dc:creator>ARIVALAGAN</dc:creator>
      <dc:date>2025-12-19T05:15:10Z</dc:date>
    </item>
    <item>
      <title>Re: Which SDK should be used to meet ASIL B standards for the FS32K144HAT0MMHT, and how can the firm</title>
      <link>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2266748#M55618</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;ARIVALAGAN&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;SPD is not free;&lt;/P&gt;
&lt;P&gt;please contact your distributor or NXP sales for more information.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/support/sample-and-buy/distributor-network:DISTRIBUTORS" target="_blank"&gt;https://www.nxp.com/support/sample-and-buy/distributor-network:DISTRIBUTORS&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;Can I get the Tech Support team’s email ID for India (Chennai and Bangalore)?&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;You can consult with TSR to see if NXP technical support is available at these locations.&lt;/P&gt;
&lt;H3 class="product-list-title"&gt;Live Chat&lt;/H3&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu" target="_blank"&gt;https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Dec 2025 09:35:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Which-SDK-should-be-used-to-meet-ASIL-B-standards-for-the/m-p/2266748#M55618</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2025-12-19T09:35:47Z</dc:date>
    </item>
  </channel>
</rss>