<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: EBtresos activate code</title>
    <link>https://community.nxp.com/t5/S32K/EBtresos-activate-code/m-p/2262105#M55363</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Here is the reply from&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Flexnet Help&lt;/SPAN&gt;:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;Now, our team is in the process of updating the activation code information in the system. It will be reflected soon, but until then, please use the new activation code provided below:&lt;/EM&gt;&lt;BR /&gt;&lt;STRONG&gt;&lt;EM&gt;F5CF-8A53-B979-CD50&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Mon, 13 Apr 2026 06:35:54 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2026-04-13T06:35:54Z</dc:date>
    <item>
      <title>EBtresos activate code</title>
      <link>https://community.nxp.com/t5/S32K/EBtresos-activate-code/m-p/2261405#M55347</link>
      <description>&lt;P&gt;您好，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;我试图在 AUTOSAR 中使用 EBtresos，但未能激活。&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;激活代码 ：B25C-AEBB-4319-BAB1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ERROR: flxActAppActivationSend (50040,41147,10248)&lt;BR /&gt;The quantity specified exceeds maximum quantity allowed (0).&lt;BR /&gt;Connection to FlexNet Operations Server failed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;因此，我需要另一个激活代码才能使用 EBtresos。&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;谢谢！&lt;/P&gt;</description>
      <pubDate>Fri, 12 Dec 2025 16:31:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EBtresos-activate-code/m-p/2261405#M55347</guid>
      <dc:creator>jawen</dc:creator>
      <dc:date>2025-12-12T16:31:22Z</dc:date>
    </item>
    <item>
      <title>Re: EBtresos activate code</title>
      <link>https://community.nxp.com/t5/S32K/EBtresos-activate-code/m-p/2262105#M55363</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Here is the reply from&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Flexnet Help&lt;/SPAN&gt;:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;Now, our team is in the process of updating the activation code information in the system. It will be reflected soon, but until then, please use the new activation code provided below:&lt;/EM&gt;&lt;BR /&gt;&lt;STRONG&gt;&lt;EM&gt;F5CF-8A53-B979-CD50&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 13 Apr 2026 06:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EBtresos-activate-code/m-p/2262105#M55363</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2026-04-13T06:35:54Z</dc:date>
    </item>
  </channel>
</rss>