<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K396 flexio SPI example not working in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K396-flexio-SPI-example-not-working/m-p/2261376#M55345</link>
    <description>&lt;P&gt;The other Spi_Transfer_S32K396 works, and is more closely aligned with what we are doing. So not a blocker for us.&lt;/P&gt;</description>
    <pubDate>Fri, 12 Dec 2025 15:46:23 GMT</pubDate>
    <dc:creator>Henrik-Wires</dc:creator>
    <dc:date>2025-12-12T15:46:23Z</dc:date>
    <item>
      <title>S32K396 flexio SPI example not working</title>
      <link>https://community.nxp.com/t5/S32K/S32K396-flexio-SPI-example-not-working/m-p/2261306#M55343</link>
      <description>&lt;P&gt;Cannot get the FlexIO SPI example Dspi_Flexio_Ip_Transfer_S32K396 to work. I have wired everything up as per the included description.txt but the FlexIO transaction never completes and the example is stuck at continiously checking&amp;nbsp;&lt;SPAN&gt;Flexio_Spi_Ip_GetStatus&lt;/SPAN&gt;().&lt;/P&gt;&lt;P&gt;Using Design Studio 3.6.3 (with 3.6.4 update) and RTD 6.0.0.&lt;/P&gt;</description>
      <pubDate>Fri, 12 Dec 2025 14:17:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K396-flexio-SPI-example-not-working/m-p/2261306#M55343</guid>
      <dc:creator>Henrik-Wires</dc:creator>
      <dc:date>2025-12-12T14:17:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K396 flexio SPI example not working</title>
      <link>https://community.nxp.com/t5/S32K/S32K396-flexio-SPI-example-not-working/m-p/2261376#M55345</link>
      <description>&lt;P&gt;The other Spi_Transfer_S32K396 works, and is more closely aligned with what we are doing. So not a blocker for us.&lt;/P&gt;</description>
      <pubDate>Fri, 12 Dec 2025 15:46:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K396-flexio-SPI-example-not-working/m-p/2261376#M55345</guid>
      <dc:creator>Henrik-Wires</dc:creator>
      <dc:date>2025-12-12T15:46:23Z</dc:date>
    </item>
    <item>
      <title>Re: S32K396 flexio SPI example not working</title>
      <link>https://community.nxp.com/t5/S32K/S32K396-flexio-SPI-example-not-working/m-p/2261397#M55346</link>
      <description>But not fully. Master do not receive data from slave. Will investigate further on monday.</description>
      <pubDate>Fri, 12 Dec 2025 16:10:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K396-flexio-SPI-example-not-working/m-p/2261397#M55346</guid>
      <dc:creator>Henrik-Wires</dc:creator>
      <dc:date>2025-12-12T16:10:38Z</dc:date>
    </item>
    <item>
      <title>Re: S32K396 flexio SPI example not working</title>
      <link>https://community.nxp.com/t5/S32K/S32K396-flexio-SPI-example-not-working/m-p/2261431#M55348</link>
      <description>Found the culpit. PTB28 is not wired to the MB by default on S32K396-BGA-DC1. Instead it is wired to the PHY connector.&lt;BR /&gt;&lt;BR /&gt;Changing pinout to using PTF0-3 for LPSPI2 works much better.&lt;BR /&gt;&lt;BR /&gt;And I am guessing this is also why the other example does not work as there is a lot of PHY pins not connected to the MB connectors.&lt;BR /&gt;&lt;BR /&gt;It is almost as if you have selected pinouts to make life extra hard in using your tools.</description>
      <pubDate>Fri, 12 Dec 2025 18:29:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K396-flexio-SPI-example-not-working/m-p/2261431#M55348</guid>
      <dc:creator>Henrik-Wires</dc:creator>
      <dc:date>2025-12-12T18:29:18Z</dc:date>
    </item>
  </channel>
</rss>