<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can the BootLoader based on RTD2.0 work properly with the APP based on RTD6.0? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Can-the-BootLoader-based-on-RTD2-0-work-properly-with-the-APP/m-p/2260562#M55320</link>
    <description>&lt;P&gt;The current version of the BootLoader I am using is based on RTD2.0 &lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099" target="_self"&gt;Obtained from this link&lt;/A&gt;&amp;nbsp;, and it can function properly with the RTD2.0 APP. After I upgraded the APP to version RTD6.0, it crashed immediately after the upgrade.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Can the BootLoader based on RTD2.0 work properly with the APP based on RTD6.0?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;There is another question, based on the same version. When the BootLoader uses &lt;STRONG&gt;LLD&lt;/STRONG&gt; and the APP uses &lt;STRONG&gt;MCAL&lt;/STRONG&gt;, will they be able to function properly?&lt;/P&gt;&lt;P&gt;These are two versions of the ld file and the memory data that has been read. The jump address from the BootLoader is 0x00441421.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="LD_compare.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/369612iFDEC8A9BA26D9BDA/image-size/large?v=v2&amp;amp;px=999" role="button" title="LD_compare.png" alt="LD_compare.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="READ_FLASH.png" style="width: 641px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/369613iF9F49309C9E97D20/image-size/large?v=v2&amp;amp;px=999" role="button" title="READ_FLASH.png" alt="READ_FLASH.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 12 Dec 2025 01:31:12 GMT</pubDate>
    <dc:creator>FrankLiu2019</dc:creator>
    <dc:date>2025-12-12T01:31:12Z</dc:date>
    <item>
      <title>Can the BootLoader based on RTD2.0 work properly with the APP based on RTD6.0?</title>
      <link>https://community.nxp.com/t5/S32K/Can-the-BootLoader-based-on-RTD2-0-work-properly-with-the-APP/m-p/2260562#M55320</link>
      <description>&lt;P&gt;The current version of the BootLoader I am using is based on RTD2.0 &lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099" target="_self"&gt;Obtained from this link&lt;/A&gt;&amp;nbsp;, and it can function properly with the RTD2.0 APP. After I upgraded the APP to version RTD6.0, it crashed immediately after the upgrade.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Can the BootLoader based on RTD2.0 work properly with the APP based on RTD6.0?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;There is another question, based on the same version. When the BootLoader uses &lt;STRONG&gt;LLD&lt;/STRONG&gt; and the APP uses &lt;STRONG&gt;MCAL&lt;/STRONG&gt;, will they be able to function properly?&lt;/P&gt;&lt;P&gt;These are two versions of the ld file and the memory data that has been read. The jump address from the BootLoader is 0x00441421.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="LD_compare.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/369612iFDEC8A9BA26D9BDA/image-size/large?v=v2&amp;amp;px=999" role="button" title="LD_compare.png" alt="LD_compare.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="READ_FLASH.png" style="width: 641px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/369613iF9F49309C9E97D20/image-size/large?v=v2&amp;amp;px=999" role="button" title="READ_FLASH.png" alt="READ_FLASH.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Dec 2025 01:31:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-the-BootLoader-based-on-RTD2-0-work-properly-with-the-APP/m-p/2260562#M55320</guid>
      <dc:creator>FrankLiu2019</dc:creator>
      <dc:date>2025-12-12T01:31:12Z</dc:date>
    </item>
    <item>
      <title>Re: Can the BootLoader based on RTD2.0 work properly with the APP based on RTD6.0?</title>
      <link>https://community.nxp.com/t5/S32K/Can-the-BootLoader-based-on-RTD2-0-work-properly-with-the-APP/m-p/2261144#M55338</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213974"&gt;@FrankLiu2019&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;DIV&gt;
&lt;DIV&gt;
&lt;P&gt;Any application built on RTD 2.0 is generally &lt;STRONG&gt;not compatible by default&lt;/STRONG&gt; with an application built on RTD 6.0. It is up to the user to validate and adapt the integration, as there are no official NXP examples for mixing these versions.&lt;/P&gt;
&lt;P&gt;BootLoader using &lt;STRONG&gt;LLD&lt;/STRONG&gt; and APP using &lt;STRONG&gt;MCAL&lt;/STRONG&gt; might work if the BootLoader leaves the system in a clean state (interrupts off, clocks/watchdog handled) and the APP reinitializes its own drivers.&lt;/P&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Fri, 12 Dec 2025 11:03:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-the-BootLoader-based-on-RTD2-0-work-properly-with-the-APP/m-p/2261144#M55338</guid>
      <dc:creator>PavelL</dc:creator>
      <dc:date>2025-12-12T11:03:02Z</dc:date>
    </item>
  </channel>
</rss>