<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GPIO IRQ in S32K</title>
    <link>https://community.nxp.com/t5/S32K/GPIO-IRQ/m-p/972095#M5524</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Antonio Pérez Laguarda&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once that you are in the interruption, you could check the &lt;SPAN class=""&gt;Port Data Input Register&lt;/SPAN&gt; (PDIR) register to verify which of the pins was the one that trigger the interruption.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/633852?commentID=633852#comment-633852" title="https://community.nxp.com/message/633852?commentID=633852#comment-633852"&gt;https://community.nxp.com/message/633852?commentID=633852#comment-633852&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="jive_macro_thread jive_macro link-titled" data-orig-content="Reading Input using PDIR(Port Data Input Register)" href="https://community.nxp.com/message/528044" title="Reading Input using PDIR(Port Data Input Register)"&gt;Reading Input using PDIR(Port Data Input Register)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Sep 2019 16:58:11 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2019-09-11T16:58:11Z</dc:date>
    <item>
      <title>GPIO IRQ</title>
      <link>https://community.nxp.com/t5/S32K/GPIO-IRQ/m-p/972094#M5523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with a S32K144 EVB. I had 5 interruptions assigned to PORTA, PORTB, PORTC, PORTD and PORTE.&lt;/P&gt;&lt;P&gt;Now I need to include more interruptions and I have a problem. Interrupts are activated when a rising edge occurs on one of the port pins regardless of the pin. &lt;BR /&gt;Is there any way to know which pin has activated the interrupt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Sep 2019 16:32:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/GPIO-IRQ/m-p/972094#M5523</guid>
      <dc:creator>antperlag1</dc:creator>
      <dc:date>2019-09-10T16:32:45Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO IRQ</title>
      <link>https://community.nxp.com/t5/S32K/GPIO-IRQ/m-p/972095#M5524</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Antonio Pérez Laguarda&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once that you are in the interruption, you could check the &lt;SPAN class=""&gt;Port Data Input Register&lt;/SPAN&gt; (PDIR) register to verify which of the pins was the one that trigger the interruption.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/633852?commentID=633852#comment-633852" title="https://community.nxp.com/message/633852?commentID=633852#comment-633852"&gt;https://community.nxp.com/message/633852?commentID=633852#comment-633852&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="jive_macro_thread jive_macro link-titled" data-orig-content="Reading Input using PDIR(Port Data Input Register)" href="https://community.nxp.com/message/528044" title="Reading Input using PDIR(Port Data Input Register)"&gt;Reading Input using PDIR(Port Data Input Register)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Sep 2019 16:58:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/GPIO-IRQ/m-p/972095#M5524</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-09-11T16:58:11Z</dc:date>
    </item>
  </channel>
</rss>