<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Uart Tx - DMA and Uart Rx - Interrupt in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Uart-Tx-DMA-and-Uart-Rx-Interrupt/m-p/2256133#M55175</link>
    <description>&lt;P&gt;Hii,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I am using s32k148 eval board and i am using s32 3.5 ide and in that i want to know how we can make uart tx channel as dma and uart rx channel as interrupt mode . But i am unable to do it because in the mex file configuration we can only configure the uart instance to only one method&amp;nbsp; either interrupt/dma mode and i have intially configured it to dma mode the total uart instance. and from there i don't know what to do, can anyone help?&lt;/P&gt;</description>
    <pubDate>Fri, 05 Dec 2025 12:10:11 GMT</pubDate>
    <dc:creator>Vamshi_</dc:creator>
    <dc:date>2025-12-05T12:10:11Z</dc:date>
    <item>
      <title>Uart Tx - DMA and Uart Rx - Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/Uart-Tx-DMA-and-Uart-Rx-Interrupt/m-p/2256133#M55175</link>
      <description>&lt;P&gt;Hii,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I am using s32k148 eval board and i am using s32 3.5 ide and in that i want to know how we can make uart tx channel as dma and uart rx channel as interrupt mode . But i am unable to do it because in the mex file configuration we can only configure the uart instance to only one method&amp;nbsp; either interrupt/dma mode and i have intially configured it to dma mode the total uart instance. and from there i don't know what to do, can anyone help?&lt;/P&gt;</description>
      <pubDate>Fri, 05 Dec 2025 12:10:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Uart-Tx-DMA-and-Uart-Rx-Interrupt/m-p/2256133#M55175</guid>
      <dc:creator>Vamshi_</dc:creator>
      <dc:date>2025-12-05T12:10:11Z</dc:date>
    </item>
  </channel>
</rss>