<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: spi in S32K</title>
    <link>https://community.nxp.com/t5/S32K/spi/m-p/971413#M5517</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hi Praveena F &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;You can corroborate if you receive data in the buffer that you specify to receive data, in this case, you have Master_receive_buff, in order to verify if you send data you can use a scope in the pad and additionaly verify if the callback is correctly called. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;As my coallgue mentioned before, we couldn't test a code as long as we don't have the specific memory that you are using, but in the datasheet of the memory should have all the commands that you need to be able to communicate, if you ahve any issue with the SPI, please let us know.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Jorge Alcala&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Jun 2019 20:08:56 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2019-06-12T20:08:56Z</dc:date>
    <item>
      <title>spi</title>
      <link>https://community.nxp.com/t5/S32K/spi/m-p/971404#M5508</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is this code correct to read device id using spi flash?if wrong please anyone correct it&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85885i7DA8A5D68451D970/image-size/large?v=v2&amp;amp;px=999" title="Screenshot (119).png" alt="Screenshot (119).png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 06:39:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi/m-p/971404#M5508</guid>
      <dc:creator>intern_praveena</dc:creator>
      <dc:date>2019-06-11T06:39:15Z</dc:date>
    </item>
    <item>
      <title>Re: spi</title>
      <link>https://community.nxp.com/t5/S32K/spi/m-p/971405#M5509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You&amp;nbsp;try to use an external flash via SPI? If yes this approach is wrong because FLASH driver provided in SDK is just for internal flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please use LPSPI driver and send the right commands to your external flash based on datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Razvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 07:22:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi/m-p/971405#M5509</guid>
      <dc:creator>razva_tilimpea</dc:creator>
      <dc:date>2019-06-11T07:22:02Z</dc:date>
    </item>
    <item>
      <title>Re: spi</title>
      <link>https://community.nxp.com/t5/S32K/spi/m-p/971406#M5510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes i did wrong,i m using only LPSPI but i dnt know the command to read&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 08:43:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi/m-p/971406#M5510</guid>
      <dc:creator>intern_praveena</dc:creator>
      <dc:date>2019-06-11T08:43:24Z</dc:date>
    </item>
    <item>
      <title>Re: spi</title>
      <link>https://community.nxp.com/t5/S32K/spi/m-p/971407#M5511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;now this is my code,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uint8_t Master_send_buff;&lt;BR /&gt; uint8_t Master_receive_buff;&lt;/P&gt;&lt;P&gt;uint16_t transferByteCount;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/&lt;BR /&gt; #ifdef PEX_RTOS_INIT&lt;BR /&gt; PEX_RTOS_INIT(); /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */&lt;BR /&gt; #endif&lt;BR /&gt; /*** End of Processor Expert internal initialization. ***/&lt;/P&gt;&lt;P&gt;/* Write your code here */&lt;BR /&gt; CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);&lt;BR /&gt; CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);&lt;/P&gt;&lt;P&gt;PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);&lt;BR /&gt; PINS_DRV_SetPinsDirection(PTB,(1&amp;lt;&amp;lt;14)&amp;amp;(1&amp;lt;&amp;lt;15)&amp;amp;(1&amp;lt;&amp;lt;16)&amp;amp;(1&amp;lt;&amp;lt;17));&lt;/P&gt;&lt;P&gt;LPSPI_DRV_MasterInit(LPSPICOM1,&amp;amp;lpspiCom1State,&amp;amp;lpspiCom1_MasterConfig0);&lt;BR /&gt; PINS_DRV_WritePins(PTB,(0&amp;lt;&amp;lt;17)); //pin low to enable device(chip_select)&lt;/P&gt;&lt;P&gt;while(1)&lt;BR /&gt; {&lt;BR /&gt; LPSPI_DRV_MasterTransfer(LPSPICOM1,Master_send_buff,&amp;amp;Master_receive_buff,transferByteCount);&lt;BR /&gt; &lt;BR /&gt; //LPSPI_DRV_MasterTransferBlocking(LPSPICOM1,Master_send_buff,&amp;amp;Master_receive_buff,transferByteCount,5);&lt;BR /&gt; PINS_DRV_WritePins(PTB,(1&amp;lt;&amp;lt;17)); //pin high to disable device&lt;BR /&gt; }&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 08:45:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi/m-p/971407#M5511</guid>
      <dc:creator>intern_praveena</dc:creator>
      <dc:date>2019-06-11T08:45:09Z</dc:date>
    </item>
    <item>
      <title>Re: spi</title>
      <link>https://community.nxp.com/t5/S32K/spi/m-p/971408#M5512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You have to fill tx buffer with data specific to your external memory and in your rx buffer you should have the ID.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Razvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 08:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi/m-p/971408#M5512</guid>
      <dc:creator>razva_tilimpea</dc:creator>
      <dc:date>2019-06-11T08:50:33Z</dc:date>
    </item>
    <item>
      <title>Re: spi</title>
      <link>https://community.nxp.com/t5/S32K/spi/m-p/971409#M5513</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;can u pls edit my code and send i cant understnd??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 09:01:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi/m-p/971409#M5513</guid>
      <dc:creator>intern_praveena</dc:creator>
      <dc:date>2019-06-11T09:01:13Z</dc:date>
    </item>
    <item>
      <title>Re: spi</title>
      <link>https://community.nxp.com/t5/S32K/spi/m-p/971410#M5514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't do this. I don't know what flash device you are using and probably I don't have it on my side to validate the code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Razvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 09:17:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi/m-p/971410#M5514</guid>
      <dc:creator>razva_tilimpea</dc:creator>
      <dc:date>2019-06-11T09:17:12Z</dc:date>
    </item>
    <item>
      <title>Re: spi</title>
      <link>https://community.nxp.com/t5/S32K/spi/m-p/971411#M5515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i m using only S32K144_100&amp;nbsp; EVB board simply.is it correct ???&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Write your local variable definition here */&lt;BR /&gt; uint8_t Master_send_buff[5]={0x10,0x20,0x30,0x40,0x50};&lt;BR /&gt; uint8_t Master_receive_buff[5]={0x00};&lt;/P&gt;&lt;P&gt;uint16_t transferByteCount;&lt;BR /&gt; uint32_t rx_size;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/&lt;BR /&gt; #ifdef PEX_RTOS_INIT&lt;BR /&gt; PEX_RTOS_INIT(); /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */&lt;BR /&gt; #endif&lt;BR /&gt; /*** End of Processor Expert internal initialization. ***/&lt;/P&gt;&lt;P&gt;/* Write your code here */&lt;BR /&gt; CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);&lt;BR /&gt; CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);&lt;/P&gt;&lt;P&gt;PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);&lt;BR /&gt; PINS_DRV_SetPinsDirection(PTB,(1&amp;lt;&amp;lt;14)&amp;amp;(1&amp;lt;&amp;lt;15)&amp;amp;(1&amp;lt;&amp;lt;16)&amp;amp;(1&amp;lt;&amp;lt;17));&lt;/P&gt;&lt;P&gt;LPSPI_DRV_MasterInit(LPSPICOM1,&amp;amp;lpspiCom1State,&amp;amp;lpspiCom1_MasterConfig0);&lt;BR /&gt; PINS_DRV_WritePins(PTB,(0&amp;lt;&amp;lt;17)); //pin low to enable device(chip_select)&lt;/P&gt;&lt;P&gt;while(1)&lt;BR /&gt; {&lt;BR /&gt; LPSPI_DRV_MasterTransfer(LPSPICOM1,Master_send_buff,&amp;amp;Master_receive_buff,transferByteCount);&lt;BR /&gt; PINS_DRV_WritePins(PTB,(1&amp;lt;&amp;lt;17)); //pin high to disable device&lt;BR /&gt; }&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 09:22:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi/m-p/971411#M5515</guid>
      <dc:creator>intern_praveena</dc:creator>
      <dc:date>2019-06-11T09:22:36Z</dc:date>
    </item>
    <item>
      <title>Re: spi</title>
      <link>https://community.nxp.com/t5/S32K/spi/m-p/971412#M5516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;is this correct? how i verify that data send and receive?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main(void)&lt;BR /&gt;{&lt;BR /&gt; /* Write your local variable definition here */&lt;BR /&gt; uint8_t Master_send_buff[2]={0x1,0x2};&lt;BR /&gt; uint8_t Master_receive_buff[2]={0x1};&lt;/P&gt;&lt;P&gt;uint16_t transferByteCount;&lt;BR /&gt; uint32_t rx_size;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/&lt;BR /&gt; #ifdef PEX_RTOS_INIT&lt;BR /&gt; PEX_RTOS_INIT(); /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */&lt;BR /&gt; #endif&lt;BR /&gt; /*** End of Processor Expert internal initialization. ***/&lt;/P&gt;&lt;P&gt;/* Write your code here */&lt;BR /&gt; CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);&lt;BR /&gt; CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);&lt;/P&gt;&lt;P&gt;PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);&lt;BR /&gt; PINS_DRV_SetPinsDirection(PTB,(1&amp;lt;&amp;lt;14)&amp;amp;(1&amp;lt;&amp;lt;15)&amp;amp;(1&amp;lt;&amp;lt;16)&amp;amp;(1&amp;lt;&amp;lt;17));&lt;/P&gt;&lt;P&gt;LPSPI_DRV_MasterInit(LPSPICOM1,&amp;amp;lpspiCom1State,&amp;amp;lpspiCom1_MasterConfig0);&lt;BR /&gt; PINS_DRV_WritePins(PTB,(0&amp;lt;&amp;lt;17)); //pin low to enable device(chip_select)&lt;/P&gt;&lt;P&gt;while(1)&lt;BR /&gt; {&lt;BR /&gt; LPSPI_DRV_MasterTransferBlocking(LPSPICOM1,Master_send_buff,&amp;amp;Master_receive_buff,transferByteCount,5);&lt;BR /&gt; PINS_DRV_WritePins(PTB,(1&amp;lt;&amp;lt;17)); //pin high to disable device&lt;BR /&gt; }&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 09:39:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi/m-p/971412#M5516</guid>
      <dc:creator>intern_praveena</dc:creator>
      <dc:date>2019-06-11T09:39:56Z</dc:date>
    </item>
    <item>
      <title>Re: spi</title>
      <link>https://community.nxp.com/t5/S32K/spi/m-p/971413#M5517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hi Praveena F &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;You can corroborate if you receive data in the buffer that you specify to receive data, in this case, you have Master_receive_buff, in order to verify if you send data you can use a scope in the pad and additionaly verify if the callback is correctly called. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;As my coallgue mentioned before, we couldn't test a code as long as we don't have the specific memory that you are using, but in the datasheet of the memory should have all the commands that you need to be able to communicate, if you ahve any issue with the SPI, please let us know.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Jorge Alcala&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2019 20:08:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi/m-p/971413#M5517</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-06-12T20:08:56Z</dc:date>
    </item>
    <item>
      <title>Re: spi</title>
      <link>https://community.nxp.com/t5/S32K/spi/m-p/971414#M5518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i just want to send and receive via spi??&lt;/P&gt;&lt;P&gt;is this correct for??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uint8_t Master_send_buff[3] = {0x01,0x02,0x03};&lt;BR /&gt; uint8_t Master_receive_buff[3] = {0x04,0x05,0x06};&lt;/P&gt;&lt;P&gt;uint32_t rx_data_size;&lt;/P&gt;&lt;P&gt;/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/&lt;BR /&gt; #ifdef PEX_RTOS_INIT&lt;BR /&gt; PEX_RTOS_INIT(); /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */&lt;BR /&gt; #endif&lt;BR /&gt; /*** End of Processor Expert internal initialization. ***/&lt;/P&gt;&lt;P&gt;/* Write your code here */&lt;BR /&gt; CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);&lt;BR /&gt; CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);&lt;/P&gt;&lt;P&gt;PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);&lt;BR /&gt; PINS_DRV_SetPinsDirection(PTD,(1&amp;lt;&amp;lt;0)&amp;amp;(1&amp;lt;&amp;lt;1));&lt;BR /&gt; PINS_DRV_SetPinsDirection(PTE,(1&amp;lt;&amp;lt;0)&amp;amp;(1&amp;lt;&amp;lt;1));&lt;/P&gt;&lt;P&gt;LPSPI_DRV_MasterInit(LPSPICOM1,&amp;amp;lpspiCom1State,&amp;amp;lpspiCom1_MasterConfig0);&lt;BR /&gt; PINS_DRV_WritePins(PTE,(0&amp;lt;&amp;lt;1)); //pin low to enable device&lt;/P&gt;&lt;P&gt;while(1)&lt;BR /&gt; {&lt;BR /&gt; LPSPI_Master_Transmit_Data(LPSPICOM1 ,Master_send_buff,3);&lt;BR /&gt; LPSPI_Master_Receive_Data(LPSPICOM1 ,Master_receive_buff,3);&lt;BR /&gt; PINS_DRV_WritePins(PTE,(1&amp;lt;&amp;lt;1)); //pin high to disable device&lt;BR /&gt; }&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jun 2019 08:29:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi/m-p/971414#M5518</guid>
      <dc:creator>intern_praveena</dc:creator>
      <dc:date>2019-06-17T08:29:38Z</dc:date>
    </item>
    <item>
      <title>Re: spi</title>
      <link>https://community.nxp.com/t5/S32K/spi/m-p/971415#M5519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hi Praveena F&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Theoretical is correct the implementation, but in this example, I cannot see what LPSPI_Master_Transmit_Data is doing. Also, you want a constantly transmission and reception? you have this in a while(1) and it will be difficult to track when the transmission happens. My recommendation is using the LPSPI_DRV_MasterTransferBlocking and with the callback set a flag that indicates that the transmission has finished.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Jorge Alcala&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jun 2019 13:12:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi/m-p/971415#M5519</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-06-18T13:12:43Z</dc:date>
    </item>
    <item>
      <title>Re: spi</title>
      <link>https://community.nxp.com/t5/S32K/spi/m-p/971416#M5520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what is the format to transmit&amp;nbsp;data, bcz there is some formate lke command + data + register address.I dnt know that format?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jun 2019 11:25:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi/m-p/971416#M5520</guid>
      <dc:creator>intern_praveena</dc:creator>
      <dc:date>2019-06-19T11:25:12Z</dc:date>
    </item>
    <item>
      <title>Re: spi</title>
      <link>https://community.nxp.com/t5/S32K/spi/m-p/971417#M5521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hi Praveena F &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;This is a common format when you work with memories, first, you have to send the specific command that could be WRITE, READ, READ ID, etc. then you send the data in the size required and finaly you specify the address of the register.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;As I mentioned before this is memory depended and you need to implement the code with the format that the datasheet of the memory specify.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Jorge Alcala&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jun 2019 20:37:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi/m-p/971417#M5521</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-06-19T20:37:27Z</dc:date>
    </item>
  </channel>
</rss>