<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: HVBMS s32k358 project</title>
    <link>https://community.nxp.com/t5/S32K/HVBMS-s32k358-project/m-p/2255130#M55105</link>
    <description>&lt;P&gt;Hi&amp;nbsp;BillWen,&lt;/P&gt;
&lt;P&gt;Here is the feedback from HVBMS team:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;Inside the Bms SL demo part there is a counter that limits the usage to a number of calls, to protect against production usage of demo SW.&amp;nbsp; This feature is inside our SW since the first release in 2021.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;So this is the intended behavior of our SW to avoid this, the customer should buy the premium.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;If they do not then, they will have to handle the TD extraction by their own.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 04 Dec 2025 08:55:26 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2025-12-04T08:55:26Z</dc:date>
    <item>
      <title>HVBMS s32k358 project</title>
      <link>https://community.nxp.com/t5/S32K/HVBMS-s32k358-project/m-p/2253548#M55025</link>
      <description>&lt;P&gt;Hi :&lt;/P&gt;&lt;P&gt;Currently, I try to develop BMS system based on s32k358 platform. I already refer the "HvBms800_774_772_TPL_Bring_Up" source code to develop.&lt;/P&gt;&lt;P&gt;Back to original code and EVB from NXP, I use this project and run on NXP&amp;nbsp;RD-K358BMU board, I found that&amp;nbsp;GeneralError would return error after system run about half to one hour. The error always related to SL layer part such as "ERROR_CMU_READ_MEASUREMENTS_SME3_ERROR".&lt;/P&gt;&lt;P&gt;I wonder know that is there a project or bring up source code without SL part? Because I can't figure out the problem. Really need NXP's help, thanks a lot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;BR, BillWen&lt;/P&gt;</description>
      <pubDate>Wed, 03 Dec 2025 00:45:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/HVBMS-s32k358-project/m-p/2253548#M55025</guid>
      <dc:creator>BillWen</dc:creator>
      <dc:date>2025-12-03T00:45:48Z</dc:date>
    </item>
    <item>
      <title>Re: HVBMS s32k358 project</title>
      <link>https://community.nxp.com/t5/S32K/HVBMS-s32k358-project/m-p/2253558#M55027</link>
      <description>&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;Updated attach files which is NXP example project "&lt;SPAN&gt;HvBms800_774_772_TPL_Bring_Up&lt;/SPAN&gt;"&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;BR, BillWen&lt;/P&gt;</description>
      <pubDate>Wed, 03 Dec 2025 00:54:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/HVBMS-s32k358-project/m-p/2253558#M55027</guid>
      <dc:creator>BillWen</dc:creator>
      <dc:date>2025-12-03T00:54:51Z</dc:date>
    </item>
    <item>
      <title>Re: HVBMS s32k358 project</title>
      <link>https://community.nxp.com/t5/S32K/HVBMS-s32k358-project/m-p/2255130#M55105</link>
      <description>&lt;P&gt;Hi&amp;nbsp;BillWen,&lt;/P&gt;
&lt;P&gt;Here is the feedback from HVBMS team:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;Inside the Bms SL demo part there is a counter that limits the usage to a number of calls, to protect against production usage of demo SW.&amp;nbsp; This feature is inside our SW since the first release in 2021.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;So this is the intended behavior of our SW to avoid this, the customer should buy the premium.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;If they do not then, they will have to handle the TD extraction by their own.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 04 Dec 2025 08:55:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/HVBMS-s32k358-project/m-p/2255130#M55105</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-12-04T08:55:26Z</dc:date>
    </item>
  </channel>
</rss>