<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K388 UART with Hardware flow control in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K388-UART-with-Hardware-flow-control/m-p/2253831#M55048</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;there is no direct example for S32K388. Also the RTD driver does not support setup for flow control.&amp;nbsp;&lt;BR clear="none" /&gt;You can add it by configuring MODIR register after UART initialization, assuming pins are properly assigned as well.&lt;/P&gt;
&lt;P&gt;I shared with you an example for S32K312 within a Case you submitted, so you can refer to it.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Wed, 03 Dec 2025 07:43:18 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2025-12-03T07:43:18Z</dc:date>
    <item>
      <title>S32K388 UART with Hardware flow control</title>
      <link>https://community.nxp.com/t5/S32K/S32K388-UART-with-Hardware-flow-control/m-p/2253154#M55011</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear sir,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there any exmple code which use cts rts in UART function of S32K388?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;BR,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sean Wu&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Dec 2025 12:05:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K388-UART-with-Hardware-flow-control/m-p/2253154#M55011</guid>
      <dc:creator>seanwu</dc:creator>
      <dc:date>2025-12-02T12:05:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32K388 UART with Hardware flow control</title>
      <link>https://community.nxp.com/t5/S32K/S32K388-UART-with-Hardware-flow-control/m-p/2253831#M55048</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;there is no direct example for S32K388. Also the RTD driver does not support setup for flow control.&amp;nbsp;&lt;BR clear="none" /&gt;You can add it by configuring MODIR register after UART initialization, assuming pins are properly assigned as well.&lt;/P&gt;
&lt;P&gt;I shared with you an example for S32K312 within a Case you submitted, so you can refer to it.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 03 Dec 2025 07:43:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K388-UART-with-Hardware-flow-control/m-p/2253831#M55048</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-12-03T07:43:18Z</dc:date>
    </item>
  </channel>
</rss>