<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: The eMcem_Fccu_ClearFault function within eMcem_Fccu_Init failed to clear errors.</title>
    <link>https://community.nxp.com/t5/S32K/The-eMcem-Fccu-ClearFault-function-within-eMcem-Fccu-Init-failed/m-p/2252260#M54957</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/179292"&gt;@Allen_863&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;This issue might be caused by active NCF faults. There is a known hardware issue with the NCF[0] lockstep error, which can be triggered when attaching a debugger.&lt;BR /&gt;Workaround: Avoid resetting the S32K device via the debugger. Instead, allow the application to start without the debugger (for example, insert a while(true) loop in the code), and then attach the debugger without causing a reset. This approach prevents raising the NCF[0] fault.&lt;BR /&gt;You can also check the NCF status registers to see if any faults are present when you observe the failure during eMcem_Init().&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
    <pubDate>Mon, 01 Dec 2025 10:49:37 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2025-12-01T10:49:37Z</dc:date>
    <item>
      <title>The eMcem_Fccu_ClearFault function within eMcem_Fccu_Init failed to clear errors.</title>
      <link>https://community.nxp.com/t5/S32K/The-eMcem-Fccu-ClearFault-function-within-eMcem-Fccu-Init-failed/m-p/2252083#M54944</link>
      <description>&lt;P&gt;I found that eMcem_Fccu_ClearFault is always returning E_NOT_OK. I tried increasing FCCU_MAX_FAULT_CLEAR_COUNT_U8, but it still doesn't clear.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Q9.png" style="width: 904px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/367952i928020CD71B1E078/image-size/large?v=v2&amp;amp;px=999" role="button" title="Q9.png" alt="Q9.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Q9.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have configured FCCU_ERR0 and FCCU_ERR1.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Q8.png" style="width: 910px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/367953iB36C706891943E5B/image-size/large?v=v2&amp;amp;px=999" role="button" title="Q8.png" alt="Q8.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Q8.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have configured the Handlers for FCCU_0_IRQn and FCCU_1_IRQn as FCCU_ALARM_ISR and FCCU_TIMEOUT_ISR, respectively.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Q7.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/367955i9B00166616D688F2/image-size/large?v=v2&amp;amp;px=999" role="button" title="Q7.png" alt="Q7.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Q7.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Then I tried setting FAULT GROUPS to DISABLE, but it still returned E_NOT_OK. What else could be the reason?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Q6.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/367956i1623AF24F9D45C11/image-size/large?v=v2&amp;amp;px=999" role="button" title="Q6.png" alt="Q6.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Q6.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Dec 2025 09:01:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/The-eMcem-Fccu-ClearFault-function-within-eMcem-Fccu-Init-failed/m-p/2252083#M54944</guid>
      <dc:creator>Allen_863</dc:creator>
      <dc:date>2025-12-01T09:01:38Z</dc:date>
    </item>
    <item>
      <title>Re: The eMcem_Fccu_ClearFault function within eMcem_Fccu_Init failed to clear errors.</title>
      <link>https://community.nxp.com/t5/S32K/The-eMcem-Fccu-ClearFault-function-within-eMcem-Fccu-Init-failed/m-p/2252260#M54957</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/179292"&gt;@Allen_863&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;This issue might be caused by active NCF faults. There is a known hardware issue with the NCF[0] lockstep error, which can be triggered when attaching a debugger.&lt;BR /&gt;Workaround: Avoid resetting the S32K device via the debugger. Instead, allow the application to start without the debugger (for example, insert a while(true) loop in the code), and then attach the debugger without causing a reset. This approach prevents raising the NCF[0] fault.&lt;BR /&gt;You can also check the NCF status registers to see if any faults are present when you observe the failure during eMcem_Init().&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 01 Dec 2025 10:49:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/The-eMcem-Fccu-ClearFault-function-within-eMcem-Fccu-Init-failed/m-p/2252260#M54957</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-12-01T10:49:37Z</dc:date>
    </item>
  </channel>
</rss>