<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックEB tresos Activation failed.</title>
    <link>https://community.nxp.com/t5/S32K/EB-tresos-Activation-failed/m-p/2250910#M54907</link>
    <description>&lt;P&gt;The activation code is the latest - F5CF-8A53-B979-CD50. Offline activation was also attempted, but it didn't work either.&lt;/P&gt;&lt;P&gt;Here is the log：&lt;/P&gt;&lt;P&gt;Activating NodeLocked License F5CF-8A53-B979-CD50, Number Of Licenses: 1&lt;BR /&gt;Status: 4, Creating request&lt;/P&gt;&lt;P&gt;Status: 5, Request created&lt;/P&gt;&lt;P&gt;Status: 6, Context created&lt;/P&gt;&lt;P&gt;Status: 7, Connected to remote server&lt;/P&gt;&lt;P&gt;Status: 0, Error&lt;/P&gt;&lt;P&gt;ERROR: flxActAppActivationSend (50018,41145,32)&lt;BR /&gt;Connection to FlexNet Operations Server failed.&lt;/P&gt;</description>
    <pubDate>Fri, 28 Nov 2025 07:22:08 GMT</pubDate>
    <dc:creator>daniel_li121</dc:creator>
    <dc:date>2025-11-28T07:22:08Z</dc:date>
    <item>
      <title>EB tresos Activation failed.</title>
      <link>https://community.nxp.com/t5/S32K/EB-tresos-Activation-failed/m-p/2250910#M54907</link>
      <description>&lt;P&gt;The activation code is the latest - F5CF-8A53-B979-CD50. Offline activation was also attempted, but it didn't work either.&lt;/P&gt;&lt;P&gt;Here is the log：&lt;/P&gt;&lt;P&gt;Activating NodeLocked License F5CF-8A53-B979-CD50, Number Of Licenses: 1&lt;BR /&gt;Status: 4, Creating request&lt;/P&gt;&lt;P&gt;Status: 5, Request created&lt;/P&gt;&lt;P&gt;Status: 6, Context created&lt;/P&gt;&lt;P&gt;Status: 7, Connected to remote server&lt;/P&gt;&lt;P&gt;Status: 0, Error&lt;/P&gt;&lt;P&gt;ERROR: flxActAppActivationSend (50018,41145,32)&lt;BR /&gt;Connection to FlexNet Operations Server failed.&lt;/P&gt;</description>
      <pubDate>Fri, 28 Nov 2025 07:22:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EB-tresos-Activation-failed/m-p/2250910#M54907</guid>
      <dc:creator>daniel_li121</dc:creator>
      <dc:date>2025-11-28T07:22:08Z</dc:date>
    </item>
    <item>
      <title>Re: EB tresos Activation failed.</title>
      <link>https://community.nxp.com/t5/S32K/EB-tresos-Activation-failed/m-p/2251121#M54914</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Seems everything is OK from our side but you cannot connect to license flexnet server of Elektrobit.&lt;/P&gt;
&lt;P&gt;Your license key is valid.&lt;/P&gt;
&lt;P&gt;Please get in touch with Elektrobit support in order to resolve this issue.&lt;/P&gt;
&lt;P&gt;Ale check the firewall, antivirus, etc if it is not blocking access to flexnet license server at your side. This is common issue.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Fri, 28 Nov 2025 10:12:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EB-tresos-Activation-failed/m-p/2251121#M54914</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2025-11-28T10:12:36Z</dc:date>
    </item>
  </channel>
</rss>