<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32DS is a mess</title>
    <link>https://community.nxp.com/t5/S32K/S32DS-is-a-mess/m-p/2249680#M54851</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222282"&gt;@ArkAndyFraser&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please delete the project (make sure to select the option Delete project contents on disk) and then recreate the S32DS project using an example? You can follow the steps in the guide &lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-S32-Design-Studio-Create-a-New-S32DS-Project-from-Example/ta-p/1098969" target="_blank" rel="noopener"&gt;HOWTO: S32 Design Studio - Create a New S32DS Project from Example&lt;/A&gt;, and then apply the previously shared steps.&lt;/P&gt;
&lt;P&gt;Please let me know if the issue persists.&lt;/P&gt;</description>
    <pubDate>Wed, 26 Nov 2025 18:08:43 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2025-11-26T18:08:43Z</dc:date>
    <item>
      <title>S32DS is a mess</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-is-a-mess/m-p/2248556#M54810</link>
      <description>&lt;P&gt;I have been using S32 DesignStudio 3.4 for quite some time for working with the S32K144 and find creating a new project, configuring the device and using the SDK so intuitive.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I decided to try the latest version of DesignStudio 3.6.4 and notice that there does not appear to be an SDK anymore but instead real-time drivers. Also, I create a new project from example and choose a simple Dio example and straight away, it will not build because a number of files are missing. Clicking on the .mex file opens the device configuration and most modules seem to be in error:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ArkAndyFraser_0-1764094348174.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/367190i20DCE7EE587FA15D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ArkAndyFraser_0-1764094348174.png" alt="ArkAndyFraser_0-1764094348174.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Why does this not compile without errors "out of the box" ?!&lt;/P&gt;&lt;P&gt;I then by accident found that you could right click on the error in the Problems window and choose to 'Add the SDK component' which then removes all the errors and the code builds&lt;/P&gt;&lt;P&gt;How is that intuitive !?&lt;/P&gt;&lt;P&gt;Sorry for the rant but it feels the design tools are becoming less intuitive over time.&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Nov 2025 18:16:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-is-a-mess/m-p/2248556#M54810</guid>
      <dc:creator>ArkAndyFraser</dc:creator>
      <dc:date>2025-11-25T18:16:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS is a mess</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-is-a-mess/m-p/2248691#M54812</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222282"&gt;@ArkAndyFraser&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;These errors occur because some required files have not been generated by S32 ConfigTools. To resolve this:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;In S32 Design Studio, open the Project Explorer view and select your current project.&lt;/LI&gt;
&lt;LI&gt;From the S32 Configuration Tool menu, choose the desired configuration tool (e.g., Pins, Clocks, Peripherals, etc.).&lt;/LI&gt;
&lt;LI&gt;Apply any desired changes&lt;/LI&gt;
&lt;LI&gt;Click S32 Configuration Tool → Update Code to regenerate the code.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Additional details for each example project are provided in the description.txt file included with it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 25 Nov 2025 22:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-is-a-mess/m-p/2248691#M54812</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2025-11-25T22:22:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS is a mess</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-is-a-mess/m-p/2249200#M54831</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Okay, so I created a new Dio project from example. Selected the project in the project explorer view. In the Config Tools menu, I clicked Update Code. It showed "No Change" for all of the source files. I hit Okay then build the project and get a number of errors including:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN&gt;../src/main.c:26:10: fatal error: Mcu.h: No such file or directory&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;C:/NXP/S32DS.3.6.4/S32DS/software/PlatformSDK_S32K1_S32M24/RTD/BaseNXP_TS_T40D2M30I0R0/include/Mcal.h:61:10: fatal error: DeviceDefinition.h: No such file or directory&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN&gt;It is interesting that this time, if I open the Peripherals view, I don't see errors against any of the modules like I did the first time.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ArkAndyFraser_0-1764149208247.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/367342i33131AD94B182B1B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ArkAndyFraser_0-1764149208247.png" alt="ArkAndyFraser_0-1764149208247.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;However, why does it not build?&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;</description>
      <pubDate>Wed, 26 Nov 2025 09:29:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-is-a-mess/m-p/2249200#M54831</guid>
      <dc:creator>ArkAndyFraser</dc:creator>
      <dc:date>2025-11-26T09:29:15Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS is a mess</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-is-a-mess/m-p/2249680#M54851</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222282"&gt;@ArkAndyFraser&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please delete the project (make sure to select the option Delete project contents on disk) and then recreate the S32DS project using an example? You can follow the steps in the guide &lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-S32-Design-Studio-Create-a-New-S32DS-Project-from-Example/ta-p/1098969" target="_blank" rel="noopener"&gt;HOWTO: S32 Design Studio - Create a New S32DS Project from Example&lt;/A&gt;, and then apply the previously shared steps.&lt;/P&gt;
&lt;P&gt;Please let me know if the issue persists.&lt;/P&gt;</description>
      <pubDate>Wed, 26 Nov 2025 18:08:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-is-a-mess/m-p/2249680#M54851</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2025-11-26T18:08:43Z</dc:date>
    </item>
  </channel>
</rss>