<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Need clarification on UART module name and clock enable method on S32K324/S32K344</title>
    <link>https://community.nxp.com/t5/S32K/Need-clarification-on-UART-module-name-and-clock-enable-method/m-p/2246833#M54757</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Can anyone answer this question?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 24 Nov 2025 08:03:34 GMT</pubDate>
    <dc:creator>minjaekang99</dc:creator>
    <dc:date>2025-11-24T08:03:34Z</dc:date>
    <item>
      <title>Need clarification on UART module name and clock enable method on S32K324/S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Need-clarification-on-UART-module-name-and-clock-enable-method/m-p/2245546#M54730</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working with the S32K324 evaluation board and using the S32K344-based HSE Demo project (S32K3XX_demo_app).&lt;BR /&gt;I am trying to initialize UART, but the header file provided in the demo (S32K344.h) does not contain any UART-related definitions.&lt;/P&gt;&lt;P&gt;The following symbols do NOT exist in the header:&lt;BR /&gt;- LPUART1 / LPUART0~4&lt;BR /&gt;- PCC_LPUARTx&lt;BR /&gt;- LPUART_CTRL_*_MASK, LPUART_STAT_*_MASK&lt;BR /&gt;- Baud register macros (OSR/SBR)&lt;/P&gt;&lt;P&gt;In the Reference Manual (Table 263), I can only see entries like “Low Power UART0~4” under Partition 2 clock mapping,&lt;BR /&gt;but there is no information about the actual peripheral module name or register block associated with these UARTs.&lt;/P&gt;&lt;P&gt;**I need clarification on the following:**&lt;/P&gt;&lt;P&gt;1. What is the exact UART peripheral name used on S32K324/S32K344?&lt;BR /&gt;(Is it LPUART, LINFlexD, FLEXIO-UART, or something else?)&lt;/P&gt;&lt;P&gt;2. What is the correct base address and register structure for this UART module?&lt;/P&gt;&lt;P&gt;3. How should I properly enable the UART clock?&lt;BR /&gt;- Which MC_ME COFB REQ bit corresponds to UART?&lt;BR /&gt;- Or should the clock be enabled via PCC instead?&lt;/P&gt;&lt;P&gt;4. Which SIUL2 MSCR pins correspond to UART TX/RX, and what ALT/SSS value should be used?&lt;/P&gt;&lt;P&gt;The S32K344.h header in the demo project contains no UART definitions, so I am unsure which UART module to use or how to enable it.&lt;BR /&gt;Any guidance or an official reference to the correct UART module and registers would be appreciated.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Sat, 22 Nov 2025 09:21:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-clarification-on-UART-module-name-and-clock-enable-method/m-p/2245546#M54730</guid>
      <dc:creator>minjaekang99</dc:creator>
      <dc:date>2025-11-22T09:21:33Z</dc:date>
    </item>
    <item>
      <title>Re: Need clarification on UART module name and clock enable method on S32K324/S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Need-clarification-on-UART-module-name-and-clock-enable-method/m-p/2246833#M54757</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Can anyone answer this question?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Nov 2025 08:03:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-clarification-on-UART-module-name-and-clock-enable-method/m-p/2246833#M54757</guid>
      <dc:creator>minjaekang99</dc:creator>
      <dc:date>2025-11-24T08:03:34Z</dc:date>
    </item>
    <item>
      <title>Re: Need clarification on UART module name and clock enable method on S32K324/S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Need-clarification-on-UART-module-name-and-clock-enable-method/m-p/2246873#M54761</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;there are individual header files for each peripheral&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1)&amp;nbsp;&lt;SPAN&gt;IP_LPUART_x (IP_LPUART_0,...),&amp;nbsp;IP_FLEXIO. See respective header files&lt;BR /&gt;2)&amp;nbsp;&amp;nbsp;This is specified in the device RM, in each peripheral chapter. Also check headers S32K344_LPUART.h,&amp;nbsp;S32K344_FLEXIO.h etc&lt;BR /&gt;3) check&amp;nbsp;Table 263. MC_ME partition peripheral mapping and clock control of the RM&lt;BR /&gt;4) not sure of the module do you refer to. It can be it is available on more pins. Refer to&amp;nbsp;S32K344_IO Signal Table sheet of S32K344_IOMUX excel file attached to the RM. chapter&amp;nbsp;4&lt;BR /&gt;Signal Multiplexing describe how to work with IO signal table.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Nov 2025 08:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-clarification-on-UART-module-name-and-clock-enable-method/m-p/2246873#M54761</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-11-24T08:40:46Z</dc:date>
    </item>
  </channel>
</rss>