<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to use eMIOS in QDEC mode on S32K396 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/How-to-use-eMIOS-in-QDEC-mode-on-S32K396/m-p/2208538#M54631</link>
    <description>&lt;P&gt;I am trying to use the eMIOS QDEC mode to decode an A/B phase signal at fairly high speed (about 100KHz), but not sure how this should be configured in Design Studio. The end goal is to connect it to a model in MBDT.&lt;/P&gt;&lt;P&gt;Does the S32DS I/O Configurator support QDEC mode? The MCAL ICU driver supports SAIC and PWM modes. But it does not seem to support QDEC mode?&lt;/P&gt;&lt;P&gt;If not supported, what is the best approach to manually configure the eMIOS and the A/B inputs to the channel?&lt;BR /&gt;&lt;BR /&gt;Or is there any other viable method to implement a Phase A/B quadrature decoder in S32K396? Looks like quadrature phase decoding is supported via eTPU as well?&lt;/P&gt;</description>
    <pubDate>Wed, 19 Nov 2025 11:16:52 GMT</pubDate>
    <dc:creator>Henrik-Wires</dc:creator>
    <dc:date>2025-11-19T11:16:52Z</dc:date>
    <item>
      <title>How to use eMIOS in QDEC mode on S32K396</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-eMIOS-in-QDEC-mode-on-S32K396/m-p/2208538#M54631</link>
      <description>&lt;P&gt;I am trying to use the eMIOS QDEC mode to decode an A/B phase signal at fairly high speed (about 100KHz), but not sure how this should be configured in Design Studio. The end goal is to connect it to a model in MBDT.&lt;/P&gt;&lt;P&gt;Does the S32DS I/O Configurator support QDEC mode? The MCAL ICU driver supports SAIC and PWM modes. But it does not seem to support QDEC mode?&lt;/P&gt;&lt;P&gt;If not supported, what is the best approach to manually configure the eMIOS and the A/B inputs to the channel?&lt;BR /&gt;&lt;BR /&gt;Or is there any other viable method to implement a Phase A/B quadrature decoder in S32K396? Looks like quadrature phase decoding is supported via eTPU as well?&lt;/P&gt;</description>
      <pubDate>Wed, 19 Nov 2025 11:16:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-eMIOS-in-QDEC-mode-on-S32K396/m-p/2208538#M54631</guid>
      <dc:creator>Henrik-Wires</dc:creator>
      <dc:date>2025-11-19T11:16:52Z</dc:date>
    </item>
    <item>
      <title>Re: How to use eMIOS in QDEC mode on S32K396</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-eMIOS-in-QDEC-mode-on-S32K396/m-p/2217238#M54667</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;eMIOS on S32K396 does not have QDEC mode implemented. List of available modes is given in Table 335&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1763615373394.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/366580iC9C1EDD22005A3EB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PetrS_0-1763615373394.png" alt="PetrS_0-1763615373394.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;PetrS_0-1763615373394.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The LCU can be configured to decode quadrature signals, see more in chapter&amp;nbsp;62.6.1.8 Incremental encoder of the RM.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;eTPU supports quadrature phase decoding as well, as you wrote.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Nov 2025 05:15:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-eMIOS-in-QDEC-mode-on-S32K396/m-p/2217238#M54667</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-11-20T05:15:28Z</dc:date>
    </item>
    <item>
      <title>Re: How to use eMIOS in QDEC mode on S32K396</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-eMIOS-in-QDEC-mode-on-S32K396/m-p/2255434#M55132</link>
      <description>&lt;P&gt;Thanks. I'll look into using the LCU, or maybe eTPU.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Dec 2025 16:22:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-eMIOS-in-QDEC-mode-on-S32K396/m-p/2255434#M55132</guid>
      <dc:creator>Henrik-Wires</dc:creator>
      <dc:date>2025-12-04T16:22:53Z</dc:date>
    </item>
  </channel>
</rss>