<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flex CAN Can't Receive in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Flex-CAN-Can-t-Receive/m-p/2205057#M54481</link>
    <description>&lt;P&gt;I have an S32K148 board, and I am running S32K148 Flex CAN code on S32 IDE for ARM.&amp;nbsp; I can check the data on the PCAN monitor, but if I am sending data from PCAN to code, I can't receive it. Kindly help me out. How to check the data in real-time expression and what to send using PCAN and check on real-time expression.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 14 Nov 2025 09:06:53 GMT</pubDate>
    <dc:creator>Turtledove</dc:creator>
    <dc:date>2025-11-14T09:06:53Z</dc:date>
    <item>
      <title>Flex CAN Can't Receive</title>
      <link>https://community.nxp.com/t5/S32K/Flex-CAN-Can-t-Receive/m-p/2205057#M54481</link>
      <description>&lt;P&gt;I have an S32K148 board, and I am running S32K148 Flex CAN code on S32 IDE for ARM.&amp;nbsp; I can check the data on the PCAN monitor, but if I am sending data from PCAN to code, I can't receive it. Kindly help me out. How to check the data in real-time expression and what to send using PCAN and check on real-time expression.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Nov 2025 09:06:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flex-CAN-Can-t-Receive/m-p/2205057#M54481</guid>
      <dc:creator>Turtledove</dc:creator>
      <dc:date>2025-11-14T09:06:53Z</dc:date>
    </item>
    <item>
      <title>Re: Flex CAN Can't Receive</title>
      <link>https://community.nxp.com/t5/S32K/Flex-CAN-Can-t-Receive/m-p/2205414#M54512</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256892"&gt;@Turtledove&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Are you using the provided examples with S32DS ARM (bare metal) or an example from the SDK (ProcessorExpert)?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Snag_989d5cd.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/365743i406E2EC72A444074/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Snag_989d5cd.png" alt="Snag_989d5cd.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Snag_989de0a.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/365744iC12AEBAA741B85FE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Snag_989de0a.png" alt="Snag_989de0a.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If you are using the bare metal approach, you can refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN5413.pdf" target="_blank" rel="noopener"&gt;AN5413&lt;/A&gt;, which provides software examples. Specifically, section 2.9 and 2.10 both provide FlexCAN 2.0 &amp;amp; FlexCAN FD routines.&lt;/P&gt;
&lt;P&gt;If you are using the SDK, you can follow the description.txt file from the imported example.&lt;/P&gt;
&lt;P&gt;1. Import the example to the workspace and generate the ProcessorExpert code through the "Components" view.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Snag_98dfe8f.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/365745i916EF728D7FDB052/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Snag_98dfe8f.png" alt="Snag_98dfe8f.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;2. "Generated_Code" folder should be present under the project directory. Next, build the project.&lt;/P&gt;
&lt;P&gt;3. This specific "can_pal_s32k148" example is setup to work with two EVBs, one as node A and the other one as node B. You can change this by defining either MASTER or SLAVE in the defines.&lt;/P&gt;
&lt;P&gt;But, since you are using a PCAN-USB, you can simply run the application on the S32K148EVB and connect J11 to your PCAN. After this, setup CAN FD bit timing as the example (500kpbs/1000kpbs &amp;amp; 87.5%/75% sample point).&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Snag_a409b1b.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/365753i676F483C3098F8DC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Snag_a409b1b.png" alt="Snag_a409b1b.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;4. After configuration and connections, you will receive a CAN frame when pressing either SW3 or SW4, and EVB will toggle LED0 and LED1 depending on data[0] for the sent frame:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Snag_a42fc4d.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/365754iFFEF1459EE9E83AE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Snag_a42fc4d.png" alt="Snag_a42fc4d.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;For Real-Time Expressions, please refer to this post:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio/How-do-I-enable-Live-View-for-variables-when-debugging/m-p/669271#:~:text=Simply%20Go%20to%20menu%20Window%20-%3E%20%22Show%20View%22,You%20should%20observe%20the%20variable%20is%20being%20updated." target="_blank"&gt;Solved: How do I enable Live View for variables when debugging? - NXP Community&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Fri, 14 Nov 2025 21:17:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flex-CAN-Can-t-Receive/m-p/2205414#M54512</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-11-14T21:17:45Z</dc:date>
    </item>
  </channel>
</rss>