<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: in-circuit flash reprogramming, executing from ram in S32K</title>
    <link>https://community.nxp.com/t5/S32K/in-circuit-flash-reprogramming-executing-from-ram/m-p/966078#M5446</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hi David Gabbay&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;So you are creating the jump function in assambly code? did you consider the thumb bit when you jump? Please remember that when a jump is perform in ARM, you need to add the bit to the address:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2012/11/14/thumbs-up-with-assembly-on-arm-cortex/" title="https://mcuoneclipse.com/2012/11/14/thumbs-up-with-assembly-on-arm-cortex/"&gt;Thumbs up with Assembly on ARM Cortex | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2017/10/29/adding-a-delay-to-the-arm-daplink-bootloader/" title="https://mcuoneclipse.com/2017/10/29/adding-a-delay-to-the-arm-daplink-bootloader/"&gt;Adding a Delay to the ARM DAPLink Bootloader | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hope this helps&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Oct 2019 22:44:44 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2019-10-18T22:44:44Z</dc:date>
    <item>
      <title>in-circuit flash reprogramming, executing from ram</title>
      <link>https://community.nxp.com/t5/S32K/in-circuit-flash-reprogramming-executing-from-ram/m-p/966075#M5443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a code example of S32K1xx&amp;nbsp;&lt;STRONG&gt;in-circuit flash reprogramming&lt;/STRONG&gt;. What I mean is a code embedded in an application. When it is called externally (interrupt)&amp;nbsp; it copied itself (and all associated sub functions) into RAM and run from there to accept (serially, via uart), a new version and program it into the flash.&lt;/P&gt;&lt;P&gt;I have done almost everything:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;copied the code to the RAM&lt;/LI&gt;&lt;LI&gt;verified all called functions are within the copied code&lt;/LI&gt;&lt;LI&gt;disabled all interrupts&lt;/LI&gt;&lt;LI&gt;jump to the right location in the ram&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I'm experiencing&amp;nbsp; exception once it starts running from ram.&lt;BR /&gt;I would expect it if the M0+ core would have an MMU, but it doesn't. Should I define ram as an executable space somewhere?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Oct 2019 13:06:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/in-circuit-flash-reprogramming-executing-from-ram/m-p/966075#M5443</guid>
      <dc:creator>MPC8313ERDB_h</dc:creator>
      <dc:date>2019-10-10T13:06:52Z</dc:date>
    </item>
    <item>
      <title>Re: in-circuit flash reprogramming, executing from ram</title>
      <link>https://community.nxp.com/t5/S32K/in-circuit-flash-reprogramming-executing-from-ram/m-p/966076#M5444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There isn't any special setting to run code from the RAM, the exception that you are facing could be happening due to overlapping your data memory and the code that you run, please verify the address that you have set for your loader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would highly recommend you using the bootloader that we already provided:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="jive_macro_thread jive_macro link-titled" data-orig-content="S32K144 Boot Mode" href="https://community.nxp.com/thread/451269" title="S32K144 Boot Mode"&gt;S32K144 Boot Mode&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Oct 2019 23:30:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/in-circuit-flash-reprogramming-executing-from-ram/m-p/966076#M5444</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-10-14T23:30:23Z</dc:date>
    </item>
    <item>
      <title>Re: in-circuit flash reprogramming, executing from ram</title>
      <link>https://community.nxp.com/t5/S32K/in-circuit-flash-reprogramming-executing-from-ram/m-p/966077#M5445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you, Jorge Antonio Alcala Vazquez, for your answer,&lt;BR /&gt;I have double-checked the copied code. It had NOT overwritten any data area or stack area.&lt;BR /&gt;Here is the flash level code:&lt;BR /&gt; &lt;BR /&gt; DG_memcpy((u32*)W32, (u32*)RAM_COPY_TO_ADDR, (u32)CPY_CODE_SIZE /* copy code */&lt;BR /&gt; asm(" isb"); /* sync */&lt;BR /&gt; asm(" dmb");&lt;BR /&gt; asm(" dsb");&lt;BR /&gt; &lt;BR /&gt; DG_jump(RAM_COPY_TO_ADDR); /* jump run from RAM */&lt;/P&gt;&lt;P&gt;Here is the first part of the copied code as captured by the FX debuger:&lt;/P&gt;&lt;P&gt;20002400: push {r7, lr}&lt;BR /&gt;20002402: sub sp, #24&lt;BR /&gt;20002404: add r7, sp, #0&lt;BR /&gt;20002406: str r0, [r7, #4]&lt;BR /&gt;20002408: cpsid i&lt;BR /&gt;2000240a: movs r0, #82 ; 0x52&lt;BR /&gt;2000240c: bl 0x20002928&lt;BR /&gt;20002410: bl 0x200024f0&lt;BR /&gt;20002414: movs r3, r0&lt;BR /&gt;20002416: str r3, [r7, #20]&lt;BR /&gt;20002418: ldr r3, [r7, #20]&lt;BR /&gt;2000241a: cmp r3, #0&lt;BR /&gt;2000241c: bne.n 0x200024ca&lt;BR /&gt;2000241e: movs r3, #0&lt;BR /&gt;20002420: str r3, [r7, #16]&lt;BR /&gt;20002422: b.n 0x200024ba&lt;BR /&gt;20002424: bl 0x20002660&lt;BR /&gt;20002428: movs r3, r0&lt;BR /&gt;......... ...&lt;/P&gt;&lt;P&gt;I have two (assembler) versions of the jump code (DG_jump): &lt;BR /&gt;First:&lt;BR /&gt; bx r0&lt;BR /&gt; &lt;BR /&gt;Second:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; push {r7, lr}&lt;BR /&gt; add r7, sp, #0&lt;BR /&gt; str r0,[r7, #4] /* take target address */&lt;BR /&gt; &lt;BR /&gt; isb&lt;BR /&gt; dmb&lt;BR /&gt; dsb&lt;BR /&gt; &lt;BR /&gt; pop {r7, pc}&lt;/P&gt;&lt;P&gt;The processor status reg prior to calling DG_jump was:&lt;BR /&gt;xpsr=0x61000000 (T bit is set)&lt;/P&gt;&lt;P&gt;When I stepped in I have experienced an exception.&lt;BR /&gt;xpsr=0x21000000&lt;BR /&gt;When I had a look at the stack(shown below) I realized that the T bit was cleared (00000020 little endian format):&lt;BR /&gt; 200037C0: 00240020 30160000 00020000 00240020 &lt;BR /&gt; 200037D0: 00000000 8F0A0000 00240020 &lt;EM&gt;&lt;STRONG&gt;00000020&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I have no idea&lt;STRONG&gt; what cause T bit to turned off&lt;/STRONG&gt;. In fact this is the bottom line where I need help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additional information: all interrupts are disabled including WDOG.&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;BR /&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Oct 2019 16:35:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/in-circuit-flash-reprogramming-executing-from-ram/m-p/966077#M5445</guid>
      <dc:creator>MPC8313ERDB_h</dc:creator>
      <dc:date>2019-10-18T16:35:31Z</dc:date>
    </item>
    <item>
      <title>Re: in-circuit flash reprogramming, executing from ram</title>
      <link>https://community.nxp.com/t5/S32K/in-circuit-flash-reprogramming-executing-from-ram/m-p/966078#M5446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hi David Gabbay&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;So you are creating the jump function in assambly code? did you consider the thumb bit when you jump? Please remember that when a jump is perform in ARM, you need to add the bit to the address:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2012/11/14/thumbs-up-with-assembly-on-arm-cortex/" title="https://mcuoneclipse.com/2012/11/14/thumbs-up-with-assembly-on-arm-cortex/"&gt;Thumbs up with Assembly on ARM Cortex | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2017/10/29/adding-a-delay-to-the-arm-daplink-bootloader/" title="https://mcuoneclipse.com/2017/10/29/adding-a-delay-to-the-arm-daplink-bootloader/"&gt;Adding a Delay to the ARM DAPLink Bootloader | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hope this helps&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Oct 2019 22:44:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/in-circuit-flash-reprogramming-executing-from-ram/m-p/966078#M5446</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-10-18T22:44:44Z</dc:date>
    </item>
  </channel>
</rss>