<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: spi_read_write</title>
    <link>https://community.nxp.com/t5/S32K/spi-read-write/m-p/963892#M5412</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please refer to the SDK documentation&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/89729i0061B61EC94563EC/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and use these functions instead:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/89732i257D5B3C55AE5D85/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If the non-blocking functions are used, you need to check whether the transfer is finished or still in progress before launching another transfer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This function can be used:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/89733i9BA292AC7DED485E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Also, I have noticed that you are using the oldest SDK 0.8.6 version.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would recommend using the new RTM 3.0.0, if possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Jun 2019 12:44:09 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2019-06-25T12:44:09Z</dc:date>
    <item>
      <title>spi_read_write</title>
      <link>https://community.nxp.com/t5/S32K/spi-read-write/m-p/963891#M5411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;i want to write data using SPI and i have to read the same.I m using S32K144_64 LQP .I attached my code below,please check that code whether it is correct or have to change ??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jun 2019 09:19:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi-read-write/m-p/963891#M5411</guid>
      <dc:creator>intern_praveena</dc:creator>
      <dc:date>2019-06-24T09:19:22Z</dc:date>
    </item>
    <item>
      <title>Re: spi_read_write</title>
      <link>https://community.nxp.com/t5/S32K/spi-read-write/m-p/963892#M5412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please refer to the SDK documentation&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/89729i0061B61EC94563EC/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and use these functions instead:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/89732i257D5B3C55AE5D85/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If the non-blocking functions are used, you need to check whether the transfer is finished or still in progress before launching another transfer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This function can be used:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/89733i9BA292AC7DED485E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Also, I have noticed that you are using the oldest SDK 0.8.6 version.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would recommend using the new RTM 3.0.0, if possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jun 2019 12:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/spi-read-write/m-p/963892#M5412</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-06-25T12:44:09Z</dc:date>
    </item>
  </channel>
</rss>