<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K342 HSE</title>
    <link>https://community.nxp.com/t5/S32K/S32K342-HSE/m-p/2198288#M54117</link>
    <description>&lt;P&gt;Have you installed on virgin device or there were already some attempts to have installed FW before?&lt;BR /&gt;Could you provide following information?&lt;BR /&gt;SBAF version:&lt;BR /&gt;HSE FW version:&lt;BR /&gt;MU registers, FSR, GSR, etc:&lt;BR /&gt;HSE GPR3:&lt;BR /&gt;Is the "HSE_STATUS_INIT_OK" have been wait set to "1"?&lt;/P&gt;
&lt;P&gt;In case AB SWAP, multiple resets may be required.&lt;/P&gt;
&lt;P&gt;Recently I have discussed installation procedure over following thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K3-HSE-Installation-differences-between-FULL-MEM-and-AB-SWAP/m-p/2190106/emcs_t/S2h8ZW1haWx8YW5zd2VyX2FjY2VwdGVkX2FzX3NvbHV0aW9ufE1ISkNBVTZXSFlVWEI1fDIxOTAxMDZ8QUNDRVBURURfU09MVVRJT05TfGhL#M53730" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K3-HSE-Installation-differences-between-FULL-MEM-and-AB-SWAP/m-p/2190106/emcs_t/S2h8ZW1haWx8YW5zd2VyX2FjY2VwdGVkX2FzX3NvbHV0aW9ufE1ISkNBVTZXSFlVWEI1fDIxOTAxMDZ8QUNDRVBURURfU09MVVRJT05TfGhL#M53730&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps&lt;/P&gt;</description>
    <pubDate>Tue, 04 Nov 2025 11:12:37 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2025-11-04T11:12:37Z</dc:date>
    <item>
      <title>S32K342 HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K342-HSE/m-p/2197997#M54086</link>
      <description>&lt;P&gt;Dear Sir：&lt;/P&gt;&lt;P&gt;We are a third-party programmer manufacturer.&lt;/P&gt;&lt;P&gt;The S32K342 programming flow has been completed.&lt;/P&gt;&lt;P&gt;After successfully programming the HSE file, repower on wait 5 seconds, and read 4039_C028h (bit 0) to confirm whether the HSE was successful.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;However, I read out 0x000001C0 (bit 0 is 0, HSE Unsuccessful).&lt;/P&gt;&lt;P&gt;What other registers can I read to confirm whether the HSE was successful?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 04 Nov 2025 05:51:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K342-HSE/m-p/2197997#M54086</guid>
      <dc:creator>gary_yang</dc:creator>
      <dc:date>2025-11-04T05:51:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32K342 HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K342-HSE/m-p/2198288#M54117</link>
      <description>&lt;P&gt;Have you installed on virgin device or there were already some attempts to have installed FW before?&lt;BR /&gt;Could you provide following information?&lt;BR /&gt;SBAF version:&lt;BR /&gt;HSE FW version:&lt;BR /&gt;MU registers, FSR, GSR, etc:&lt;BR /&gt;HSE GPR3:&lt;BR /&gt;Is the "HSE_STATUS_INIT_OK" have been wait set to "1"?&lt;/P&gt;
&lt;P&gt;In case AB SWAP, multiple resets may be required.&lt;/P&gt;
&lt;P&gt;Recently I have discussed installation procedure over following thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K3-HSE-Installation-differences-between-FULL-MEM-and-AB-SWAP/m-p/2190106/emcs_t/S2h8ZW1haWx8YW5zd2VyX2FjY2VwdGVkX2FzX3NvbHV0aW9ufE1ISkNBVTZXSFlVWEI1fDIxOTAxMDZ8QUNDRVBURURfU09MVVRJT05TfGhL#M53730" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K3-HSE-Installation-differences-between-FULL-MEM-and-AB-SWAP/m-p/2190106/emcs_t/S2h8ZW1haWx8YW5zd2VyX2FjY2VwdGVkX2FzX3NvbHV0aW9ufE1ISkNBVTZXSFlVWEI1fDIxOTAxMDZ8QUNDRVBURURfU09MVVRJT05TfGhL#M53730&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps&lt;/P&gt;</description>
      <pubDate>Tue, 04 Nov 2025 11:12:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K342-HSE/m-p/2198288#M54117</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2025-11-04T11:12:37Z</dc:date>
    </item>
  </channel>
</rss>