<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Wake the MCU from VLPS using a GPIO pin</title>
    <link>https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPS-using-a-GPIO-pin/m-p/2195849#M53997</link>
    <description>No, I don't want MCAL. I use Freescale Semiconductor libraries.&lt;BR /&gt;If there are ready-made functions instead of writing directly to registers, that would be better.</description>
    <pubDate>Thu, 30 Oct 2025 13:09:30 GMT</pubDate>
    <dc:creator>adem_marangoz</dc:creator>
    <dc:date>2025-10-30T13:09:30Z</dc:date>
    <item>
      <title>Wake the MCU from VLPS using a GPIO pin</title>
      <link>https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPS-using-a-GPIO-pin/m-p/2195572#M53979</link>
      <description>&lt;P&gt;Hello NXP team.&lt;/P&gt;&lt;P&gt;I am using the S32K144 microcontroller.&lt;/P&gt;&lt;P&gt;I want to wake up the MCU from VPLS using GPIO.&lt;/P&gt;&lt;P&gt;Do you have a ready example using RTD?&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="S32K144EVB" id="S32K144EVB"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 30 Oct 2025 07:29:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPS-using-a-GPIO-pin/m-p/2195572#M53979</guid>
      <dc:creator>adem_marangoz</dc:creator>
      <dc:date>2025-10-30T07:29:25Z</dc:date>
    </item>
    <item>
      <title>Re: Wake the MCU from VLPS using a GPIO pin</title>
      <link>https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPS-using-a-GPIO-pin/m-p/2195847#M53996</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249464"&gt;@adem_marangoz&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Let me check.&lt;/P&gt;
&lt;P&gt;Do you need MCAL or IP example?&lt;/P&gt;</description>
      <pubDate>Thu, 30 Oct 2025 13:04:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPS-using-a-GPIO-pin/m-p/2195847#M53996</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-10-30T13:04:07Z</dc:date>
    </item>
    <item>
      <title>Re: Wake the MCU from VLPS using a GPIO pin</title>
      <link>https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPS-using-a-GPIO-pin/m-p/2195849#M53997</link>
      <description>No, I don't want MCAL. I use Freescale Semiconductor libraries.&lt;BR /&gt;If there are ready-made functions instead of writing directly to registers, that would be better.</description>
      <pubDate>Thu, 30 Oct 2025 13:09:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPS-using-a-GPIO-pin/m-p/2195849#M53997</guid>
      <dc:creator>adem_marangoz</dc:creator>
      <dc:date>2025-10-30T13:09:30Z</dc:date>
    </item>
    <item>
      <title>Re: Wake the MCU from VLPS using a GPIO pin</title>
      <link>https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPS-using-a-GPIO-pin/m-p/2195861#M53998</link>
      <description>&lt;P&gt;What do you mean by the&amp;nbsp;Freescale Semiconductor libraries?&lt;/P&gt;
&lt;P&gt;The S32K1xx RTD has&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;MCAL MCU driver that manages the power modes and&lt;/LI&gt;
&lt;LI&gt;low-level Power_Ip driver.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Does it mean you need an example with the&amp;nbsp;Ip drivers?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 30 Oct 2025 13:27:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPS-using-a-GPIO-pin/m-p/2195861#M53998</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-10-30T13:27:11Z</dc:date>
    </item>
    <item>
      <title>Re: Wake the MCU from VLPS using a GPIO pin</title>
      <link>https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPS-using-a-GPIO-pin/m-p/2196378#M54022</link>
      <description>low-level Power_Ip driver.</description>
      <pubDate>Fri, 31 Oct 2025 05:52:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPS-using-a-GPIO-pin/m-p/2196378#M54022</guid>
      <dc:creator>adem_marangoz</dc:creator>
      <dc:date>2025-10-31T05:52:15Z</dc:date>
    </item>
    <item>
      <title>Re: Wake the MCU from VLPS using a GPIO pin</title>
      <link>https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPS-using-a-GPIO-pin/m-p/2198364#M54124</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249464"&gt;@adem_marangoz&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;In your other community thread, you mentioned using the legacy SDK v3.0.0:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPR-using-a-GPIO-pin/m-p/2198256#M54116" target="_blank"&gt;https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPR-using-a-GPIO-pin/m-p/2198256#M54116&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;This SDK includes a default example that demonstrates low-power modes, including VLPS.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 04 Nov 2025 13:52:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPS-using-a-GPIO-pin/m-p/2198364#M54124</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-11-04T13:52:30Z</dc:date>
    </item>
  </channel>
</rss>