<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32k388 ethercat config in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32k388-ethercat-config/m-p/2195366#M53963</link>
    <description>&lt;P&gt;Thank you Sir, so i cannot use above design for s32k388 work as ethercat master to control ethercat motor ..?&lt;/P&gt;</description>
    <pubDate>Thu, 30 Oct 2025 01:48:15 GMT</pubDate>
    <dc:creator>vinmotion</dc:creator>
    <dc:date>2025-10-30T01:48:15Z</dc:date>
    <item>
      <title>S32k388 ethercat config</title>
      <link>https://community.nxp.com/t5/S32K/S32k388-ethercat-config/m-p/2193972#M53893</link>
      <description>&lt;P&gt;Hello engineers, im new to nxp and ethercat. I wonder if anyone has experience using ethercat with nxp ; how should i config the project or pin to use ethercat with KSZ9131...&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="nxpETHERCAT.png" style="width: 536px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/362814i049BB04BA0E3E7FD/image-size/large?v=v2&amp;amp;px=999" role="button" title="nxpETHERCAT.png" alt="nxpETHERCAT.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Oct 2025 05:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k388-ethercat-config/m-p/2193972#M53893</guid>
      <dc:creator>vinmotion</dc:creator>
      <dc:date>2025-10-28T05:29:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32k388 ethercat config</title>
      <link>https://community.nxp.com/t5/S32K/S32k388-ethercat-config/m-p/2194958#M53936</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254753"&gt;@vinmotion&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;It seems that S32K388 might not be the best choice for EtherCAT, because EtherCAT typically requires a dedicated EtherCAT Slave Controller (ESC)&amp;nbsp;- this is a hardware block that handles on-the-fly frame processing and distributed clocks. S32K388 does not have an integrated ESC, so implementing EtherCAT would require an external controller or a software stack with strict timing constraints.&lt;/P&gt;
&lt;P&gt;EtherCAT is generally a domain of the i.MX family, and NXP provides solutions with integrated ESC. For example, the &lt;STRONG&gt;i.MX RT1180&lt;/STRONG&gt; includes a built-in EtherCAT two-port slave controller, making it much easier to implement EtherCAT without additional hardware.&lt;/P&gt;
&lt;P&gt;Please check this application note related to i.MX RT1180 and EtherCAT:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN14155.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN14155.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 29 Oct 2025 08:32:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k388-ethercat-config/m-p/2194958#M53936</guid>
      <dc:creator>PavelL</dc:creator>
      <dc:date>2025-10-29T08:32:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32k388 ethercat config</title>
      <link>https://community.nxp.com/t5/S32K/S32k388-ethercat-config/m-p/2195366#M53963</link>
      <description>&lt;P&gt;Thank you Sir, so i cannot use above design for s32k388 work as ethercat master to control ethercat motor ..?&lt;/P&gt;</description>
      <pubDate>Thu, 30 Oct 2025 01:48:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k388-ethercat-config/m-p/2195366#M53963</guid>
      <dc:creator>vinmotion</dc:creator>
      <dc:date>2025-10-30T01:48:15Z</dc:date>
    </item>
    <item>
      <title>Re: S32k388 ethercat config</title>
      <link>https://community.nxp.com/t5/S32K/S32k388-ethercat-config/m-p/2195570#M53978</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254753"&gt;@vinmotion&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I reviewed EtherCAT once again, and even though &lt;STRONG&gt;S32K388 does not have integrated EtherCAT Slave Controller (ESC)&lt;/STRONG&gt;, it features &lt;STRONG&gt;two GMAC interfaces with TSN/AVB support&lt;/STRONG&gt; and sufficient processing power to run an EtherCAT software stack.&lt;/P&gt;
&lt;P&gt;Please verify &lt;STRONG&gt;S32K388 &amp;amp; EtherCAT compatibility&lt;/STRONG&gt; with your EtherCAT stack provider to ensure proper integration and timing requirements.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 30 Oct 2025 07:27:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k388-ethercat-config/m-p/2195570#M53978</guid>
      <dc:creator>PavelL</dc:creator>
      <dc:date>2025-10-30T07:27:42Z</dc:date>
    </item>
  </channel>
</rss>