<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K358 CAN Example Configuration in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K358-CAN-Example-Configuration/m-p/2194853#M53928</link>
    <description>&lt;P&gt;I am checking CAN transceiver configuration and init sequence for&amp;nbsp; "Can_Example_S32K358". But, I could not find anything related to this. Also, there is no Dio module configured in the MCAL driver. Then how does the CAN transceiver functions with this example ? I am using RTD "SW32K3_S32M27x_RTD_R21-11_6.0.0_QLP04_HF01_D2510_DesignStudio_updatesite".&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="prabtani_0-1761721269735.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/363019i220510C81E94C17B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="prabtani_0-1761721269735.png" alt="prabtani_0-1761721269735.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;prabtani_0-1761721269735.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 29 Oct 2025 07:01:41 GMT</pubDate>
    <dc:creator>prabtani</dc:creator>
    <dc:date>2025-10-29T07:01:41Z</dc:date>
    <item>
      <title>S32K358 CAN Example Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K358-CAN-Example-Configuration/m-p/2194853#M53928</link>
      <description>&lt;P&gt;I am checking CAN transceiver configuration and init sequence for&amp;nbsp; "Can_Example_S32K358". But, I could not find anything related to this. Also, there is no Dio module configured in the MCAL driver. Then how does the CAN transceiver functions with this example ? I am using RTD "SW32K3_S32M27x_RTD_R21-11_6.0.0_QLP04_HF01_D2510_DesignStudio_updatesite".&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="prabtani_0-1761721269735.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/363019i220510C81E94C17B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="prabtani_0-1761721269735.png" alt="prabtani_0-1761721269735.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;prabtani_0-1761721269735.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Oct 2025 07:01:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K358-CAN-Example-Configuration/m-p/2194853#M53928</guid>
      <dc:creator>prabtani</dc:creator>
      <dc:date>2025-10-29T07:01:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K358 CAN Example Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K358-CAN-Example-Configuration/m-p/2195079#M53945</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;RTD demo CAN examples shows internal loopback usage/config, so there is no need of pin init. You will need to add it by own. Also with TJA1153 initialization, if this is still in default Vanilla state.&lt;BR /&gt;You can refer to below examples&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/RTD600-MCAL-amp-IP-S32K3X4EVB-T172-FlexCAN-Example-Interrupt/ta-p/2142069" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/RTD600-MCAL-amp-IP-S32K3X4EVB-T172-FlexCAN-Example-Interrupt/ta-p/2142069&lt;/A&gt;&amp;nbsp;It is for S32K344, but can be used as reference.&amp;nbsp;&lt;BR /&gt;The S32K358 FlexCAN IP example is e.g on&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K358-FlexCAN-TXRX-ISR-S32DS35-RTD400-500/ta-p/1981987" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K358-FlexCAN-TXRX-ISR-S32DS35-RTD400-500/ta-p/1981987&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 29 Oct 2025 11:26:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K358-CAN-Example-Configuration/m-p/2195079#M53945</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-10-29T11:26:28Z</dc:date>
    </item>
  </channel>
</rss>