<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Command-Line RTD Code Generation for S32K3xx</title>
    <link>https://community.nxp.com/t5/S32K/Command-Line-RTD-Code-Generation-for-S32K3xx/m-p/2193335#M53864</link>
    <description>&lt;P&gt;Hello NXP Community,&lt;BR /&gt;We are developing a project with S32K3xx MCUs using S32 Design Studio. Our workflow uses RTD to configure clocks and peripherals, which generates a large amount of auto-generated code. Our project has ~400 files, and we want to avoid committing these generated files.&lt;BR /&gt;Goal:&lt;BR /&gt;Automate RTD code generation from .mex and clock files via command line in Linux, instead of manually using the IDE. We also want to integrate this into our existing Makefile.&lt;/P&gt;&lt;P&gt;Request:&lt;BR /&gt;Any guidance or examples for:&lt;BR /&gt;* Running Auto generation of code from command line&lt;BR /&gt;* Integrating it with Makefile&lt;BR /&gt;* Best practices for managing auto-generated code&lt;BR /&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="S32K3" id="S32K3"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 27 Oct 2025 08:35:35 GMT</pubDate>
    <dc:creator>leo_Z</dc:creator>
    <dc:date>2025-10-27T08:35:35Z</dc:date>
    <item>
      <title>Command-Line RTD Code Generation for S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/Command-Line-RTD-Code-Generation-for-S32K3xx/m-p/2193335#M53864</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;BR /&gt;We are developing a project with S32K3xx MCUs using S32 Design Studio. Our workflow uses RTD to configure clocks and peripherals, which generates a large amount of auto-generated code. Our project has ~400 files, and we want to avoid committing these generated files.&lt;BR /&gt;Goal:&lt;BR /&gt;Automate RTD code generation from .mex and clock files via command line in Linux, instead of manually using the IDE. We also want to integrate this into our existing Makefile.&lt;/P&gt;&lt;P&gt;Request:&lt;BR /&gt;Any guidance or examples for:&lt;BR /&gt;* Running Auto generation of code from command line&lt;BR /&gt;* Integrating it with Makefile&lt;BR /&gt;* Best practices for managing auto-generated code&lt;BR /&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="S32K3" id="S32K3"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Oct 2025 08:35:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Command-Line-RTD-Code-Generation-for-S32K3xx/m-p/2193335#M53864</guid>
      <dc:creator>leo_Z</dc:creator>
      <dc:date>2025-10-27T08:35:35Z</dc:date>
    </item>
    <item>
      <title>Re: Command-Line RTD Code Generation for S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/Command-Line-RTD-Code-Generation-for-S32K3xx/m-p/2194564#M53913</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252204"&gt;@leo_Z&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For more information related to the S32 Design Studio Command Line Interface, please refer to the following PDF document:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;C:\NXP\S32DS.3.6.2\S32DS\help\resources\howto\HOWTO_S32_Design_Studio_Command_Line_Interface.pdf&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;Please note that the path may vary depending on the version of the IDE and your installation directory.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 28 Oct 2025 21:10:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Command-Line-RTD-Code-Generation-for-S32K3xx/m-p/2194564#M53913</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2025-10-28T21:10:05Z</dc:date>
    </item>
  </channel>
</rss>