<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SDK Attachment Issue in S32K</title>
    <link>https://community.nxp.com/t5/S32K/SDK-Attachment-Issue/m-p/2193304#M53858</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;1. I don't recommend installing an older version like "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.zip."&lt;BR /&gt;2. Is there any special reason for needing such an old RTD version? Otherwise, I recommend installing the latest version, "SW32K3_S32M27x_RTD_R21-11_6.0.0_D2506_DesignStudio_updatesite.zip."&lt;BR /&gt;3. Go to File -&amp;gt; New -&amp;gt; S32DS Application Project, select S32K358, and then click ... to choose the SDKs. I recommend selecting it at that time.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Mon, 27 Oct 2025 08:01:40 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2025-10-27T08:01:40Z</dc:date>
    <item>
      <title>SDK Attachment Issue</title>
      <link>https://community.nxp.com/t5/S32K/SDK-Attachment-Issue/m-p/2193228#M53856</link>
      <description>&lt;P&gt;I am trying to create an example application project for LED blinking for S32K358. When creating a project, I am not able to attach the SDK and it shows the error that "SDK cannot be attached as it does not support the toolchain required by the project".&lt;/P&gt;&lt;P&gt;I have installed S32DS 3.6.4. Have installed SDK "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.zip"&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Error_1.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/362621i69E52F60786DD51C/image-size/large?v=v2&amp;amp;px=999" role="button" title="Error_1.png" alt="Error_1.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Error_1.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Oct 2025 06:53:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SDK-Attachment-Issue/m-p/2193228#M53856</guid>
      <dc:creator>prabtani</dc:creator>
      <dc:date>2025-10-27T06:53:36Z</dc:date>
    </item>
    <item>
      <title>Re: SDK Attachment Issue</title>
      <link>https://community.nxp.com/t5/S32K/SDK-Attachment-Issue/m-p/2193304#M53858</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;1. I don't recommend installing an older version like "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.zip."&lt;BR /&gt;2. Is there any special reason for needing such an old RTD version? Otherwise, I recommend installing the latest version, "SW32K3_S32M27x_RTD_R21-11_6.0.0_D2506_DesignStudio_updatesite.zip."&lt;BR /&gt;3. Go to File -&amp;gt; New -&amp;gt; S32DS Application Project, select S32K358, and then click ... to choose the SDKs. I recommend selecting it at that time.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 27 Oct 2025 08:01:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SDK-Attachment-Issue/m-p/2193304#M53858</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-10-27T08:01:40Z</dc:date>
    </item>
    <item>
      <title>Re: SDK Attachment Issue</title>
      <link>https://community.nxp.com/t5/S32K/SDK-Attachment-Issue/m-p/2193310#M53859</link>
      <description>&lt;P&gt;Hello Robin,&lt;/P&gt;&lt;P&gt;Thank you for your response. Could you please send the link to the latest RTD that will be supported with 3.6.4 S32DS IDE.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also in your step 3, I do not see any SDK to attach. It shows empty list.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Oct 2025 08:05:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SDK-Attachment-Issue/m-p/2193310#M53859</guid>
      <dc:creator>prabtani</dc:creator>
      <dc:date>2025-10-27T08:05:31Z</dc:date>
    </item>
    <item>
      <title>Re: SDK Attachment Issue</title>
      <link>https://community.nxp.com/t5/S32K/SDK-Attachment-Issue/m-p/2193315#M53860</link>
      <description>&lt;P&gt;Click&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=SW32K3-STDSW-D" target="_self"&gt;S32K3 Standard Software&lt;/A&gt; -&amp;gt; Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M -&amp;gt;&amp;nbsp;S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0&lt;BR /&gt;By the way, the latest S32K3 RTD 6.0.0 was tested in S32 Design Studio &lt;STRONG&gt;3.6.1&lt;/STRONG&gt;. I have not tried to install S32K3 RTD 6.0.0 in S32DSv3.6.4.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Oct 2025 08:12:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SDK-Attachment-Issue/m-p/2193315#M53860</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-10-27T08:12:43Z</dc:date>
    </item>
  </channel>
</rss>