<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: OSDA D14 LED goes RED in S32K</title>
    <link>https://community.nxp.com/t5/S32K/OSDA-D14-LED-goes-RED/m-p/2189729#M53707</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;If you don't pull &lt;STRONG&gt;FS23_CSB/SDA&lt;/STRONG&gt; PTB0 low, the FS23 shouldn't be misconfigured via SPI commands.&lt;BR /&gt;If possible, please take a photo of the S32K31XEVB-Q100 so I can clearly see the jumper settings and which LEDs are lit.&lt;BR /&gt;Regarding the 0V output from the PMIC, are you referring to &lt;STRONG&gt;FS23_HBUCK_V1&lt;/STRONG&gt; (FS23_V1), &lt;STRONG&gt;FS23_LVDO_V2&lt;/STRONG&gt; (FS23_V2), or &lt;STRONG&gt;FS23_LVDO_V3&lt;/STRONG&gt; (FS23_V3)?&lt;BR /&gt;If I disconnect &lt;STRONG&gt;J26&lt;/STRONG&gt;, does the voltage output of &lt;STRONG&gt;FS23_HBUCK_V1&lt;/STRONG&gt; or &lt;STRONG&gt;FS23_LVDO_V2&lt;/STRONG&gt; return to normal?&amp;nbsp;If this is the case, there may be a short circuit on the board, and the FS23 should be heating up.&lt;/P&gt;
&lt;P&gt;If &lt;STRONG&gt;SDA_RST_TGTMCU&lt;/STRONG&gt; is low, &lt;STRONG&gt;D14&lt;/STRONG&gt; will light up &lt;STRONG&gt;&lt;FONT color="#FF0000"&gt;red&lt;/FONT&gt;&lt;/STRONG&gt;, which means that &lt;STRONG&gt;RESET_MCU&lt;/STRONG&gt; is low and the S32K311 is in reset state. If &lt;STRONG&gt;J1&lt;/STRONG&gt; connects&amp;nbsp;&lt;STRONG&gt;RESET_MCU&lt;/STRONG&gt; and &lt;STRONG&gt;FS23_RSTB&lt;/STRONG&gt;, you need to disconnect &lt;STRONG&gt;J1&lt;/STRONG&gt; to check whether the low level comes from FS23's &lt;STRONG&gt;RSTB&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Tue, 21 Oct 2025 07:42:25 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2025-10-21T07:42:25Z</dc:date>
    <item>
      <title>OSDA D14 LED goes RED</title>
      <link>https://community.nxp.com/t5/S32K/OSDA-D14-LED-goes-RED/m-p/2189190#M53685</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear NXP Support Team,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have configured two LPSPI for my SPI data transfer protocol code using S32 design studio.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But during my configuration I have disturbed the pre-configured FS23 SPI which is PTC9 and PTB1 in S32k11 nxp controller. While testing this Software I have encountered a different problem like OSDA D14 pin goes RED it is confirmed that the output from the PMIC is 0V.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Now my question is this RED LED is due to my configuration or any other possibilities to go RED. I need clarification on this.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;also need list of which the OSDA D14 can go RED&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Santhosh P&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Oct 2025 12:17:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/OSDA-D14-LED-goes-RED/m-p/2189190#M53685</guid>
      <dc:creator>SanthoshP</dc:creator>
      <dc:date>2025-10-20T12:17:07Z</dc:date>
    </item>
    <item>
      <title>Re: OSDA D14 LED goes RED</title>
      <link>https://community.nxp.com/t5/S32K/OSDA-D14-LED-goes-RED/m-p/2189729#M53707</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;If you don't pull &lt;STRONG&gt;FS23_CSB/SDA&lt;/STRONG&gt; PTB0 low, the FS23 shouldn't be misconfigured via SPI commands.&lt;BR /&gt;If possible, please take a photo of the S32K31XEVB-Q100 so I can clearly see the jumper settings and which LEDs are lit.&lt;BR /&gt;Regarding the 0V output from the PMIC, are you referring to &lt;STRONG&gt;FS23_HBUCK_V1&lt;/STRONG&gt; (FS23_V1), &lt;STRONG&gt;FS23_LVDO_V2&lt;/STRONG&gt; (FS23_V2), or &lt;STRONG&gt;FS23_LVDO_V3&lt;/STRONG&gt; (FS23_V3)?&lt;BR /&gt;If I disconnect &lt;STRONG&gt;J26&lt;/STRONG&gt;, does the voltage output of &lt;STRONG&gt;FS23_HBUCK_V1&lt;/STRONG&gt; or &lt;STRONG&gt;FS23_LVDO_V2&lt;/STRONG&gt; return to normal?&amp;nbsp;If this is the case, there may be a short circuit on the board, and the FS23 should be heating up.&lt;/P&gt;
&lt;P&gt;If &lt;STRONG&gt;SDA_RST_TGTMCU&lt;/STRONG&gt; is low, &lt;STRONG&gt;D14&lt;/STRONG&gt; will light up &lt;STRONG&gt;&lt;FONT color="#FF0000"&gt;red&lt;/FONT&gt;&lt;/STRONG&gt;, which means that &lt;STRONG&gt;RESET_MCU&lt;/STRONG&gt; is low and the S32K311 is in reset state. If &lt;STRONG&gt;J1&lt;/STRONG&gt; connects&amp;nbsp;&lt;STRONG&gt;RESET_MCU&lt;/STRONG&gt; and &lt;STRONG&gt;FS23_RSTB&lt;/STRONG&gt;, you need to disconnect &lt;STRONG&gt;J1&lt;/STRONG&gt; to check whether the low level comes from FS23's &lt;STRONG&gt;RSTB&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 21 Oct 2025 07:42:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/OSDA-D14-LED-goes-RED/m-p/2189729#M53707</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-10-21T07:42:25Z</dc:date>
    </item>
  </channel>
</rss>