<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Real Time Clock enable problem</title>
    <link>https://community.nxp.com/t5/S32K/Real-Time-Clock-enable-problem/m-p/2189375#M53696</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242600"&gt;@minjaekang99&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;To quote my colleague from another community post (&lt;A href="https://community.nxp.com/t5/S32K/S32K3X4EVB-Q172-32768Hz-clock/td-p/2121175" target="_blank"&gt;Solved: S32K3X4EVB-Q172 32768Hz clock&lt;/A&gt;&lt;LI-EMOJI id="lia_disappointed-face" title=":disappointed_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;There is no 32.768 kHz crystal included on the S32K3x4EVB-Q172 or the S32K3X4EVB-T172 evaluation boards; although the crystal is present on boards such as the S32K344-WB, S32K3-T-BOX, S32K3X8EVB-Q289 and S32K388EVB-Q289 -&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;DNP resistors must be soldered on the&amp;nbsp;latter&amp;nbsp;to connect the crystal to the chip."&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can use the external oscillator from these other boards as reference. For recommendations, you can look at the BOM.xlsx file included in the design files.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 20 Oct 2025 19:54:55 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2025-10-20T19:54:55Z</dc:date>
    <item>
      <title>Real Time Clock enable problem</title>
      <link>https://community.nxp.com/t5/S32K/Real-Time-Clock-enable-problem/m-p/2189048#M53673</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I’m currently using the &lt;STRONG&gt;S32K324 EVB board&lt;/STRONG&gt;, and I’m trying to use the &lt;STRONG&gt;RTC&lt;/STRONG&gt; module.&lt;/P&gt;&lt;P&gt;When I configure the RTC to use &lt;STRONG&gt;SXOSC (32.768 kHz external crystal oscillator)&lt;/STRONG&gt; as the clock source,&lt;BR /&gt;the SXOSC_STAT register remains 0x00000000 — it never shows the “ready” status.&lt;/P&gt;&lt;P&gt;So I’d like to confirm the following:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;STRONG&gt;Do I need to purchase and solder an external 32.768 kHz crystal on the EVB to use SXOSC,&lt;BR /&gt;or is it already available on the board and just needs to be enabled in software (MC_ME / Clock_Ip)?&lt;/STRONG&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Currently, it seems that no crystal is mounted at the &lt;STRONG&gt;Y1&lt;/STRONG&gt; position on my EVB.&lt;BR /&gt;If the external component is required, could you please let me know the recommended crystal specifications&lt;BR /&gt;(frequency, load capacitance, package size, etc.) for the S32K324?&lt;/P&gt;&lt;P&gt;Thank you very much for your support.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Oct 2025 08:30:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Real-Time-Clock-enable-problem/m-p/2189048#M53673</guid>
      <dc:creator>minjaekang99</dc:creator>
      <dc:date>2025-10-20T08:30:18Z</dc:date>
    </item>
    <item>
      <title>Re: Real Time Clock enable problem</title>
      <link>https://community.nxp.com/t5/S32K/Real-Time-Clock-enable-problem/m-p/2189375#M53696</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242600"&gt;@minjaekang99&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;To quote my colleague from another community post (&lt;A href="https://community.nxp.com/t5/S32K/S32K3X4EVB-Q172-32768Hz-clock/td-p/2121175" target="_blank"&gt;Solved: S32K3X4EVB-Q172 32768Hz clock&lt;/A&gt;&lt;LI-EMOJI id="lia_disappointed-face" title=":disappointed_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;There is no 32.768 kHz crystal included on the S32K3x4EVB-Q172 or the S32K3X4EVB-T172 evaluation boards; although the crystal is present on boards such as the S32K344-WB, S32K3-T-BOX, S32K3X8EVB-Q289 and S32K388EVB-Q289 -&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;DNP resistors must be soldered on the&amp;nbsp;latter&amp;nbsp;to connect the crystal to the chip."&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can use the external oscillator from these other boards as reference. For recommendations, you can look at the BOM.xlsx file included in the design files.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Oct 2025 19:54:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Real-Time-Clock-enable-problem/m-p/2189375#M53696</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-10-20T19:54:55Z</dc:date>
    </item>
  </channel>
</rss>