<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K144 - flexio_i2c (i2c) does not work as expected when compiler optimization level set at -O0</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-flexio-i2c-i2c-does-not-work-as-expected-when-compiler/m-p/960235#M5363</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to use I2C with the S32K144 EVB. I decided to start&amp;nbsp;with the flexio_i2c_s32k144 SDK example project from the&amp;nbsp;S32SDK_S32K1xx_RTM_3.0.0.&lt;/P&gt;&lt;P&gt;After facing several issues, and debugging the project, I have found the following:&lt;/P&gt;&lt;P&gt;When compiling the&amp;nbsp;&lt;SPAN&gt;flexio_i2c_s32k144 SDK example project using the&amp;nbsp;S32 Design Studio, and setting the C Compiler and Assembler Optimization level to -O0, the project is not working properly.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;After the&amp;nbsp;FLEXIO_I2C_DRV_MasterSendDataBlocking() is called, the&amp;nbsp;i2cMasterState flexio_i2c_master_state_t.status is&amp;nbsp;STATUS_I2C_TX_UNDERRUN,&amp;nbsp;lpi2cSlaveState lpi2c_slave_state_t.status is&amp;nbsp;&lt;SPAN&gt;STATUS_SUCCESS&lt;/SPAN&gt;&amp;nbsp;but&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;the&amp;nbsp;slave buffer is filled&amp;nbsp;up with incorrect values.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Then when the&amp;nbsp;FLEXIO_I2C_DRV_MasterReceiveDataBlocking() is called, the&amp;nbsp;lpi2cSlaveState lpi2c_slave_state_t.status is&amp;nbsp;STATUS_BUSY, the&amp;nbsp; i2cMasterState flexio_i2c_master_state_t.status&amp;nbsp; is&amp;nbsp;STATUS_I2C_RECEIVED_NACK, and the master buffer is filled up again with incorrect values.&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When I set up the optimization level to -O1, the project works correctly as expected.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Per my project requirements, I should set the optimization level to -O0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I verified the code size, and I can confirm that the code is not large enough to not fit the flash memory. Here are the results for the .elf file generated after running the&amp;nbsp;arm-none-eabi-size utility tool with and without compiler optimization. It can be seen that the .text section without optimization is&amp;nbsp;0x96ac, which is fairly smaller than the available size of 512KB defined in the linker file as:&amp;nbsp;0x0007FBF0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;******************************WITHOUT OPTIMIZATION (-O0)********************************&lt;/P&gt;&lt;P&gt;$ ./arm-none-eabi-size.exe --format=SysV -x /c/Users/rcortes/workspaceS32DS.ARM.2018.R1/flexio_i2c_s32k144/flexio_i2c_s32k144/Debug_FLASH/flexio_i2c_s32k144.elf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;section size addr&lt;BR /&gt;.interrupts 0x400 0x0&lt;BR /&gt;.flash_config 0x10 0x400&lt;BR /&gt;.text 0x96ac 0x410&lt;BR /&gt;.interrupts_ram 0x400 0x1fff8000&lt;BR /&gt;.data 0x1e4 0x1fff8400&lt;BR /&gt;.code 0x0 0x1fff85e4&lt;BR /&gt;.bss 0x54 0x20000000&lt;BR /&gt;.heap 0x404 0x20000054&lt;BR /&gt;.stack 0x400 0x20006c00&lt;BR /&gt;.ARM.attributes 0x30 0x0&lt;BR /&gt;.debug_info 0x195b2 0x0&lt;BR /&gt;.debug_abbrev 0x2374 0x0&lt;BR /&gt;.debug_aranges 0x1288 0x0&lt;BR /&gt;.debug_ranges 0x1108 0x0&lt;BR /&gt;.debug_macro 0x20ebd 0x0&lt;BR /&gt;.debug_line 0xa1a4 0x0&lt;BR /&gt;.debug_str 0x73661 0x0&lt;BR /&gt;.comment 0xa0 0x0&lt;BR /&gt;.debug_frame 0x4ebc 0x0&lt;BR /&gt;Total 0xcbbfc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;******************************WITH OPTIMIZATION (-O1)********************************&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;$ ./arm-none-eabi-size.exe --format=SysV -x /c/Users/rcortes/workspaceS32DS.ARM.2018.R1/flexio_i2c_s32k144/flexio_i2c_s32k144/Debug_FLASH/flexio_i2c_s32k144.elf&lt;BR /&gt;&lt;BR /&gt;section size addr&lt;BR /&gt;.interrupts 0x400 0x0&lt;BR /&gt;.flash_config 0x10 0x400&lt;BR /&gt;.text 0x4044 0x410&lt;BR /&gt;.interrupts_ram 0x400 0x1fff8000&lt;BR /&gt;.data 0x1e4 0x1fff8400&lt;BR /&gt;.code 0x0 0x1fff85e4&lt;BR /&gt;.bss 0x54 0x20000000&lt;BR /&gt;.heap 0x404 0x20000054&lt;BR /&gt;.stack 0x400 0x20006c00&lt;BR /&gt;.ARM.attributes 0x30 0x0&lt;BR /&gt;.debug_info 0x22c1d 0x0&lt;BR /&gt;.debug_abbrev 0x2c50 0x0&lt;BR /&gt;.debug_loc 0x1177a 0x0&lt;BR /&gt;.debug_aranges 0x8f8 0x0&lt;BR /&gt;.debug_ranges 0xdf8 0x0&lt;BR /&gt;.debug_macro 0x20ebd 0x0&lt;BR /&gt;.debug_line 0x9b90 0x0&lt;BR /&gt;.debug_str 0x73660 0x0&lt;BR /&gt;.comment 0xa0 0x0&lt;BR /&gt;.debug_frame 0x1688 0x0&lt;BR /&gt;Total 0xdd16c&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks in advance for any inputs. I would expect the code to behave correctly regardless the compiler optimization level (specially if no optimization is selected)..&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Rodrigo&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jul 2019 21:45:26 GMT</pubDate>
    <dc:creator>rcortes</dc:creator>
    <dc:date>2019-07-23T21:45:26Z</dc:date>
    <item>
      <title>S32K144 - flexio_i2c (i2c) does not work as expected when compiler optimization level set at -O0</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-flexio-i2c-i2c-does-not-work-as-expected-when-compiler/m-p/960235#M5363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to use I2C with the S32K144 EVB. I decided to start&amp;nbsp;with the flexio_i2c_s32k144 SDK example project from the&amp;nbsp;S32SDK_S32K1xx_RTM_3.0.0.&lt;/P&gt;&lt;P&gt;After facing several issues, and debugging the project, I have found the following:&lt;/P&gt;&lt;P&gt;When compiling the&amp;nbsp;&lt;SPAN&gt;flexio_i2c_s32k144 SDK example project using the&amp;nbsp;S32 Design Studio, and setting the C Compiler and Assembler Optimization level to -O0, the project is not working properly.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;After the&amp;nbsp;FLEXIO_I2C_DRV_MasterSendDataBlocking() is called, the&amp;nbsp;i2cMasterState flexio_i2c_master_state_t.status is&amp;nbsp;STATUS_I2C_TX_UNDERRUN,&amp;nbsp;lpi2cSlaveState lpi2c_slave_state_t.status is&amp;nbsp;&lt;SPAN&gt;STATUS_SUCCESS&lt;/SPAN&gt;&amp;nbsp;but&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;the&amp;nbsp;slave buffer is filled&amp;nbsp;up with incorrect values.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Then when the&amp;nbsp;FLEXIO_I2C_DRV_MasterReceiveDataBlocking() is called, the&amp;nbsp;lpi2cSlaveState lpi2c_slave_state_t.status is&amp;nbsp;STATUS_BUSY, the&amp;nbsp; i2cMasterState flexio_i2c_master_state_t.status&amp;nbsp; is&amp;nbsp;STATUS_I2C_RECEIVED_NACK, and the master buffer is filled up again with incorrect values.&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When I set up the optimization level to -O1, the project works correctly as expected.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Per my project requirements, I should set the optimization level to -O0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I verified the code size, and I can confirm that the code is not large enough to not fit the flash memory. Here are the results for the .elf file generated after running the&amp;nbsp;arm-none-eabi-size utility tool with and without compiler optimization. It can be seen that the .text section without optimization is&amp;nbsp;0x96ac, which is fairly smaller than the available size of 512KB defined in the linker file as:&amp;nbsp;0x0007FBF0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;******************************WITHOUT OPTIMIZATION (-O0)********************************&lt;/P&gt;&lt;P&gt;$ ./arm-none-eabi-size.exe --format=SysV -x /c/Users/rcortes/workspaceS32DS.ARM.2018.R1/flexio_i2c_s32k144/flexio_i2c_s32k144/Debug_FLASH/flexio_i2c_s32k144.elf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;section size addr&lt;BR /&gt;.interrupts 0x400 0x0&lt;BR /&gt;.flash_config 0x10 0x400&lt;BR /&gt;.text 0x96ac 0x410&lt;BR /&gt;.interrupts_ram 0x400 0x1fff8000&lt;BR /&gt;.data 0x1e4 0x1fff8400&lt;BR /&gt;.code 0x0 0x1fff85e4&lt;BR /&gt;.bss 0x54 0x20000000&lt;BR /&gt;.heap 0x404 0x20000054&lt;BR /&gt;.stack 0x400 0x20006c00&lt;BR /&gt;.ARM.attributes 0x30 0x0&lt;BR /&gt;.debug_info 0x195b2 0x0&lt;BR /&gt;.debug_abbrev 0x2374 0x0&lt;BR /&gt;.debug_aranges 0x1288 0x0&lt;BR /&gt;.debug_ranges 0x1108 0x0&lt;BR /&gt;.debug_macro 0x20ebd 0x0&lt;BR /&gt;.debug_line 0xa1a4 0x0&lt;BR /&gt;.debug_str 0x73661 0x0&lt;BR /&gt;.comment 0xa0 0x0&lt;BR /&gt;.debug_frame 0x4ebc 0x0&lt;BR /&gt;Total 0xcbbfc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;******************************WITH OPTIMIZATION (-O1)********************************&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;$ ./arm-none-eabi-size.exe --format=SysV -x /c/Users/rcortes/workspaceS32DS.ARM.2018.R1/flexio_i2c_s32k144/flexio_i2c_s32k144/Debug_FLASH/flexio_i2c_s32k144.elf&lt;BR /&gt;&lt;BR /&gt;section size addr&lt;BR /&gt;.interrupts 0x400 0x0&lt;BR /&gt;.flash_config 0x10 0x400&lt;BR /&gt;.text 0x4044 0x410&lt;BR /&gt;.interrupts_ram 0x400 0x1fff8000&lt;BR /&gt;.data 0x1e4 0x1fff8400&lt;BR /&gt;.code 0x0 0x1fff85e4&lt;BR /&gt;.bss 0x54 0x20000000&lt;BR /&gt;.heap 0x404 0x20000054&lt;BR /&gt;.stack 0x400 0x20006c00&lt;BR /&gt;.ARM.attributes 0x30 0x0&lt;BR /&gt;.debug_info 0x22c1d 0x0&lt;BR /&gt;.debug_abbrev 0x2c50 0x0&lt;BR /&gt;.debug_loc 0x1177a 0x0&lt;BR /&gt;.debug_aranges 0x8f8 0x0&lt;BR /&gt;.debug_ranges 0xdf8 0x0&lt;BR /&gt;.debug_macro 0x20ebd 0x0&lt;BR /&gt;.debug_line 0x9b90 0x0&lt;BR /&gt;.debug_str 0x73660 0x0&lt;BR /&gt;.comment 0xa0 0x0&lt;BR /&gt;.debug_frame 0x1688 0x0&lt;BR /&gt;Total 0xdd16c&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks in advance for any inputs. I would expect the code to behave correctly regardless the compiler optimization level (specially if no optimization is selected)..&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Rodrigo&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 21:45:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-flexio-i2c-i2c-does-not-work-as-expected-when-compiler/m-p/960235#M5363</guid>
      <dc:creator>rcortes</dc:creator>
      <dc:date>2019-07-23T21:45:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 - flexio_i2c (i2c) does not work as expected when compiler optimization level set at -O0</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-flexio-i2c-i2c-does-not-work-as-expected-when-compiler/m-p/960236#M5364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rodrigo, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the late reply. I made some tests and I was able to reproduce the behavior you mentioned. I will make more tests on my side to figure out what is causing this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jul 2019 23:00:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-flexio-i2c-i2c-does-not-work-as-expected-when-compiler/m-p/960236#M5364</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2019-07-30T23:00:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 - flexio_i2c (i2c) does not work as expected when compiler optimization level set at -O0</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-flexio-i2c-i2c-does-not-work-as-expected-when-compiler/m-p/960237#M5365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rodrigo, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the S32 SDK Release Notes Version 3.0.0 pdf, you will find the following information about the FlexIO_I2C example.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/81933i34A42356939129F5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When you turned off the optimizations you are making less effective the functions to receive and send information. Without the capability to do clock stretching, you are seeing that Tx underflows and Rx overflows occur. The correct way to avoid this to happen is to low the baudrate of the flexio_i2c_master. By default, the baudrate is 400000, if you modify this value for 40000, the project will work correctly even without optimizations because no clock stretching would be needed. You can make this modification with the help of Processor Expert.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/82026i3AEA86265445DA4F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jul 2019 16:57:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-flexio-i2c-i2c-does-not-work-as-expected-when-compiler/m-p/960237#M5365</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2019-07-31T16:57:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 - flexio_i2c (i2c) does not work as expected when compiler optimization level set at -O0</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-flexio-i2c-i2c-does-not-work-as-expected-when-compiler/m-p/960238#M5366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Victor for your help. Effectively, without optimization the project works with a smaller baud rate. I will have this in consideration for future developments.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jul 2019 17:19:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-flexio-i2c-i2c-does-not-work-as-expected-when-compiler/m-p/960238#M5366</guid>
      <dc:creator>rcortes</dc:creator>
      <dc:date>2019-07-31T17:19:20Z</dc:date>
    </item>
  </channel>
</rss>