<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: What makes the MCU ASIL compliant?</title>
    <link>https://community.nxp.com/t5/S32K/What-makes-the-MCU-ASIL-compliant/m-p/960209#M5362</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, ASIL certification is being above whole ECU/system level, so customer could develop ASIL-x compliant appliance with other devices, but such approach could be in-efficient, slow, expensive, complicated, and so on…&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Functional safety and the ISO26262 standard define the general guidelines needed to fulfill the requirements for the different ASIL levels. In NXP we have a program called safe assure. For more information about this program and the devices see following link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/product-information/functional-safety-for-iso-26262-and-iec-61508:FNCTNLSFTY"&gt;https://www.nxp.com/products/product-information/functional-safety-for-iso-26262-and-iec-61508:FNCTNLSFTY&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;“The SafeAssure program highlights selected solutions - including hardware and software - that are targeted for use in functional safety applications, enabling system designers to design with confidence and achieve their system-level design goals and standards compliance more efficiently.”&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The S32 kit itself certainly is not ASIL compliant, it is just evaluation board. I am not aware we had an evaluation board being ASIL compliant as a whole.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The MCU itself is developed according safety standard:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/supporting-information/ISO-26262.pdf"&gt;https://www.nxp.com/docs/en/supporting-information/ISO-26262.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regarding SW, NXP or NXP partners can offers certain software (safety MCAL for instance).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Finally there are additional documents and tools, we says “safety support”. It is mainly safety manual, FMEDA and others. Details you may find here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/product-information/functional-safety-for-iso-26262-and-iec-61508:FNCTNLSFTY"&gt;https://www.nxp.com/products/product-information/functional-safety-for-iso-26262-and-iec-61508:FNCTNLSFTY&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;That’s what makes MCU ASIL compliant.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Oct 2019 14:43:45 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2019-10-09T14:43:45Z</dc:date>
    <item>
      <title>What makes the MCU ASIL compliant?</title>
      <link>https://community.nxp.com/t5/S32K/What-makes-the-MCU-ASIL-compliant/m-p/960208#M5361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm starting a project on one of the S32K boards, specifically the S32K116 board. I have read some information about the ISO 26262 but I still have some doubts about this norm.&amp;nbsp;What makes the S32K boards ASIL B/D compliant? What kind of software/hardware does it have that categorizes them as "&lt;SPAN style="color: #4a4a4d; background-color: #ffffff; font-size: 16px;"&gt;ASIL-B ISO26262 functional safety". Sorry if this is a stupid question, but I'm very fresh on the ASIL thing.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #4a4a4d; background-color: #ffffff; font-size: 16px;"&gt;Regards,&lt;BR /&gt;Rui&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 16:24:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-makes-the-MCU-ASIL-compliant/m-p/960208#M5361</guid>
      <dc:creator>rjmalmeida0</dc:creator>
      <dc:date>2019-10-08T16:24:02Z</dc:date>
    </item>
    <item>
      <title>Re: What makes the MCU ASIL compliant?</title>
      <link>https://community.nxp.com/t5/S32K/What-makes-the-MCU-ASIL-compliant/m-p/960209#M5362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, ASIL certification is being above whole ECU/system level, so customer could develop ASIL-x compliant appliance with other devices, but such approach could be in-efficient, slow, expensive, complicated, and so on…&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Functional safety and the ISO26262 standard define the general guidelines needed to fulfill the requirements for the different ASIL levels. In NXP we have a program called safe assure. For more information about this program and the devices see following link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/product-information/functional-safety-for-iso-26262-and-iec-61508:FNCTNLSFTY"&gt;https://www.nxp.com/products/product-information/functional-safety-for-iso-26262-and-iec-61508:FNCTNLSFTY&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;“The SafeAssure program highlights selected solutions - including hardware and software - that are targeted for use in functional safety applications, enabling system designers to design with confidence and achieve their system-level design goals and standards compliance more efficiently.”&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The S32 kit itself certainly is not ASIL compliant, it is just evaluation board. I am not aware we had an evaluation board being ASIL compliant as a whole.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The MCU itself is developed according safety standard:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/supporting-information/ISO-26262.pdf"&gt;https://www.nxp.com/docs/en/supporting-information/ISO-26262.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regarding SW, NXP or NXP partners can offers certain software (safety MCAL for instance).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Finally there are additional documents and tools, we says “safety support”. It is mainly safety manual, FMEDA and others. Details you may find here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/product-information/functional-safety-for-iso-26262-and-iec-61508:FNCTNLSFTY"&gt;https://www.nxp.com/products/product-information/functional-safety-for-iso-26262-and-iec-61508:FNCTNLSFTY&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;That’s what makes MCU ASIL compliant.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Oct 2019 14:43:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-makes-the-MCU-ASIL-compliant/m-p/960209#M5362</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2019-10-09T14:43:45Z</dc:date>
    </item>
    <item>
      <title>Re: What makes the MCU ASIL compliant?</title>
      <link>https://community.nxp.com/t5/S32K/What-makes-the-MCU-ASIL-compliant/m-p/1404825#M13795</link>
      <description>&lt;P&gt;Hi sir,&lt;/P&gt;&lt;P&gt;I have one question about ASIL-level, our customer requirement is to use ASIL-B compliant MCU, so we can choose S32K144. But this is only a hardware level meet the requirement. But for the software, we don't know if we can only use NXP provided freeRTOS to meet ASIL-B requirement, or we must choose a ASIL-level OS like AUTOSAT to meet requirement ?&lt;/P&gt;&lt;P&gt;The conclusion is if we want to meet&amp;nbsp; ASIL-B, then we should choose ASIL-B chip and ASIL-B software, or we just use ASIL-B chip with freeRTOS then we can still meet ASIL requirement,&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jan 2022 00:22:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-makes-the-MCU-ASIL-compliant/m-p/1404825#M13795</guid>
      <dc:creator>chen_jackcw</dc:creator>
      <dc:date>2022-01-26T00:22:46Z</dc:date>
    </item>
  </channel>
</rss>