<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Nxps32k312 RAM Check Understanding in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Nxps32k312-RAM-Check-Understanding/m-p/2187132#M53601</link>
    <description>Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&lt;BR /&gt;Thank you for your response. Could you please suggest a solution for how to check for RAM and ROM memory errors.</description>
    <pubDate>Thu, 16 Oct 2025 04:44:24 GMT</pubDate>
    <dc:creator>Anitha7</dc:creator>
    <dc:date>2025-10-16T04:44:24Z</dc:date>
    <item>
      <title>Nxps32k312 RAM Check Understanding</title>
      <link>https://community.nxp.com/t5/S32K/Nxps32k312-RAM-Check-Understanding/m-p/2186398#M53567</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37795"&gt;@lukaszadrapa&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on the NXP S32K312 microcontroller and would like to understand how to detect RAM and ROM memory errors. I noticed that the FCCU (Fault Collection and Control Unit) can be used to monitor such errors. However, it seems that using the FCCU typically requires SAF (Safety) driver installation. I would prefer not to use any additional drivers. Is there a way to access or activate the FCCU registers directly, or alternatively, is there another method to detect RAM and ROM errors without relying on SAF drivers?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Oct 2025 07:36:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Nxps32k312-RAM-Check-Understanding/m-p/2186398#M53567</guid>
      <dc:creator>Anitha7</dc:creator>
      <dc:date>2025-10-15T07:36:36Z</dc:date>
    </item>
    <item>
      <title>Re: Nxps32k312 RAM Check Understanding</title>
      <link>https://community.nxp.com/t5/S32K/Nxps32k312-RAM-Check-Understanding/m-p/2186476#M53572</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228025"&gt;@Anitha7&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You don't need the SAF to inject faults into SRAM or Flash memories and detect them via the FCCU.&lt;BR /&gt;Instead, you can use the SDP drivers included in the standard S32K3xx software package, which are available free of charge.&lt;BR /&gt;To configure the FCCU, use the eMcem driver and call eMcem_InjectFault() to inject faults.&lt;BR /&gt;A SPD demo is available in the SPD standalone installer (.exe) for reference.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Of course, you're free to implement your own EIM/FCCU solution if needed.&lt;/P&gt;
&lt;P&gt;Additionally, faults injected via EIM can be detected by the ERM module, although we currently do not provide a solution for that.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Oct 2025 08:45:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Nxps32k312-RAM-Check-Understanding/m-p/2186476#M53572</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-10-15T08:45:18Z</dc:date>
    </item>
    <item>
      <title>Re: Nxps32k312 RAM Check Understanding</title>
      <link>https://community.nxp.com/t5/S32K/Nxps32k312-RAM-Check-Understanding/m-p/2187132#M53601</link>
      <description>Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&lt;BR /&gt;Thank you for your response. Could you please suggest a solution for how to check for RAM and ROM memory errors.</description>
      <pubDate>Thu, 16 Oct 2025 04:44:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Nxps32k312-RAM-Check-Understanding/m-p/2187132#M53601</guid>
      <dc:creator>Anitha7</dc:creator>
      <dc:date>2025-10-16T04:44:24Z</dc:date>
    </item>
    <item>
      <title>Re: Nxps32k312 RAM Check Understanding</title>
      <link>https://community.nxp.com/t5/S32K/Nxps32k312-RAM-Check-Understanding/m-p/2188943#M53664</link>
      <description>&lt;P&gt;HI&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228025"&gt;@Anitha7&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;As I said, use the SPD drivers.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Oct 2025 06:28:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Nxps32k312-RAM-Check-Understanding/m-p/2188943#M53664</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-10-20T06:28:51Z</dc:date>
    </item>
  </channel>
</rss>