<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 EEPROM sector erase count in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-EEPROM-sector-erase-count/m-p/958034#M5349</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maciej,&lt;/P&gt;&lt;P&gt;I'm sorry for the delay.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Brown-out (BO) detection code depends on the moment when the reset occurs while there is a write in progress.&lt;/P&gt;&lt;P&gt;Please note that the CCIF flag indicates that a command is in progress from the Flash Controller perspective, so that no other commands can be triggered, but the EEPROM state machine has its own timing. If resetting too early, there is no interrupted EEPROM write and the EEPROM simply retains the last valid written record.&lt;/P&gt;&lt;P&gt;You&amp;nbsp;can try delaying the reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FlexMemory Endurance calculator calculates the number of estimated erase cycles on EEPROM backup based on the partition&amp;nbsp;and application requirements. The application can&amp;nbsp;get the number of erase cycles using the EEPROM status query command.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Sep 2019 13:18:32 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2019-09-12T13:18:32Z</dc:date>
    <item>
      <title>S32K144 EEPROM sector erase count</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-EEPROM-sector-erase-count/m-p/958031#M5346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all, &lt;BR /&gt;I am using S32K144 in my project, now I'm implementing EEPROM functionality and all is working fine, but now I want to add some extra feature such as: detected the power loss, or calculation the endurance of the EEPROM in the code. &lt;BR /&gt;I am not using quick write functionality - only standard.&lt;/P&gt;&lt;P&gt;For this purpose, I'm reading the FlexRAM Function command FCCOB, below there is my code it is base on the example from S32 Studio.&lt;BR /&gt;My problem here is that all-time I got 0 in Brown-out (BO) Detection Codes and in EEPROM sector erase count. Even if the power loss is observed in the data reading from backup EFlash because they are initialized with 0xFF. Can you give me some hint?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;Std_Return_t &lt;SPAN class="token function"&gt;Flash_SetFlexRamFunction&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt; FlexRamFunctionControlCode_t tFlexRamFuncCode&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;  NvmStatus_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; psNvmStatus&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 Std_Return_t tResult &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; STD_OK&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="comment token"&gt;/* Check CCIF to verify the previous command is completed */&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0U&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FTFC&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;FSTAT &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; FTFC_FSTAT_CCIF_MASK&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
  tResult &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; STD_BUSY&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
    &lt;SPAN class="keyword token"&gt;else&lt;/SPAN&gt;
    &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
        &lt;SPAN class="comment token"&gt;/* Clear RDCOLERR &amp;amp; ACCERR &amp;amp; FPVIOL flag in flash status register. Write 1 to clear */&lt;/SPAN&gt;
     FTFC&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;FSTAT &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint8&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FTFC_FSTAT_FPVIOL_MASK &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; FTFC_FSTAT_ACCERR_MASK &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; FTFC_FSTAT_RDCOLERR_MASK&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
        &lt;SPAN class="comment token"&gt;/* Passing parameter to the command */&lt;/SPAN&gt;
  FTFC&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;FCCOB&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;FLASH_FCCOB0_INDEX&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; FLASH_FCMD_SET_EERAM&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
  FTFC&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;FCCOB&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;FLASH_FCCOB1_INDEX&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint8_t&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;tFlexRamFuncCode&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

        &lt;SPAN class="comment token"&gt;/* Calling flash command sequence function to execute the command */&lt;/SPAN&gt;
        &lt;SPAN class="token function"&gt;DISABLE_IRQ&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
  tResult &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;Fls_CommandSequence&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
  &lt;SPAN class="token function"&gt;ENABLE_IRQ&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

        &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;tFlexRamFuncCode &lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt; EEE_STATUS_QUERY&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&amp;amp;&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;tResult &lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt; STD_OK&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
        &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
            &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;psNvmStatus &lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0u&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
            &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
             tResult &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; STD_NOT_OK&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
            &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
            &lt;SPAN class="keyword token"&gt;else&lt;/SPAN&gt;
            &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
                psNvmStatus&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;u8BrownOutCode &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; FTFC&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;FCCOB&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;FLASH_FCCOB5_INDEX&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
                psNvmStatus&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;u16SectorEraseCount &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint16_t&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint16_t&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;FTFC&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;FCCOB&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;FLASH_FCCOB8_INDEX&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;8U&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
                psNvmStatus&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;u16SectorEraseCount &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint16_t&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;FTFC&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;FCCOB&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;FLASH_FCCOB9_INDEX&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
            &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
        &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
    &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
    &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; tResult&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2019 07:02:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-EEPROM-sector-erase-count/m-p/958031#M5346</guid>
      <dc:creator>maciej_cebula</dc:creator>
      <dc:date>2019-08-22T07:02:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 EEPROM sector erase count</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-EEPROM-sector-erase-count/m-p/958032#M5347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is the EERRDY flag set after POR?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/88917i56D089E5B1579956/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;How many records have you written to the FlexRAM that you expect erased EEPROM backup sectors?&lt;/P&gt;&lt;P&gt;The EEPROM state machine erases sectors when&amp;nbsp;there is no place left only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2019 14:25:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-EEPROM-sector-erase-count/m-p/958032#M5347</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-08-22T14:25:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 EEPROM sector erase count</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-EEPROM-sector-erase-count/m-p/958033#M5348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;1.&amp;nbsp;EERRDY flag is set after POR.&amp;nbsp;I have a similar algorithm like in flow chart above and it is all time return 0.&lt;/P&gt;&lt;P&gt;2. Thanks for the hint, yesterday I did not enough write to the FlexRam, today I did more, and it returns correctly the number of erasing. Here is my question what is the best way to calculate lifetime for EEPROM? I know that is the dedicated application for this FlexMEmory Endurance Calculator but to me, it is not clear how I can move result from there to the code, that I can in runtime calculate the used of EEPROM.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2019 15:23:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-EEPROM-sector-erase-count/m-p/958033#M5348</guid>
      <dc:creator>maciej_cebula</dc:creator>
      <dc:date>2019-08-22T15:23:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 EEPROM sector erase count</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-EEPROM-sector-erase-count/m-p/958034#M5349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maciej,&lt;/P&gt;&lt;P&gt;I'm sorry for the delay.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Brown-out (BO) detection code depends on the moment when the reset occurs while there is a write in progress.&lt;/P&gt;&lt;P&gt;Please note that the CCIF flag indicates that a command is in progress from the Flash Controller perspective, so that no other commands can be triggered, but the EEPROM state machine has its own timing. If resetting too early, there is no interrupted EEPROM write and the EEPROM simply retains the last valid written record.&lt;/P&gt;&lt;P&gt;You&amp;nbsp;can try delaying the reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FlexMemory Endurance calculator calculates the number of estimated erase cycles on EEPROM backup based on the partition&amp;nbsp;and application requirements. The application can&amp;nbsp;get the number of erase cycles using the EEPROM status query command.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Sep 2019 13:18:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-EEPROM-sector-erase-count/m-p/958034#M5349</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-09-12T13:18:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 EEPROM sector erase count</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-EEPROM-sector-erase-count/m-p/958035#M5350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi sir,&lt;/P&gt;&lt;P&gt;Ian using S32K144 I made partition of flash memory 4kB as EEE Memory and 64kb of flex-NVM.&lt;/P&gt;&lt;P&gt;I used this for sector erase but it's showing status error.&lt;/P&gt;&lt;PRE class="" style="color: #000000;"&gt;address = flashSSDConfig.DFlashBase;&lt;/PRE&gt;&lt;PRE class="" style="color: #000000;"&gt;size = FEATURE_FLS_DF_BLOCK_SECTOR_SIZE;&lt;/PRE&gt;&lt;PRE class="" style="color: #000000;"&gt;ret = FLASH_DRV_EraseSector(&amp;amp;flashSSDConfig, address, size);&lt;/PRE&gt;&lt;PRE class="" style="color: #000000;"&gt;DEV_ASSERT(STATUS_SUCCESS == ret);

Please help me to erase eeprom sector

&lt;/PRE&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Veeraju V Hallikeri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2020 17:08:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-EEPROM-sector-erase-count/m-p/958035#M5350</guid>
      <dc:creator>veerajuvh619</dc:creator>
      <dc:date>2020-03-02T17:08:21Z</dc:date>
    </item>
  </channel>
</rss>