<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K3 HSE</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-HSE/m-p/2183974#M53412</link>
    <description>&lt;P&gt;I would guess, we don't have specific example project combining HSE FW installation with further application simultaneously.&lt;/P&gt;
&lt;P&gt;There are examples S32K344_HSE_FW_INSTALL in HSE examples package&lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;which can be used as a base.&lt;/P&gt;</description>
    <pubDate>Fri, 10 Oct 2025 15:43:25 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2025-10-10T15:43:25Z</dc:date>
    <item>
      <title>S32K3 HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE/m-p/2183734#M53395</link>
      <description>&lt;P&gt;I am currently using the S32K344 chip to debug the information security function. I am flashing the Boot software through PE and hope to integrate the HSE installation part of the code into the Boot project. Is there a sample file for reference? The attachment shows the modified part of the code in the current application project. Currently, the software has entered a hardware error when running&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Oct 2025 08:42:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE/m-p/2183734#M53395</guid>
      <dc:creator>ALXY_WANG1</dc:creator>
      <dc:date>2025-10-10T08:42:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE/m-p/2183974#M53412</link>
      <description>&lt;P&gt;I would guess, we don't have specific example project combining HSE FW installation with further application simultaneously.&lt;/P&gt;
&lt;P&gt;There are examples S32K344_HSE_FW_INSTALL in HSE examples package&lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;which can be used as a base.&lt;/P&gt;</description>
      <pubDate>Fri, 10 Oct 2025 15:43:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE/m-p/2183974#M53412</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2025-10-10T15:43:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE/m-p/2184143#M53419</link>
      <description>The above code is written based on this sample file. Before determining whether to perform UTEST region writing, the address value of 0x1B000000 needs to be obtained. In my application project, directly obtaining 0x1B000000 through a pointer will trigger the hardware error void HardFault_Handler(void). However, when flashing S32K344_HSE_FW_INSTALL, 0x1B000000 can still be directly obtained through a pointer without any problem. Could you please tell me what causes this and what solutions are there</description>
      <pubDate>Sat, 11 Oct 2025 01:27:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE/m-p/2184143#M53419</guid>
      <dc:creator>ALXY_WANG1</dc:creator>
      <dc:date>2025-10-11T01:27:39Z</dc:date>
    </item>
  </channel>
</rss>