<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックInquiry on Secure Debug Authentication and Flash Memory Protection for S32K324 RTD 3.0.0</title>
    <link>https://community.nxp.com/t5/S32K/Inquiry-on-Secure-Debug-Authentication-and-Flash-Memory/m-p/2181114#M53271</link>
    <description>&lt;P&gt;Hi NXP team ,&lt;/P&gt;&lt;P class=""&gt;I am currently working with the NXP S32K324 microcontroller using the RTD version 3.0.0, and I would like to implement secure debug and flash memory protection features with the following requirements:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P class=""&gt;&lt;STRONG&gt;Secure Debug Access:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P class=""&gt;I want to protect the debug port by requiring password-based authentication before enabling any debug session, similar in concept to a UDS service.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Could you please provide recommended best practices or sample code that demonstrates how to enforce debugger authentication effectively on the S32K324 within the RTD 3.0.0 framework?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Guidance on integrating this authentication process into the debug workflow (e.g., with PEmicro Python scripts or equivalent) would be highly appreciated.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;&lt;STRONG&gt;Flash Memory Protection:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P class=""&gt;I aim to secure the flash memory such that write or erase operations require prior authorization or security clearance.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;If available, could you share example code or reference designs that illustrate how to implement flash write/erase locking mechanisms?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Insight into relevant API usage or flash configuration registers for enforcing such protection is also requested.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P class=""&gt;Kind regards,&lt;BR /&gt;Ranjithkumar&lt;/P&gt;</description>
    <pubDate>Tue, 07 Oct 2025 09:53:36 GMT</pubDate>
    <dc:creator>Ranjith_kumar</dc:creator>
    <dc:date>2025-10-07T09:53:36Z</dc:date>
    <item>
      <title>Inquiry on Secure Debug Authentication and Flash Memory Protection for S32K324 RTD 3.0.0</title>
      <link>https://community.nxp.com/t5/S32K/Inquiry-on-Secure-Debug-Authentication-and-Flash-Memory/m-p/2181114#M53271</link>
      <description>&lt;P&gt;Hi NXP team ,&lt;/P&gt;&lt;P class=""&gt;I am currently working with the NXP S32K324 microcontroller using the RTD version 3.0.0, and I would like to implement secure debug and flash memory protection features with the following requirements:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P class=""&gt;&lt;STRONG&gt;Secure Debug Access:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P class=""&gt;I want to protect the debug port by requiring password-based authentication before enabling any debug session, similar in concept to a UDS service.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Could you please provide recommended best practices or sample code that demonstrates how to enforce debugger authentication effectively on the S32K324 within the RTD 3.0.0 framework?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Guidance on integrating this authentication process into the debug workflow (e.g., with PEmicro Python scripts or equivalent) would be highly appreciated.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;&lt;STRONG&gt;Flash Memory Protection:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P class=""&gt;I aim to secure the flash memory such that write or erase operations require prior authorization or security clearance.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;If available, could you share example code or reference designs that illustrate how to implement flash write/erase locking mechanisms?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Insight into relevant API usage or flash configuration registers for enforcing such protection is also requested.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P class=""&gt;Kind regards,&lt;BR /&gt;Ranjithkumar&lt;/P&gt;</description>
      <pubDate>Tue, 07 Oct 2025 09:53:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Inquiry-on-Secure-Debug-Authentication-and-Flash-Memory/m-p/2181114#M53271</guid>
      <dc:creator>Ranjith_kumar</dc:creator>
      <dc:date>2025-10-07T09:53:36Z</dc:date>
    </item>
    <item>
      <title>Re: Inquiry on Secure Debug Authentication and Flash Memory Protection for S32K324 RTD 3.0.0</title>
      <link>https://community.nxp.com/t5/S32K/Inquiry-on-Secure-Debug-Authentication-and-Flash-Memory/m-p/2181410#M53290</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236684"&gt;@Ranjith_kumar&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It is possible to protect JTAG access using a password, and the process varies depending on whether HSE firmware is used or not. For detailed information about both approaches, please refer to the following community threads.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/Can-I-disable-S32K3-s-JTAG-permanently-by-LifeCycle/m-p/1505254" target="_blank" rel="noopener"&gt;Can I disable S32K3's JTAG permanently by LifeCycle configuration bit without ADKP?&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K3-Restrict-the-debug-access-with-a-password-when-HSE-is-used/m-p/1756696" target="_blank" rel="noopener"&gt;[S32K3] Restrict the debug access with a password when HSE is used&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regarding the authentication process for secure debugging, PEmicro provides comprehensive guidance, including explanations and the necessary Python scripts to enable and use the secure debug feature effectively.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.pemicro.com/learningcenter/contents.cfm?content_id=82" target="_blank" rel="noopener"&gt;NXP: Using PEmicro Tools to Enable S32K3xx Secure Debug Support&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;For information on FLASH protection, please refer to the following threads, where this topic has been discussed.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/How-do-I-configure-FLASH-protection-for-the-S32K312/td-p/2116456" target="_blank" rel="noopener"&gt;How do I configure FLASH protection for the S32K312&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/Flash-Protection-Register/td-p/2141729" target="_blank" rel="noopener"&gt;Flash Protection Register&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 07 Oct 2025 18:09:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Inquiry-on-Secure-Debug-Authentication-and-Flash-Memory/m-p/2181410#M53290</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2025-10-07T18:09:46Z</dc:date>
    </item>
  </channel>
</rss>