<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: about test  write dflash and pflash in S32K</title>
    <link>https://community.nxp.com/t5/S32K/about-test-write-dflash-and-pflash/m-p/956082#M5317</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm afraid that we do not have an example of testing all allowed simultaneous memory operations.&lt;/P&gt;&lt;P&gt;I'm not sure if you need help with program/erase PFlash/DFlash functions and&amp;nbsp;which MCU you have, but keep in mind that&amp;nbsp;you can't access partition (flash block) which is being erased or programmed. The code must be executed from RAM memory or another partition.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Jul 2019 07:52:15 GMT</pubDate>
    <dc:creator>dianabatrlova</dc:creator>
    <dc:date>2019-07-25T07:52:15Z</dc:date>
    <item>
      <title>about test  write dflash and pflash</title>
      <link>https://community.nxp.com/t5/S32K/about-test-write-dflash-and-pflash/m-p/956081#M5316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;how to test the following function， can give me some examples?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83136i509DC11F95282EA5/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 03:31:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/about-test-write-dflash-and-pflash/m-p/956081#M5316</guid>
      <dc:creator>814420552</dc:creator>
      <dc:date>2019-07-23T03:31:51Z</dc:date>
    </item>
    <item>
      <title>Re: about test  write dflash and pflash</title>
      <link>https://community.nxp.com/t5/S32K/about-test-write-dflash-and-pflash/m-p/956082#M5317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm afraid that we do not have an example of testing all allowed simultaneous memory operations.&lt;/P&gt;&lt;P&gt;I'm not sure if you need help with program/erase PFlash/DFlash functions and&amp;nbsp;which MCU you have, but keep in mind that&amp;nbsp;you can't access partition (flash block) which is being erased or programmed. The code must be executed from RAM memory or another partition.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jul 2019 07:52:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/about-test-write-dflash-and-pflash/m-p/956082#M5317</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2019-07-25T07:52:15Z</dc:date>
    </item>
  </channel>
</rss>