<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K3 HSE firmware installation issues in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176283#M53065</link>
    <description>&lt;P&gt;Did you follow the Clock &lt;STRONG&gt;Option B&lt;/STRONG&gt; ratio? Any clock frequency selected must adhere to the same clock divider ratios shown in &lt;STRONG&gt;System clocking configurations&lt;/STRONG&gt; of S32K3XXRM.&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K312-flexcan-example-not-running-on-Power-reset/m-p/1802558" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K312-flexcan-example-not-running-on-Power-reset/m-p/1802558&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 26 Sep 2025 05:52:16 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2025-09-26T05:52:16Z</dc:date>
    <item>
      <title>S32K3 HSE firmware installation issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2173113#M52887</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I am using the S32K312 chip and would like to ask if there is a way to reinstall the HSE firmware.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The project compiled with the HSE firmware installation image was programmed and run. After that, the firmware became unusable, and upon re-debugging, I found that I could not retrieve the HSE status and version number. I suspect that the firmware installation failed and resulted in a bad firmware being installed in the secure area. Upon further debugging the firmware installation program, I discovered that the UTEST area has already been written to, and the firmware cannot be reinstalled.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would like to know if there is a way to reinstall the HSE firmware.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;我使用S32K312的芯片，想问下是否有方法可以重新安装Hse固件。&lt;/P&gt;&lt;P&gt;使用Hse固件安装的工程编译后的镜像进行安装。烧录该镜像，运行。之后固件不可用，重新调试发现无法获取到Hse状态和版本号。我怀疑是固件安装失败导致坏的固件被安装到安全保护区。再调试运行固件安装程序发现UTEST区已经被写入了，固件不会被重新安装。&lt;/P&gt;&lt;P&gt;现在想问下是否有方法可以重新安装Hse固件。&lt;/P&gt;</description>
      <pubDate>Sun, 21 Sep 2025 06:33:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2173113#M52887</guid>
      <dc:creator>YuZheng1</dc:creator>
      <dc:date>2025-09-21T06:33:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 HSE firmware installation issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2173326#M52898</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Check HSE GPR register at &lt;STRONG&gt;0x4039C028&lt;/STRONG&gt;. Bit '0' says if HSE firmware is installed or not.&lt;/P&gt;
&lt;P&gt;Programming of the HSE FW feature flag at 0x1B00_0000 is one-time operation. It’s not necessary to do that second time (it’s even not possible). Once it is programmed, the device is unlocked for HSE installation forever.&lt;BR /&gt;You can install HSE FW 0.2.55.0, erase it and install it again without touching the feature flag second time.&lt;/P&gt;
&lt;P&gt;Could you please tell me which project you are using?&amp;nbsp; 如果是...\s32k3_hse_lib_rtd400hf01_20250903\HseLib_HseFwInstall_Rtd400 工程的话，应该不存在这个问题。&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 22 Sep 2025 07:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2173326#M52898</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-09-22T07:03:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 HSE firmware installation issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2173495#M52912</link>
      <description>&lt;P&gt;我是用的工程是 S32K3x2_HseFwInstall_MassProduction_Rtd200_Ds343。&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;0x4039C028&lt;/STRONG&gt;&amp;nbsp;&amp;nbsp;Bit '0' 是 0。 SBAF 的版本号看是01 0D。&lt;/P&gt;&lt;P&gt;Hse固件Flash地址被保护了，我如何去擦除刷写新的Hse固件？&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="YuZheng1_0-1758537596344.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357949i786CFD3BCFEDAE55/image-size/medium?v=v2&amp;amp;px=400" role="button" title="YuZheng1_0-1758537596344.png" alt="YuZheng1_0-1758537596344.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Sep 2025 10:44:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2173495#M52912</guid>
      <dc:creator>YuZheng1</dc:creator>
      <dc:date>2025-09-22T10:44:42Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 HSE firmware installation issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176174#M53061</link>
      <description>&lt;P&gt;&amp;nbsp;...\MassProduction_1_0_1\0.2.1.0_0.2.6.0\MassProduction\image\s19\S32K3x2_HseFwInstall_MassProduction_Rtd200_Ds343_AB_SWAP_FW_0260.srec&lt;/P&gt;
&lt;P&gt;The offline programming process in &lt;STRONG&gt;S32K3_HseAppProgram_MassProduction_UserGuide_AbSwap.pdf&lt;/STRONG&gt; are for CYCLONE and should also be followed when using other Flash Programmer. For example, &lt;STRONG&gt;delay&lt;/STRONG&gt; at least &lt;STRONG&gt;3 seconds&lt;/STRONG&gt; after download &lt;EM&gt;S32K3x2_HseFwInstall_MassProduction_Rtd200_Ds343_AB_SWAP_FW_0260.srec&lt;/EM&gt; and &lt;STRONG&gt;Run&lt;/STRONG&gt;(F9 when using J-Flash)&amp;nbsp;&amp;nbsp;Wait for the HSE FW to complete the installation.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="delay at least 3 seconds after download S32K3x2_HseFwInstall_MassProduction_Rtd200_Ds343_AB_SWAP_FW_0260 srec and Run.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/358627iD84F1DDD19753692/image-size/large?v=v2&amp;amp;px=999" role="button" title="delay at least 3 seconds after download S32K3x2_HseFwInstall_MassProduction_Rtd200_Ds343_AB_SWAP_FW_0260 srec and Run.png" alt="delay at least 3 seconds after download S32K3x2_HseFwInstall_MassProduction_Rtd200_Ds343_AB_SWAP_FW_0260 srec and Run.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Here is the value shown the HSE FW already installed:&lt;BR /&gt;SBAF version &lt;STRONG&gt;0x4039C020&lt;/STRONG&gt;= 010D0000 00090001 means 1.13.0_2.6.0 (AB_SWAP)&lt;BR /&gt;&lt;STRONG&gt;0x4039C028&lt;/STRONG&gt; bit 0=1&amp;nbsp;says HSE firmware is installed.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="0x4039C020 J-Flash S32K3x2_HseFwInstall_MassProduction_Rtd200_Ds343_AB_SWAP_FW_0260 srec.png" style="width: 594px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/358626iD4C157B0679AA0CE/image-size/large?v=v2&amp;amp;px=999" role="button" title="0x4039C020 J-Flash S32K3x2_HseFwInstall_MassProduction_Rtd200_Ds343_AB_SWAP_FW_0260 srec.png" alt="0x4039C020 J-Flash S32K3x2_HseFwInstall_MassProduction_Rtd200_Ds343_AB_SWAP_FW_0260 srec.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 02:12:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176174#M53061</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-09-26T02:12:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 HSE firmware installation issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176277#M53064</link>
      <description>&lt;P&gt;好的，我又进行了尝试，也是可以正常安装的啦。&lt;/P&gt;&lt;P&gt;我发现是我们合并了一版修改时钟和添加Power模块休眠唤醒功能的代码后，运行后导致Hse固件损坏了。再也无法获取到Hse的状态啦。&lt;/P&gt;&lt;P&gt;麻烦再请问下这个情况可能是什么原因会导致Hse固件损坏，有什么方法可以修复它吗？&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Okay, I've tried again and it can be installed normally.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I found that after we merged a version of code that modified the clock and added the Power module's sleep/wake functionality, running it caused the Hse firmware to become corrupted. We can no longer retrieve the Hse status. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you please advise what might have caused the Hse firmware corruption in this case, and is there any way to fix it?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 05:25:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176277#M53064</guid>
      <dc:creator>YuZheng1</dc:creator>
      <dc:date>2025-09-26T05:25:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 HSE firmware installation issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176283#M53065</link>
      <description>&lt;P&gt;Did you follow the Clock &lt;STRONG&gt;Option B&lt;/STRONG&gt; ratio? Any clock frequency selected must adhere to the same clock divider ratios shown in &lt;STRONG&gt;System clocking configurations&lt;/STRONG&gt; of S32K3XXRM.&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K312-flexcan-example-not-running-on-Power-reset/m-p/1802558" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K312-flexcan-example-not-running-on-Power-reset/m-p/1802558&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 05:52:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176283#M53065</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-09-26T05:52:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 HSE firmware installation issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176305#M53067</link>
      <description>&lt;P&gt;请问这个Hse Clk只能配置为60MHz吗？我们这个配置是之前就已经配置为80MHz了并且没有出现问题。在合入其他修改后出现的这个问题。&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is this Hse Clk limited to a configuration of only 60MHz? We previously configured it to 80MHz without any issues. This problem only appeared after merging other modifications.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wechat_2025-09-26_140411_841.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/358656i58BA428729DE651B/image-size/large?v=v2&amp;amp;px=999" role="button" title="wechat_2025-09-26_140411_841.png" alt="wechat_2025-09-26_140411_841.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 06:09:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176305#M53067</guid>
      <dc:creator>YuZheng1</dc:creator>
      <dc:date>2025-09-26T06:09:52Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 HSE firmware installation issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176325#M53069</link>
      <description>&lt;P&gt;CORE_CLK并不是必须80MHz，但是比例必须遵顼 可以参考这里的比率&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/All-Example-S32K312-DS3-5-RTD-3-0-0/ta-p/1790004" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/All-Example-S32K312-DS3-5-RTD-3-0-0/ta-p/1790004&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;HSE FW丢失的原因有许多，建议阅读&lt;A href="https://community.nxp.com/t5/S32K/S32K3%E5%B8%B8%E8%A7%81%E9%97%AE%E9%A2%98%E6%A3%80%E6%9F%A5%E5%88%97%E8%A1%A8-Check-list-%E5%88%86%E4%BA%AB/m-p/2020858#M44683" target="_self"&gt;S32K3常见问题检查列表(Check list)分享&lt;/A&gt;的&lt;STRONG&gt;4.20&amp;nbsp;&lt;/STRONG&gt;&lt;STRONG style="font-family: inherit;"&gt;HSE&lt;/STRONG&gt;&lt;STRONG style="font-family: inherit;"&gt;固件损坏或被擦除的原因&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 06:48:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176325#M53069</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-09-26T06:48:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 HSE firmware installation issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176348#M53072</link>
      <description>&lt;P&gt;还想问下如果Hse固件已经确认损坏，有什么方法可以修复吗？还是只能更换新的芯片啊？&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 07:08:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176348#M53072</guid>
      <dc:creator>YuZheng1</dc:creator>
      <dc:date>2025-09-26T07:08:36Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 HSE firmware installation issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176438#M53080</link>
      <description>&lt;P&gt;请尝试&lt;SPAN&gt;MU Restore FW_EN.pdf 里提到的方法修复：&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/S32K/19042/1/MU%20Restore%20FW_EN.pdf" target="_blank" rel="noopener"&gt;https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/S32K/19042/1/MU%20Restore%20FW_EN.pdf&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 08:37:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE-firmware-installation-issues/m-p/2176438#M53080</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-09-26T08:37:26Z</dc:date>
    </item>
  </channel>
</rss>