<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: cannot connect M7_1 on K322</title>
    <link>https://community.nxp.com/t5/S32K/cannot-connect-M7-1-on-K322/m-p/2175008#M53003</link>
    <description>That was the problem.&lt;BR /&gt;Thx</description>
    <pubDate>Wed, 24 Sep 2025 12:05:54 GMT</pubDate>
    <dc:creator>Micha4566465</dc:creator>
    <dc:date>2025-09-24T12:05:54Z</dc:date>
    <item>
      <title>cannot connect M7_1 on K322</title>
      <link>https://community.nxp.com/t5/S32K/cannot-connect-M7-1-on-K322/m-p/2170336#M52711</link>
      <description>&lt;P&gt;when I create an application project in Design Studio 3.6.x for K322,&lt;/P&gt;&lt;P&gt;I can debug the M7_0 core with my PEmicro and the Debug_FLASH_PNE configuration.&lt;/P&gt;&lt;P&gt;When I try to debug the M7_1 core, I cannot establish a connection to this core.&lt;/P&gt;&lt;P&gt;In console there is an error message:&lt;/P&gt;&lt;P&gt;"&lt;SPAN&gt;Could not connect to semihosting port due to connection timeout. Please check that the correct port number is configured."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The status always is halted at 95%.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;At the end there is an error window with message: "error 138".&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I checked that there are no breaking points at start up for the other core.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I also checked that I am using the 100-pin K322 and I checked the correct clock settings.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I checked that in both mex-files.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can anybody help me please?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Sep 2025 09:24:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/cannot-connect-M7-1-on-K322/m-p/2170336#M52711</guid>
      <dc:creator>Micha4566465</dc:creator>
      <dc:date>2025-09-16T09:24:12Z</dc:date>
    </item>
    <item>
      <title>Re: cannot connect M7_1 on K322</title>
      <link>https://community.nxp.com/t5/S32K/cannot-connect-M7-1-on-K322/m-p/2170783#M52737</link>
      <description>&lt;P&gt;Debugging the M7_1 core on K322 in Design Studio 3.6.x fails due to a semihosting connection timeout and "error 138." This issue likely stems from a port number misconfiguration or a race condition between the two cores, preventing a successful connection to M7_1. To fix this, ensure the correct semihosting port is set for M7_1 and consider initializing M7_0 in a way that doesn't interfere with the debugger's connection&amp;nbsp;&lt;FONT size="1 2 3 4 5 6 7" color="#FFFFFF"&gt;&lt;A href="https://www.kaisermemberservices.org" target="_self"&gt;&lt;FONT color="#FFFFFF"&gt;KaiserMemberServices&lt;/FONT&gt;&lt;/A&gt;&lt;/FONT&gt; to the second core.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Sep 2025 03:59:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/cannot-connect-M7-1-on-K322/m-p/2170783#M52737</guid>
      <dc:creator>elsie78ash</dc:creator>
      <dc:date>2025-09-17T03:59:36Z</dc:date>
    </item>
    <item>
      <title>Re: cannot connect M7_1 on K322</title>
      <link>https://community.nxp.com/t5/S32K/cannot-connect-M7-1-on-K322/m-p/2170945#M52761</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214057"&gt;@Micha4566465&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Debug both cores in Launch Group:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1758096453497.png" style="width: 686px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357258i42FC9C05AFCA11FE/image-dimensions/686x580?v=v2" width="686" height="580" role="button" title="danielmartynek_0-1758096453497.png" alt="danielmartynek_0-1758096453497.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1758096453497.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if you have questions,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Sep 2025 08:08:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/cannot-connect-M7-1-on-K322/m-p/2170945#M52761</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-09-17T08:08:21Z</dc:date>
    </item>
    <item>
      <title>Re: cannot connect M7_1 on K322</title>
      <link>https://community.nxp.com/t5/S32K/cannot-connect-M7-1-on-K322/m-p/2175008#M53003</link>
      <description>That was the problem.&lt;BR /&gt;Thx</description>
      <pubDate>Wed, 24 Sep 2025 12:05:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/cannot-connect-M7-1-on-K322/m-p/2175008#M53003</guid>
      <dc:creator>Micha4566465</dc:creator>
      <dc:date>2025-09-24T12:05:54Z</dc:date>
    </item>
  </channel>
</rss>