<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: LIN stack configuration file generation</title>
    <link>https://community.nxp.com/t5/S32K/Re-LIN-stack-configuration-file-generation/m-p/2174294#M52976</link>
    <description>&lt;P&gt;Hey&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239163"&gt;@mayliu1&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thank you for the quick response.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I integrated the MCUX SDK LIN stack into Zephyr OS and I am testing it now on a S32K344-wb board, but I want to change the cfg files and I was wondering if there is a method through which I can automatically generate them from a .ldf file.&lt;/P&gt;</description>
    <pubDate>Tue, 23 Sep 2025 11:58:52 GMT</pubDate>
    <dc:creator>SarMol</dc:creator>
    <dc:date>2025-09-23T11:58:52Z</dc:date>
    <item>
      <title>Re: LIN stack configuration file generation</title>
      <link>https://community.nxp.com/t5/S32K/Re-LIN-stack-configuration-file-generation/m-p/2174294#M52976</link>
      <description>&lt;P&gt;Hey&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239163"&gt;@mayliu1&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thank you for the quick response.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I integrated the MCUX SDK LIN stack into Zephyr OS and I am testing it now on a S32K344-wb board, but I want to change the cfg files and I was wondering if there is a method through which I can automatically generate them from a .ldf file.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 11:58:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Re-LIN-stack-configuration-file-generation/m-p/2174294#M52976</guid>
      <dc:creator>SarMol</dc:creator>
      <dc:date>2025-09-23T11:58:52Z</dc:date>
    </item>
    <item>
      <title>Re: LIN stack configuration file generation</title>
      <link>https://community.nxp.com/t5/S32K/Re-LIN-stack-configuration-file-generation/m-p/2174637#M52977</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;SarMol&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Why do you use MCUX instead of S32 DS when using S32K3 series MCU?&lt;/P&gt;
&lt;P&gt;Can't these things you said be done with S32 DS?&lt;/P&gt;
&lt;P&gt;After installing S32 DS and RTD, find the corresponding version of LIN STANCK, import your LDF file, and generate the configuration file.&lt;/P&gt;
&lt;P&gt;These practices can be done with S32 DS.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 02:17:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Re-LIN-stack-configuration-file-generation/m-p/2174637#M52977</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2025-09-24T02:17:06Z</dc:date>
    </item>
    <item>
      <title>Re: LIN stack configuration file generation</title>
      <link>https://community.nxp.com/t5/S32K/Re-LIN-stack-configuration-file-generation/m-p/2174806#M52985</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188029"&gt;@Senlent&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;I am working with Zephyr and the only way (that I have found) to integrate the LIN stack into the OS is to use the MCUX version. This requires the lin_cfg.c/.h files and I took them from the demos that were present in the MCUX demo repository and modified them by hand just to see if my integration was successful, though I would like to have an automated method to generate them. I tried to generate them from S32DS, but the lin_stack_cfg.c/.h files were not compatible with what the MCUX version expected.&lt;/P&gt;&lt;P&gt;My question now is where did the lin_cfg.c/.h files from the demos come from? Were they written by hand or is there a tool capable of generating configuration files compatible with what the MCUX SDK LIN stack expects?&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 06:46:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Re-LIN-stack-configuration-file-generation/m-p/2174806#M52985</guid>
      <dc:creator>SarMol</dc:creator>
      <dc:date>2025-09-24T06:46:02Z</dc:date>
    </item>
    <item>
      <title>Re: LIN stack configuration file generation</title>
      <link>https://community.nxp.com/t5/S32K/Re-LIN-stack-configuration-file-generation/m-p/2174823#M52986</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;SarMol&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I consulted an engineer who is familiar with MCUX. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The IDE does not support importing LDF files to generate these configuration and driver files. To put it simply, they are handwritten.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 07:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Re-LIN-stack-configuration-file-generation/m-p/2174823#M52986</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2025-09-24T07:25:35Z</dc:date>
    </item>
    <item>
      <title>Re: LIN stack configuration file generation</title>
      <link>https://community.nxp.com/t5/S32K/Re-LIN-stack-configuration-file-generation/m-p/2174825#M52987</link>
      <description>Ok, thank you very much!</description>
      <pubDate>Wed, 24 Sep 2025 07:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Re-LIN-stack-configuration-file-generation/m-p/2174825#M52987</guid>
      <dc:creator>SarMol</dc:creator>
      <dc:date>2025-09-24T07:29:43Z</dc:date>
    </item>
  </channel>
</rss>