<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックProblems building MCSPTR2AK396 example application</title>
    <link>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2173643#M52921</link>
    <description>&lt;P&gt;I am trying to rebuild the&amp;nbsp;MCSPTR2AK396 example application, but cannot quite get Design Studio to cooperate with me.&lt;BR /&gt;&lt;BR /&gt;The issue I am having is that when I open the .mex file for the main (boot) core I get a popup flash of some kind and then it immediately opens a browser window but without directing it to a page. Looks like some error occurs, but the message popup immediately disappears. No messages at all shown in the log.&lt;BR /&gt;&lt;BR /&gt;Further, if I select to "Update code" then all drivers are removed from the project.&lt;BR /&gt;&lt;BR /&gt;Any hints on what I am missing?&lt;BR /&gt;&lt;BR /&gt;The installed software stack is almost the same as the same as stated as tested in the release notes for the example app&lt;BR /&gt;&lt;BR /&gt;Design Studio 3.6.3 (3.6.1 stated)&lt;BR /&gt;S32K3xx Development Package 3.6.3 (3.6.0 stated)&lt;BR /&gt;S32K3 Real-Time Drivers AUTOSAR R21-11 Version 5.0.0 (same as stated)&lt;BR /&gt;AMMCLIB 1.1.41 (1.1.39 stated, but is not available)&lt;BR /&gt;S32K3 FreeMASTER Serial Communication Driver 1.4.2 (same as stated)&lt;BR /&gt;S32K3 ETPU SW 4.7 2.0.0 Version 2.0.0&amp;nbsp; (2.0.0 CD04 stated)&lt;BR /&gt;&lt;BR /&gt;What I have noticed is that the path to AMMCLIB is hardcoded in the project include &amp;amp; library paths. And there is also RTD references hardcoded to the 5.0.0 release.&lt;/P&gt;</description>
    <pubDate>Mon, 22 Sep 2025 15:31:56 GMT</pubDate>
    <dc:creator>Henrik-Wires</dc:creator>
    <dc:date>2025-09-22T15:31:56Z</dc:date>
    <item>
      <title>Problems building MCSPTR2AK396 example application</title>
      <link>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2173643#M52921</link>
      <description>&lt;P&gt;I am trying to rebuild the&amp;nbsp;MCSPTR2AK396 example application, but cannot quite get Design Studio to cooperate with me.&lt;BR /&gt;&lt;BR /&gt;The issue I am having is that when I open the .mex file for the main (boot) core I get a popup flash of some kind and then it immediately opens a browser window but without directing it to a page. Looks like some error occurs, but the message popup immediately disappears. No messages at all shown in the log.&lt;BR /&gt;&lt;BR /&gt;Further, if I select to "Update code" then all drivers are removed from the project.&lt;BR /&gt;&lt;BR /&gt;Any hints on what I am missing?&lt;BR /&gt;&lt;BR /&gt;The installed software stack is almost the same as the same as stated as tested in the release notes for the example app&lt;BR /&gt;&lt;BR /&gt;Design Studio 3.6.3 (3.6.1 stated)&lt;BR /&gt;S32K3xx Development Package 3.6.3 (3.6.0 stated)&lt;BR /&gt;S32K3 Real-Time Drivers AUTOSAR R21-11 Version 5.0.0 (same as stated)&lt;BR /&gt;AMMCLIB 1.1.41 (1.1.39 stated, but is not available)&lt;BR /&gt;S32K3 FreeMASTER Serial Communication Driver 1.4.2 (same as stated)&lt;BR /&gt;S32K3 ETPU SW 4.7 2.0.0 Version 2.0.0&amp;nbsp; (2.0.0 CD04 stated)&lt;BR /&gt;&lt;BR /&gt;What I have noticed is that the path to AMMCLIB is hardcoded in the project include &amp;amp; library paths. And there is also RTD references hardcoded to the 5.0.0 release.&lt;/P&gt;</description>
      <pubDate>Mon, 22 Sep 2025 15:31:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2173643#M52921</guid>
      <dc:creator>Henrik-Wires</dc:creator>
      <dc:date>2025-09-22T15:31:56Z</dc:date>
    </item>
    <item>
      <title>Re: Problems building MCSPTR2AK396 example application</title>
      <link>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2174068#M52943</link>
      <description>&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;Found the error log. And there is two errors reported when reloading the .mex&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;LI-CODE lang="markup"&gt;[DATA] Error resolving: (($configSet.PwmGeneral.PwmDutycycleUpdatedEndperiod.getValue() == true) || ($configSet.PwmGeneral.PwmPeriodUpdatedEndperiod.getValue() == true)), Value of: $configSet.PwmGeneral.PwmDutycycleUpdatedEndperiod not found&lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;and&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;An error has occurred. See error log for more details.

PeripheralExpressionException[

Description: Could not retrieve resource setting for arguments `MotorControl` and `Channel.List` of the function: getResource

Function: getResource(valid, valid)

Contexts:

ExpressionContext[ child_context = ChildContext[

$this = Etpu_Resolver_Ip.ResolverConfiguration.0.ResolverInstanceContainer.ResolverChanNumExcID

component = Etpu_Resolver_Ip

$instance = Etpu_Resolver_Ip

$group = BOARD_InitPeripherals]]


ExpressionContext[ child_context = ChildContext[

$this = Etpu_Resolver_Ip.ResolverConfiguration.0.ResolverInstanceContainer.ResolverChanNumExcID

component = Etpu_Resolver_Ip

$instance = Etpu_Resolver_Ip

$group = BOARD_InitPeripherals]]


ExpressionContext[ child_context = ChildContext[

$this = Etpu_Resolver_Ip.ResolverConfiguration.0.ResolverInstanceContainer.ResolverChanNumExcID

component = Etpu_Resolver_Ip

$instance = Etpu_Resolver_Ip

$group = BOARD_InitPeripherals]]

]&lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 07:29:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2174068#M52943</guid>
      <dc:creator>Henrik-Wires</dc:creator>
      <dc:date>2025-09-23T07:29:57Z</dc:date>
    </item>
    <item>
      <title>Re: Problems building MCSPTR2AK396 example application</title>
      <link>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2174266#M52958</link>
      <description>Downgraded to 3.6.1 and the problem remains. The above two errors, and whenever I generate code almost all drivers are removed from the project.</description>
      <pubDate>Tue, 23 Sep 2025 10:59:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2174266#M52958</guid>
      <dc:creator>Henrik-Wires</dc:creator>
      <dc:date>2025-09-23T10:59:14Z</dc:date>
    </item>
    <item>
      <title>Re: Problems building MCSPTR2AK396 example application</title>
      <link>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2174522#M52969</link>
      <description>&lt;P&gt;Thank you for your interest in our products and for contributing to our community.&lt;/P&gt;
&lt;P&gt;I have installed the SW according with the &lt;EM&gt;MCSPTR2AK396_ReleaseNotes.txt&lt;/EM&gt;:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;The Development Kit application was built and tested using the following IDE, Drivers and Tools:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;=====================================================================================&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- Examples based on the RTD low level API:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- S32 Design Studio for S32 Platform Version 3.6.1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- S32K3xx development package version 3.6.0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- S32K39X Real-Time Drivers AUTOSAR R21-11 Version 5.0.0 (exclude SGEN)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- S32K3 ETPU SW 4.7 2.0.0 CD04 Version 2.0.0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- S32K3 FreeMASTER Serial Communication Driver Version 1.4.2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- FreeMASTER 3.2.4.5&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;And project builds successfully:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="_Leo__0-1758655160473.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/358208iA6D7E9941144AAC6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="_Leo__0-1758655160473.png" alt="_Leo__0-1758655160473.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Also using &lt;EM&gt;AMMCLib v1.1.39&lt;/EM&gt;:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="_Leo__1-1758655188050.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/358209i81E6BEC63D7A4F1B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="_Leo__1-1758655188050.png" alt="_Leo__1-1758655188050.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please share an screenshot of your &lt;EM&gt;Installation details&lt;/EM&gt; (in &lt;EM&gt;Help&lt;/EM&gt; tab), to check.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 19:20:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2174522#M52969</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2025-09-23T19:20:43Z</dc:date>
    </item>
    <item>
      <title>Re: Problems building MCSPTR2AK396 example application</title>
      <link>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2176575#M53087</link>
      <description>I can build the application as-is if I only import the project and correct AMMCLIB paths in the project settings to refer to 1.1.41 instead of 1.1.39.&lt;BR /&gt;&lt;BR /&gt;The issues arise if I open the main mex file.&lt;BR /&gt;/MCSPTR2AK396_PMSM_FOC_3Sh_SwRes_ll_M7_0_0/MCSPTR2AK396_PMSM_FOC_3Sh_SwRes_ll_M7_0_0.mex</description>
      <pubDate>Fri, 26 Sep 2025 11:07:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2176575#M53087</guid>
      <dc:creator>Henrik-Wires</dc:creator>
      <dc:date>2025-09-26T11:07:33Z</dc:date>
    </item>
    <item>
      <title>Re: Problems building MCSPTR2AK396 example application</title>
      <link>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2176576#M53088</link>
      <description>I can not find AMMCLIB 1.1.39 available for download.&lt;BR /&gt;&lt;BR /&gt;And Design Studio refuses to not upgrade the platform packages when installing the RTD 5.0.0 package.</description>
      <pubDate>Fri, 26 Sep 2025 11:10:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2176576#M53088</guid>
      <dc:creator>Henrik-Wires</dc:creator>
      <dc:date>2025-09-26T11:10:30Z</dc:date>
    </item>
    <item>
      <title>Re: Problems building MCSPTR2AK396 example application</title>
      <link>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2176627#M53093</link>
      <description>&lt;P&gt;Finally got it working. I apparently had a somewhat newer ETPU version installed.&lt;BR /&gt;&lt;BR /&gt;S32K3_ETPU_SW_4.7_2.0.0_D2509&lt;/P&gt;&lt;P&gt;instead of&lt;/P&gt;&lt;P&gt;S32K3_ETPU_SW_4.7_2.0.0_CD04_D2502&lt;BR /&gt;&lt;BR /&gt;And this caused a lot of problems.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 12:41:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problems-building-MCSPTR2AK396-example-application/m-p/2176627#M53093</guid>
      <dc:creator>Henrik-Wires</dc:creator>
      <dc:date>2025-09-26T12:41:16Z</dc:date>
    </item>
  </channel>
</rss>