<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to Configure ADC Multiple Channels with DMA using Software Trigger in S32K358 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/How-to-Configure-ADC-Multiple-Channels-with-DMA-using-Software/m-p/2173497#M52913</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I posted one example for continuous scan of multiple ADC channels with DMA reading on&amp;nbsp;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K/How-to-Configure-ADC-Multiple-Channels-with-DMA-using-Software/td-p/2173045" target="_blank"&gt;https://community.nxp.com/t5/S32K/How-to-Configure-ADC-Multiple-Channels-with-DMA-using-Software/td-p/2173045&lt;/A&gt;&lt;BR /&gt;It is for S32K312, but you can refer to it.&lt;BR /&gt;The DMA setting is dependent on which ADC channels are going to be sampled. Ideally consecutive channels should be used, so DMA can be easily set.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Mon, 22 Sep 2025 10:46:02 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2025-09-22T10:46:02Z</dc:date>
    <item>
      <title>How to Configure ADC Multiple Channels with DMA using Software Trigger in S32K358</title>
      <link>https://community.nxp.com/t5/S32K/How-to-Configure-ADC-Multiple-Channels-with-DMA-using-Software/m-p/2173045#M52881</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on the S32K358 and I want to configure the ADC to read multiple channels using DMA. Specifically, I would like to:&lt;/P&gt;&lt;P&gt;Use a software trigger to start ADC conversion.&lt;/P&gt;&lt;P&gt;Configure the DMA so that the converted results from multiple channels are transferred to a buffer automatically.&lt;/P&gt;&lt;P&gt;Handle the sequence of multiple ADC channels without CPU intervention for each conversion.&lt;/P&gt;&lt;P&gt;I am a bit confused about the steps required in the S32DS + RTD environment (or SDK).&lt;/P&gt;&lt;P&gt;How do I configure the ADC for multiple channels with software trigger?&lt;/P&gt;&lt;P&gt;How should I set up the DMA TCD (Transfer Control Descriptor) so that each ADC conversion result is placed correctly in memory?&lt;/P&gt;&lt;P&gt;Is there an example or application note for ADC + DMA + software trigger on S32K3 MCUs?&lt;/P&gt;&lt;P&gt;Any guidance, example code, or reference material will be very helpful.&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Sat, 20 Sep 2025 04:04:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-Configure-ADC-Multiple-Channels-with-DMA-using-Software/m-p/2173045#M52881</guid>
      <dc:creator>D_K</dc:creator>
      <dc:date>2025-09-20T04:04:40Z</dc:date>
    </item>
    <item>
      <title>Re: How to Configure ADC Multiple Channels with DMA using Software Trigger in S32K358</title>
      <link>https://community.nxp.com/t5/S32K/How-to-Configure-ADC-Multiple-Channels-with-DMA-using-Software/m-p/2173497#M52913</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I posted one example for continuous scan of multiple ADC channels with DMA reading on&amp;nbsp;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K/How-to-Configure-ADC-Multiple-Channels-with-DMA-using-Software/td-p/2173045" target="_blank"&gt;https://community.nxp.com/t5/S32K/How-to-Configure-ADC-Multiple-Channels-with-DMA-using-Software/td-p/2173045&lt;/A&gt;&lt;BR /&gt;It is for S32K312, but you can refer to it.&lt;BR /&gt;The DMA setting is dependent on which ADC channels are going to be sampled. Ideally consecutive channels should be used, so DMA can be easily set.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 22 Sep 2025 10:46:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-Configure-ADC-Multiple-Channels-with-DMA-using-Software/m-p/2173497#M52913</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-09-22T10:46:02Z</dc:date>
    </item>
  </channel>
</rss>