<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K146 / 148 Externall Interrupt</title>
    <link>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2173006#M52879</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211726"&gt;@E_GK&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;2. Normally, when adding drivers to the config tools, the driver is added to the project as well. Simply clicking "Update Code" generates the necessary files. You can also right-click and add them to the toolchain manually:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Snag_1819ba3.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357806iD7AC85C83F83EA86/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Snag_1819ba3.png" alt="Snag_1819ba3.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;3. Instead of using RTD, you can use&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5413.pdf" target="_blank"&gt;AN5413: S32K1xx Series Cookbook.&lt;/A&gt;&amp;nbsp;While there is no pin interrupt example, you can use it as reference. Chapter&amp;nbsp;2.3 (Hello World + Interrupts) shows how to configure interrupts.&lt;/P&gt;
&lt;P&gt;If the examples are not being imported correctly, there may be an issue with your RTD installations. If possible, please try to do a clean install. I've attached a simple guide on how to download and install the RTD packages. It is based on S32K3XX devices, but procedure is the same for S32K1.&lt;/P&gt;
&lt;P&gt;Hope this helps.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 19 Sep 2025 22:22:51 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2025-09-19T22:22:51Z</dc:date>
    <item>
      <title>S32K146 / 148 Externall Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2171123#M52776</link>
      <description>&lt;P&gt;Hello Everyone,&lt;/P&gt;&lt;P&gt;I need to use in my project the externall interrupt functionality. So I have a question -&amp;nbsp; How to add its in the S32 Design Studio? I used "Routing Details" (inside the "Pin" perspective window) to modify "Interrupt Configuration&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="E_GK_0-1758111179667.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357314i634DE30379894D33/image-size/medium?v=v2&amp;amp;px=400" role="button" title="E_GK_0-1758111179667.png" alt="E_GK_0-1758111179667.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;" Where is the interrupt handler? I have analused modification of source code after I cliced&amp;nbsp; on "Update Code", but I wasn't able to find it.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="E_GK_1-1758111570078.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357315i7019CF5D86B7CAAA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="E_GK_1-1758111570078.png" alt="E_GK_1-1758111570078.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use S32 DS v3.5 versionon.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Sep 2025 12:20:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2171123#M52776</guid>
      <dc:creator>E_GK</dc:creator>
      <dc:date>2025-09-17T12:20:09Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 / 148 Externall Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2171247#M52781</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211726"&gt;@E_GK&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Port_Icu and IntCtrl drivers are needed to control the pin interrupt. Please refer to this post:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/GPIO-interrupt-example-project-using-S32K1xx-RTD-without-AUTOSAR/ta-p/1540959" target="_blank" rel="noopener"&gt;GPIO interrupt example project using S32K1xx RTD without AUTOSAR - NXP Community&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;It is based on S32DS v3.4, but routine should be the same in newer version.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Sep 2025 16:20:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2171247#M52781</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-09-17T16:20:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 / 148 Externall Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2171963#M52815</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Thank you for this information. I have install the autosar extension (RTD for S32K1 and S32 RTD Autosar), but there is no the driver in my project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are a screans from my project below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="E_GK_0-1758191668519.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357519iE6B47C66054C096C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="E_GK_0-1758191668519.png" alt="E_GK_0-1758191668519.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="E_GK_1-1758191764259.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357520iEEB86202F40378AB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="E_GK_1-1758191764259.png" alt="E_GK_1-1758191764259.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have additional question: How to add any example for SS32DS V3.6?&lt;/P&gt;&lt;P&gt;I have installed the same extension, but there are no examples...&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="E_GK_2-1758192360409.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357526i7CA3B98D7442F020/image-size/medium?v=v2&amp;amp;px=400" role="button" title="E_GK_2-1758192360409.png" alt="E_GK_2-1758192360409.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Sep 2025 10:59:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2171963#M52815</guid>
      <dc:creator>E_GK</dc:creator>
      <dc:date>2025-09-18T10:59:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 / 148 Externall Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2172140#M52819</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211726"&gt;@E_GK&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Have you expanded the RTD list for the examples?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_2-1758210496639.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357572i8137F7B1AC836D7D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_2-1758210496639.png" alt="Julin_AragnM_2-1758210496639.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;From the pictures you've shared, it seems that you have installed multiple RTD packages into the IDE. This is&amp;nbsp;&lt;STRONG&gt;not&lt;/STRONG&gt; supported. Please try installing a singular RTD version.&lt;/P&gt;
&lt;P&gt;Lastly, I can see you have S32K1 RTD 2.0.0&amp;nbsp;&lt;STRONG&gt;QLP1&lt;/STRONG&gt; installed. This release is a quality patch, mainly focused on crypto:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1758210351987.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357569i569C96BF6D8CC30B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_0-1758210351987.png" alt="Julin_AragnM_0-1758210351987.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please try installing the&amp;nbsp;&lt;STRONG&gt;base&lt;/STRONG&gt; version of the patch (RTD 2.0.0, without &lt;STRONG&gt;QLP1&lt;/STRONG&gt;) in order to get full drivers support.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Sep 2025 15:48:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2172140#M52819</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-09-18T15:48:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 / 148 Externall Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2172691#M52844</link>
      <description>&lt;P&gt;Hello&amp;nbsp;Julián&lt;/P&gt;&lt;P&gt;Thank you for your answer. I have uninstalled all the versions of S32 DS (V3.5 and 3.6.3). After that I have installed verion 3.6.3 and the bellow package:&lt;/P&gt;&lt;P&gt;SW32K1_S32M24x_RTD_4.4_R21-11_2.0.0_D2308.exe&lt;/P&gt;&lt;P&gt;SW32K1_S32M24x_RTD_4.4_R21-11_2.0.0_D2308_DS_Updatesite.zip.&lt;/P&gt;&lt;P&gt;My extension are on the bellow screan&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="E_GK_0-1758272656758.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357733i938314E82DB801AD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="E_GK_0-1758272656758.png" alt="E_GK_0-1758272656758.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have a problem with example project - some missing path / tools&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="E_GK_1-1758272787393.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357734i821F5A89D3C479F8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="E_GK_1-1758272787393.png" alt="E_GK_1-1758272787393.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When I try to create new empty project and add the needed driver I see the bellow problems&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="E_GK_2-1758273199137.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357735i7F739B061A26186E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="E_GK_2-1758273199137.png" alt="E_GK_2-1758273199137.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;""driver" is not found in the toolchain/IDE project. The project will not compile!"&lt;/P&gt;&lt;P&gt;I'm going to develop software for S32K146 and S32K148 MCU base on the driver topology.&lt;/P&gt;&lt;P&gt;There are many version on your webside and many topics on the nxp community forum descibe a problem, but other versions of tool and IDE. For me there is a huge problem with namig of your version and tool. It is difficul to find what is necessary to start develop the software.&amp;nbsp;there's always something missing.&lt;/P&gt;&lt;P&gt;Could you please send me any short guide how to install all necessary tool for S32K14x family please?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Sep 2025 09:28:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2172691#M52844</guid>
      <dc:creator>E_GK</dc:creator>
      <dc:date>2025-09-19T09:28:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 / 148 Externall Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2172890#M52872</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211726"&gt;@E_GK&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;I apologize if the installation steps seem confusing.&lt;/P&gt;
&lt;P&gt;When importing a project, please carefully read the &lt;STRONG&gt;description.txt&lt;/STRONG&gt; file included with it. The steps to build it are described there:&lt;/P&gt;
&lt;P&gt;"Before running the example a configuration needs to be generated. First go to Project Explorer View in S32 DS and select the current project. Select the "S32 Configuration Tool" menu then click on the desired configuration tool (Pins, Cocks, Peripherals etc...). Clicking on any one of those will generate all the components. Make the desired changes(if any) then click on the "S32 Configuration Tool-&amp;gt;Update Code" button."&lt;/P&gt;
&lt;P&gt;You must click the "Update Code" button in order to generate the necessary code for the project:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Snag_45aa0b.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357781i95C0F14EB11EEB82/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Snag_45aa0b.png" alt="Snag_45aa0b.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;After this, you can build the project successfully. You can refer to the&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32DS-list-of-HOWTOs/ta-p/1113475" target="_blank" rel="noopener"&gt;S32DS - list of HOWTOs&lt;/A&gt;&amp;nbsp;for some introductory guides on how to use S32DS and its features.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Sep 2025 16:41:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2172890#M52872</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-09-19T16:41:34Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 / 148 Externall Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2172956#M52877</link>
      <description>&lt;P&gt;Hello Julian,&lt;/P&gt;&lt;P&gt;Thank you for this information.&lt;/P&gt;&lt;P&gt;1. I used "Update Code" button, but it was not solve my problem. I can't compile an example project.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="E_GK_1-1758309784374.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357792i2474AA48247AA557/image-size/medium?v=v2&amp;amp;px=400" role="button" title="E_GK_1-1758309784374.png" alt="E_GK_1-1758309784374.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2. In case of new project - how to solve the problem mentioned in my previous message?&lt;/P&gt;&lt;P&gt;"driver" is not found in the toolchain/IDE project. The project will not compile!"&lt;/P&gt;&lt;P&gt;How to add any driver to the MCU?&lt;/P&gt;&lt;P&gt;3. Is there any others possibility to use external interrupt without Autosar RTD extension?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Sep 2025 19:32:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2172956#M52877</guid>
      <dc:creator>E_GK</dc:creator>
      <dc:date>2025-09-19T19:32:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 / 148 Externall Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2173006#M52879</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211726"&gt;@E_GK&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;2. Normally, when adding drivers to the config tools, the driver is added to the project as well. Simply clicking "Update Code" generates the necessary files. You can also right-click and add them to the toolchain manually:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Snag_1819ba3.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357806iD7AC85C83F83EA86/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Snag_1819ba3.png" alt="Snag_1819ba3.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;3. Instead of using RTD, you can use&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5413.pdf" target="_blank"&gt;AN5413: S32K1xx Series Cookbook.&lt;/A&gt;&amp;nbsp;While there is no pin interrupt example, you can use it as reference. Chapter&amp;nbsp;2.3 (Hello World + Interrupts) shows how to configure interrupts.&lt;/P&gt;
&lt;P&gt;If the examples are not being imported correctly, there may be an issue with your RTD installations. If possible, please try to do a clean install. I've attached a simple guide on how to download and install the RTD packages. It is based on S32K3XX devices, but procedure is the same for S32K1.&lt;/P&gt;
&lt;P&gt;Hope this helps.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Sep 2025 22:22:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2173006#M52879</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-09-19T22:22:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 / 148 Externall Interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2175730#M53046</link>
      <description>&lt;P&gt;Hello tech support,&lt;BR /&gt;Finally I founded myself the example for externall interrupt for SDK and it works on my PCB.&lt;BR /&gt;I lost few days for find the proper solution.&lt;BR /&gt;For everyone who will use externall interrupt - The example looks like on the bellow screan.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="E_GK_0-1758794977834.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/358520iC4E8921DCF35CD44/image-size/medium?v=v2&amp;amp;px=400" role="button" title="E_GK_0-1758794977834.png" alt="E_GK_0-1758794977834.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Sep 2025 10:12:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-148-Externall-Interrupt/m-p/2175730#M53046</guid>
      <dc:creator>E_GK</dc:creator>
      <dc:date>2025-09-25T10:12:30Z</dc:date>
    </item>
  </channel>
</rss>