<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Use case for the digital filter on an input pin in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Use-case-for-the-digital-filter-on-an-input-pin/m-p/2171344#M52782</link>
    <description>&lt;P&gt;What is the intended use case for the digital filter on the I/O pins of the S32K1xx MCUs? It can delay the input for up to 31 clock cycles, but that is too small to be a debouncer for a push button (with the clock running from any source except for the 32kHz source), so it seems an external schmitt trigger or a software debouncer is needed for that. Is my understanding correct?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, on an unrelated note, when I access the NXP forums all the titles are in some Asian language; only the user generated code is in English (I am accessing this from the United States). This makes it cumbersome to use the site. I use Chrome running on Windows 11, but I have noticed the same behavior with Internet explorer as well.&lt;/P&gt;</description>
    <pubDate>Wed, 17 Sep 2025 18:59:14 GMT</pubDate>
    <dc:creator>durga_choudhury</dc:creator>
    <dc:date>2025-09-17T18:59:14Z</dc:date>
    <item>
      <title>Use case for the digital filter on an input pin</title>
      <link>https://community.nxp.com/t5/S32K/Use-case-for-the-digital-filter-on-an-input-pin/m-p/2171344#M52782</link>
      <description>&lt;P&gt;What is the intended use case for the digital filter on the I/O pins of the S32K1xx MCUs? It can delay the input for up to 31 clock cycles, but that is too small to be a debouncer for a push button (with the clock running from any source except for the 32kHz source), so it seems an external schmitt trigger or a software debouncer is needed for that. Is my understanding correct?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, on an unrelated note, when I access the NXP forums all the titles are in some Asian language; only the user generated code is in English (I am accessing this from the United States). This makes it cumbersome to use the site. I use Chrome running on Windows 11, but I have noticed the same behavior with Internet explorer as well.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Sep 2025 18:59:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Use-case-for-the-digital-filter-on-an-input-pin/m-p/2171344#M52782</guid>
      <dc:creator>durga_choudhury</dc:creator>
      <dc:date>2025-09-17T18:59:14Z</dc:date>
    </item>
    <item>
      <title>Re: Use case for the digital filter on an input pin</title>
      <link>https://community.nxp.com/t5/S32K/Use-case-for-the-digital-filter-on-an-input-pin/m-p/2171570#M52792</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;durga_choudhury&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;yes, your understanding is correct.&lt;/P&gt;
&lt;P&gt;The digital filter can delay input transitions by up to 31 clock cycles, which is useful for:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Filtering out short glitches or noise on digital inputs (e.g., from EMI or bouncing signals in high-speed environments).&lt;/LI&gt;
&lt;LI&gt;Ensuring signal stability before triggering interrupts or logic transitions.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;This is especially helpful for high-frequency signals or noisy environments, where short spikes could cause false triggering.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Use the digital filter for high-speed signal cleanup, like encoder inputs or external interrupts from fast peripherals.&lt;BR /&gt;For push buttons, rely on:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;Software debouncing (e.g., wait for stable state for 5–20 ms).&lt;/LI&gt;
&lt;LI&gt;Or external debounce circuits if hardware reliability is critical.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The language of the webpage can be changed after logging in. This should be related to your IP location, but I am not sure about the details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Sep 2025 03:12:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Use-case-for-the-digital-filter-on-an-input-pin/m-p/2171570#M52792</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2025-09-18T03:12:07Z</dc:date>
    </item>
  </channel>
</rss>